<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimx8mp</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp/m-p/1754560#M215474</link>
    <description>&lt;P&gt;Hello:&lt;/P&gt;&lt;P&gt;Hello:&lt;/P&gt;&lt;P&gt;My network port hardware is set to 1000Mb/s, and the phy is also 1000Mb/s phy. My switch has two modes, one is 1000Mb/s and the other is 100MB /s phy, which can be used after 1000Mb/s mode. If 100MB /s is used, it cannot be connected to the Internet. If the phy is identified as 100 Mbit /s, the transmission rate is different from that of 1000 MB /s. Is there any way to modify the driver or device tree, or any configuration, so that the network port can be identified as 1000 MB /s even when the network port is inserted into 100 Mbit /s?&lt;/P&gt;</description>
    <pubDate>Thu, 09 Nov 2023 02:24:57 GMT</pubDate>
    <dc:creator>qwerqq</dc:creator>
    <dc:date>2023-11-09T02:24:57Z</dc:date>
    <item>
      <title>imx8mp</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp/m-p/1754560#M215474</link>
      <description>&lt;P&gt;Hello:&lt;/P&gt;&lt;P&gt;Hello:&lt;/P&gt;&lt;P&gt;My network port hardware is set to 1000Mb/s, and the phy is also 1000Mb/s phy. My switch has two modes, one is 1000Mb/s and the other is 100MB /s phy, which can be used after 1000Mb/s mode. If 100MB /s is used, it cannot be connected to the Internet. If the phy is identified as 100 Mbit /s, the transmission rate is different from that of 1000 MB /s. Is there any way to modify the driver or device tree, or any configuration, so that the network port can be identified as 1000 MB /s even when the network port is inserted into 100 Mbit /s?&lt;/P&gt;</description>
      <pubDate>Thu, 09 Nov 2023 02:24:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp/m-p/1754560#M215474</guid>
      <dc:creator>qwerqq</dc:creator>
      <dc:date>2023-11-09T02:24:57Z</dc:date>
    </item>
  </channel>
</rss>