<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: imx8 running Linux not able to recognize USB ACM device</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8-running-Linux-not-able-to-recognize-USB-ACM-device/m-p/1754232#M215452</link>
    <description>&lt;P&gt;The driver name is different in github.&amp;nbsp; Instead of usb_acm the driver is cdc-acm.&lt;/P&gt;</description>
    <pubDate>Wed, 08 Nov 2023 12:56:34 GMT</pubDate>
    <dc:creator>Mojosound</dc:creator>
    <dc:date>2023-11-08T12:56:34Z</dc:date>
    <item>
      <title>imx8 running Linux not able to recognize USB ACM device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8-running-Linux-not-able-to-recognize-USB-ACM-device/m-p/1753622#M215382</link>
      <description>&lt;P&gt;I am working on a project where we are changing from an older imx6 architecture (not NXP) to an NXP based imx8 based system.&amp;nbsp; The imx6 system was running a stock Debian and included support for the usb_acm driver.&amp;nbsp; I cannot find support for the usb_acm driver in the github repository.&amp;nbsp; The board I am testing on is not recognizing the device.&amp;nbsp; This is a key peripheral to our system and a show stopper if not supported.&amp;nbsp; The device being connected has a STM32 processor and should come up as a comm port.&amp;nbsp; I did a search but could not find an answer to this.&amp;nbsp; If I missed it, please provide the link.&amp;nbsp; Otherwise, how can I resolve this?&amp;nbsp; Thanks.&lt;/P&gt;&lt;P&gt;&lt;A href="https://urldefense.com/v3/__https:/github.com/nxp-imx/linux-imx/tree/lf-5.15.y/drivers/media/radio__;!!N9ucCxr7cyPkMQ!tmuua6Vg4TWgk4Ev6dYBuxOhCYLWCee4_6QQz13h824CARHLscacwT9Eu4E-PX_R33Guhsr6xNHSY5Dw3XQ3f8xPJZvUGaZ_KcrSh7IV$" target="_blank" rel="noopener"&gt;https://github.com/nxp-imx/linux-imx/tree/lf-5.15.y/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Evaluation board used is&amp;nbsp;8MPLUSLPD4-EVK.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 07 Nov 2023 17:55:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8-running-Linux-not-able-to-recognize-USB-ACM-device/m-p/1753622#M215382</guid>
      <dc:creator>Mojosound</dc:creator>
      <dc:date>2023-11-07T17:55:10Z</dc:date>
    </item>
    <item>
      <title>Re: imx8 running Linux not able to recognize USB ACM device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8-running-Linux-not-able-to-recognize-USB-ACM-device/m-p/1754232#M215452</link>
      <description>&lt;P&gt;The driver name is different in github.&amp;nbsp; Instead of usb_acm the driver is cdc-acm.&lt;/P&gt;</description>
      <pubDate>Wed, 08 Nov 2023 12:56:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8-running-Linux-not-able-to-recognize-USB-ACM-device/m-p/1754232#M215452</guid>
      <dc:creator>Mojosound</dc:creator>
      <dc:date>2023-11-08T12:56:34Z</dc:date>
    </item>
    <item>
      <title>Re: imx8 running Linux not able to recognize USB ACM device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8-running-Linux-not-able-to-recognize-USB-ACM-device/m-p/1754266#M215454</link>
      <description>&lt;P&gt;(y)&lt;/P&gt;</description>
      <pubDate>Wed, 08 Nov 2023 14:07:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8-running-Linux-not-able-to-recognize-USB-ACM-device/m-p/1754266#M215454</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2023-11-08T14:07:10Z</dc:date>
    </item>
  </channel>
</rss>