<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Xip Bee  Bootloader Bug</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Xip-Bee-Bootloader-Bug/m-p/1753712#M215396</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you in advance for contacting NXP support.&lt;/P&gt;
&lt;P&gt;We have the following &lt;A title="document " href="https://www.nxp.com/docs/en/application-note/AN12604.pdf" target="_blank" rel="noopener"&gt;document&lt;/A&gt; that will help you out with the BEE XIP configuration this is based for RT10xx products please let me know if this guide was useful.&lt;/P&gt;</description>
    <pubDate>Tue, 07 Nov 2023 21:16:18 GMT</pubDate>
    <dc:creator>nxf77486</dc:creator>
    <dc:date>2023-11-07T21:16:18Z</dc:date>
    <item>
      <title>Xip Bee  Bootloader Bug</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Xip-Bee-Bootloader-Bug/m-p/1751801#M215200</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;Hello, I recently discovered an issue with BEE XIP encryption while debugging the RT1021 chip.&lt;/SPAN&gt;&lt;SPAN class=""&gt; My program structure is to write a bootloader myself (address: 0x6000000-0x60040000), and then load the APP to start (address: 0x60040000 0x6040000).&lt;/SPAN&gt;&lt;SPAN class=""&gt; The bootloader itself uses XIP BEE encryption to start, and then loads the APP and configures BEE to the APP startup area, achieving encrypted operation of both the bootloader and the App.&lt;/SPAN&gt;&lt;SPAN class=""&gt; The problem now is that even if the bootloader itself is not suitable for bee encryption, it runs normally. Once the bootloader uses bee encryption, the program will encounter inexplicable problems.&lt;/SPAN&gt;&lt;SPAN class=""&gt; Sometimes it can run normally, and sometimes modifying one or two lines of code can cause it to run away.&lt;/SPAN&gt;&lt;SPAN class=""&gt; I hope the engineers from the original factory can help analyze where the problem may be.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 03 Nov 2023 08:37:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Xip-Bee-Bootloader-Bug/m-p/1751801#M215200</guid>
      <dc:creator>leoqian</dc:creator>
      <dc:date>2023-11-03T08:37:25Z</dc:date>
    </item>
    <item>
      <title>Re: Xip Bee  Bootloader Bug</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Xip-Bee-Bootloader-Bug/m-p/1753712#M215396</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you in advance for contacting NXP support.&lt;/P&gt;
&lt;P&gt;We have the following &lt;A title="document " href="https://www.nxp.com/docs/en/application-note/AN12604.pdf" target="_blank" rel="noopener"&gt;document&lt;/A&gt; that will help you out with the BEE XIP configuration this is based for RT10xx products please let me know if this guide was useful.&lt;/P&gt;</description>
      <pubDate>Tue, 07 Nov 2023 21:16:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Xip-Bee-Bootloader-Bug/m-p/1753712#M215396</guid>
      <dc:creator>nxf77486</dc:creator>
      <dc:date>2023-11-07T21:16:18Z</dc:date>
    </item>
  </channel>
</rss>