<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックH.264 encoding using the i.MX processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/H-264-encoding-using-the-i-MX-processors/m-p/1748362#M214887</link>
    <description>&lt;P&gt;To whom it may concern,&lt;/P&gt;&lt;P&gt;I have the requirement of encoding a video (1080p30) using H.264 and then live stream the encoded video via Ethernet. I’m considering the i.MX 6 or the i.MX 8 for my application and I have the following questions:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Can the i.MX 8 and the i.MX 6 encode an interlaced video using H.264?&lt;/LI&gt;&lt;LI&gt;Would you please recommend an evaluation kit that is equipped with a PAL video decoder connected to the i.MX 8 or the i.MX 6 processor.&lt;/LI&gt;&lt;LI&gt;Would you please recommend an evaluation kit that is equipped with an SDI receiver chip (such as a Semtech SDI receiver) connected to the i.MX 8 or the i.MX 6 processor. I think that the i.MX 6 can interface to Semtech SDI receivers via the CSI interface?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Regards, &amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Fuad&lt;/P&gt;</description>
    <pubDate>Mon, 30 Oct 2023 06:38:09 GMT</pubDate>
    <dc:creator>Fuad</dc:creator>
    <dc:date>2023-10-30T06:38:09Z</dc:date>
    <item>
      <title>H.264 encoding using the i.MX processors</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/H-264-encoding-using-the-i-MX-processors/m-p/1748362#M214887</link>
      <description>&lt;P&gt;To whom it may concern,&lt;/P&gt;&lt;P&gt;I have the requirement of encoding a video (1080p30) using H.264 and then live stream the encoded video via Ethernet. I’m considering the i.MX 6 or the i.MX 8 for my application and I have the following questions:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Can the i.MX 8 and the i.MX 6 encode an interlaced video using H.264?&lt;/LI&gt;&lt;LI&gt;Would you please recommend an evaluation kit that is equipped with a PAL video decoder connected to the i.MX 8 or the i.MX 6 processor.&lt;/LI&gt;&lt;LI&gt;Would you please recommend an evaluation kit that is equipped with an SDI receiver chip (such as a Semtech SDI receiver) connected to the i.MX 8 or the i.MX 6 processor. I think that the i.MX 6 can interface to Semtech SDI receivers via the CSI interface?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Regards, &amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Fuad&lt;/P&gt;</description>
      <pubDate>Mon, 30 Oct 2023 06:38:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/H-264-encoding-using-the-i-MX-processors/m-p/1748362#M214887</guid>
      <dc:creator>Fuad</dc:creator>
      <dc:date>2023-10-30T06:38:09Z</dc:date>
    </item>
    <item>
      <title>Re: H.264 encoding using the i.MX processors</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/H-264-encoding-using-the-i-MX-processors/m-p/1749156#M214961</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224991"&gt;@Fuad&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;i.MX8 &amp;amp; i.MX6 series does have VPU for&amp;nbsp;H.264 encoding.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot from 2023-10-31 10-59-45.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/247603i8AFAF5CFD9585359/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot from 2023-10-31 10-59-45.png" alt="Screenshot from 2023-10-31 10-59-45.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;GStreamer 1.0 plugins for the same are also available.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot from 2023-10-31 11-03-38.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/247604i84ED10D004A8CCD0/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot from 2023-10-31 11-03-38.png" alt="Screenshot from 2023-10-31 11-03-38.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Dhruvit Vasavada&lt;/P&gt;</description>
      <pubDate>Tue, 31 Oct 2023 05:35:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/H-264-encoding-using-the-i-MX-processors/m-p/1749156#M214961</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2023-10-31T05:35:00Z</dc:date>
    </item>
  </channel>
</rss>