<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: copying kernel image to sd card failed</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/copying-kernel-image-to-sd-card-failed/m-p/1748254#M214871</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224924"&gt;@iDave&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;bootloader would be located at the fixed offset, but the kernel is probably not.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;To load these individuals one-by-one, refer to the&amp;nbsp;4.3 Preparing an SD/MMC card to boot of Linux User guide.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
    <pubDate>Mon, 30 Oct 2023 03:51:34 GMT</pubDate>
    <dc:creator>Harvey021</dc:creator>
    <dc:date>2023-10-30T03:51:34Z</dc:date>
    <item>
      <title>copying kernel image to sd card failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/copying-kernel-image-to-sd-card-failed/m-p/1747648#M214804</link>
      <description>&lt;P&gt;Hello, I am using imx8mm-evk, and testing to copy kernel image to sd card via dd command.&lt;/P&gt;&lt;P&gt;when I copy wic file(core-image-minimal) to sd card below, it boots well.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;zstdcat core-image-minimal-imx8mm-lpddr4-evk-20231025060017.rootfs.wic.zst  | sudo dd of=/dev/sdb bs=1M conv=fsync status=progress&lt;/LI-CODE&gt;&lt;P&gt;after I copied wic file, I copied kernel image(located /arch/arm64/boot/) from linux-imx below, but it doesn't boot after that.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;sudo dd if=Image of=/dev/sdb bs=512 seek=2048 conv=fsync&lt;/LI-CODE&gt;&lt;P&gt;is it right that the va seek parameter is 2048?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The following image is booting with sdcard which is after copying kernel image.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="iDave_0-1698393832284.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/247167i010BD6B176040F36/image-size/medium?v=v2&amp;amp;px=400" role="button" title="iDave_0-1698393832284.png" alt="iDave_0-1698393832284.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 27 Oct 2023 08:04:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/copying-kernel-image-to-sd-card-failed/m-p/1747648#M214804</guid>
      <dc:creator>iDave</dc:creator>
      <dc:date>2023-10-27T08:04:01Z</dc:date>
    </item>
    <item>
      <title>Re: copying kernel image to sd card failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/copying-kernel-image-to-sd-card-failed/m-p/1748254#M214871</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224924"&gt;@iDave&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;bootloader would be located at the fixed offset, but the kernel is probably not.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;To load these individuals one-by-one, refer to the&amp;nbsp;4.3 Preparing an SD/MMC card to boot of Linux User guide.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Mon, 30 Oct 2023 03:51:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/copying-kernel-image-to-sd-card-failed/m-p/1748254#M214871</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2023-10-30T03:51:34Z</dc:date>
    </item>
    <item>
      <title>Re: copying kernel image to sd card failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/copying-kernel-image-to-sd-card-failed/m-p/1748333#M214883</link>
      <description>Thank you. '4.3.5 Copying the kernel image and DTB file - Default VFAT partition' method works.</description>
      <pubDate>Mon, 30 Oct 2023 06:14:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/copying-kernel-image-to-sd-card-failed/m-p/1748333#M214883</guid>
      <dc:creator>iDave</dc:creator>
      <dc:date>2023-10-30T06:14:23Z</dc:date>
    </item>
  </channel>
</rss>