<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: QT creator example project fails to deploy</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/QT-creator-example-project-fails-to-deploy/m-p/1746266#M214704</link>
    <description>&lt;P&gt;in addition:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;when i go to launch the deployed application in /usr/examples/demos/mediaplayer i get this error:&lt;/P&gt;&lt;P&gt;./MediaPlayerApp: error while loading shared libraries: libQt6Multimedia.so.6: cannot open shared object file: No such file or directory&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and when i look in /usr/lib i do not see&amp;nbsp;libQt6Multimedia.so.6&lt;/P&gt;&lt;P&gt;so it looks like it won't run the actual demo by itself because it doesn't have the right library installed. i'm a bit of a newbie when it comes to yocto. where would i change the recipe to add this library and what do i need to add to do it?&lt;/P&gt;</description>
    <pubDate>Wed, 25 Oct 2023 18:37:13 GMT</pubDate>
    <dc:creator>Michael_Jacobson</dc:creator>
    <dc:date>2023-10-25T18:37:13Z</dc:date>
    <item>
      <title>QT creator example project fails to deploy</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/QT-creator-example-project-fails-to-deploy/m-p/1745482#M214645</link>
      <description>&lt;P&gt;i am using the imx93evk board with the full image running on it&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i just installed QT creator and picked an example project and loaded it with the boot2qt 6.6.0 NXP 93 EVK 11x11 environment. the example i picked was media player&lt;/P&gt;&lt;P&gt;it builds fine&lt;/P&gt;&lt;P&gt;i had to alter the deploy because rsync doesn't exist on the "full" image. that is issue 1&lt;/P&gt;&lt;P&gt;i changed it to deploy using sftp&lt;/P&gt;&lt;P&gt;when it goes to run it says this:&lt;/P&gt;&lt;P&gt;16:32:58: Starting /usr/bin/appcontroller /usr/examples/demos/mediaplayer/MediaPlayerApp on NXP imx93EVK...&lt;BR /&gt;sh: line 1: /usr/bin/appcontroller: No such file or directory&lt;BR /&gt;16:32:58: /usr/bin/appcontroller on NXP imx93EVK exited with code 127&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i assume app controller doesn't exist in the "full" image build&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;where do i start to fix this? why would example projects not work? is there some QT setting that needs to be added to make this work?&lt;/P&gt;</description>
      <pubDate>Tue, 24 Oct 2023 21:46:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/QT-creator-example-project-fails-to-deploy/m-p/1745482#M214645</guid>
      <dc:creator>Michael_Jacobson</dc:creator>
      <dc:date>2023-10-24T21:46:36Z</dc:date>
    </item>
    <item>
      <title>Re: QT creator example project fails to deploy</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/QT-creator-example-project-fails-to-deploy/m-p/1746266#M214704</link>
      <description>&lt;P&gt;in addition:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;when i go to launch the deployed application in /usr/examples/demos/mediaplayer i get this error:&lt;/P&gt;&lt;P&gt;./MediaPlayerApp: error while loading shared libraries: libQt6Multimedia.so.6: cannot open shared object file: No such file or directory&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and when i look in /usr/lib i do not see&amp;nbsp;libQt6Multimedia.so.6&lt;/P&gt;&lt;P&gt;so it looks like it won't run the actual demo by itself because it doesn't have the right library installed. i'm a bit of a newbie when it comes to yocto. where would i change the recipe to add this library and what do i need to add to do it?&lt;/P&gt;</description>
      <pubDate>Wed, 25 Oct 2023 18:37:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/QT-creator-example-project-fails-to-deploy/m-p/1746266#M214704</guid>
      <dc:creator>Michael_Jacobson</dc:creator>
      <dc:date>2023-10-25T18:37:13Z</dc:date>
    </item>
    <item>
      <title>Re: QT creator example project fails to deploy</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/QT-creator-example-project-fails-to-deploy/m-p/1750406#M215070</link>
      <description>&lt;P&gt;apparently there is a linking issue in that specific project which was discovered by Sam Davies&lt;/P&gt;</description>
      <pubDate>Wed, 01 Nov 2023 16:26:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/QT-creator-example-project-fails-to-deploy/m-p/1750406#M215070</guid>
      <dc:creator>Michael_Jacobson</dc:creator>
      <dc:date>2023-11-01T16:26:35Z</dc:date>
    </item>
  </channel>
</rss>