<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SPI as slave from user space in linux in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SPI-as-slave-from-user-space-in-linux/m-p/1743457#M214479</link>
    <description>&lt;P&gt;Are you using the NXP reference board? Which version BSP are you using? How do the controller connect to the i.MX8MP board?&lt;/P&gt;</description>
    <pubDate>Fri, 20 Oct 2023 06:51:24 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2023-10-20T06:51:24Z</dc:date>
    <item>
      <title>SPI as slave from user space in linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPI-as-slave-from-user-space-in-linux/m-p/1741880#M214248</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;I'm using a board with an imx8m plus CPU called a humming board pulse (controller). My controller will be used as an SPI slave. Tell me about any Linux user space APIs that I may use to use my controller as a slave, please.&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Kartheek&lt;/P&gt;</description>
      <pubDate>Wed, 18 Oct 2023 07:16:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPI-as-slave-from-user-space-in-linux/m-p/1741880#M214248</guid>
      <dc:creator>kartheek</dc:creator>
      <dc:date>2023-10-18T07:16:01Z</dc:date>
    </item>
    <item>
      <title>Re: SPI as slave from user space in linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPI-as-slave-from-user-space-in-linux/m-p/1743457#M214479</link>
      <description>&lt;P&gt;Are you using the NXP reference board? Which version BSP are you using? How do the controller connect to the i.MX8MP board?&lt;/P&gt;</description>
      <pubDate>Fri, 20 Oct 2023 06:51:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPI-as-slave-from-user-space-in-linux/m-p/1743457#M214479</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2023-10-20T06:51:24Z</dc:date>
    </item>
  </channel>
</rss>