<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックJ-Flash Error  on MIMXRT1064: Verification of RAMCode failed @ address 0x...</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/J-Flash-Error-on-MIMXRT1064-Verification-of-RAMCode-failed/m-p/1743378#M214468</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I can detect and connect to a MIMXRT1064 using JFlasher ARM with JFlash software.&amp;nbsp; But I could not do any readback or programming.&lt;/P&gt;&lt;P&gt;It always meet with some sort of RAMCode failure resulting with 'Failed to prepare for programming'.&amp;nbsp; I have tried V7.58 as well as V7.92.&lt;/P&gt;&lt;P&gt;Any advice please, thank you.&lt;/P&gt;</description>
    <pubDate>Fri, 20 Oct 2023 04:31:27 GMT</pubDate>
    <dc:creator>noni082002</dc:creator>
    <dc:date>2023-10-20T04:31:27Z</dc:date>
    <item>
      <title>J-Flash Error  on MIMXRT1064: Verification of RAMCode failed @ address 0x...</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/J-Flash-Error-on-MIMXRT1064-Verification-of-RAMCode-failed/m-p/1743378#M214468</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I can detect and connect to a MIMXRT1064 using JFlasher ARM with JFlash software.&amp;nbsp; But I could not do any readback or programming.&lt;/P&gt;&lt;P&gt;It always meet with some sort of RAMCode failure resulting with 'Failed to prepare for programming'.&amp;nbsp; I have tried V7.58 as well as V7.92.&lt;/P&gt;&lt;P&gt;Any advice please, thank you.&lt;/P&gt;</description>
      <pubDate>Fri, 20 Oct 2023 04:31:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/J-Flash-Error-on-MIMXRT1064-Verification-of-RAMCode-failed/m-p/1743378#M214468</guid>
      <dc:creator>noni082002</dc:creator>
      <dc:date>2023-10-20T04:31:27Z</dc:date>
    </item>
    <item>
      <title>Re: J-Flash Error  on MIMXRT1064: Verification of RAMCode failed @ address 0x...</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/J-Flash-Error-on-MIMXRT1064-Verification-of-RAMCode-failed/m-p/1745364#M214631</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/42997"&gt;@noni082002&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope you are doing well!&amp;nbsp;&lt;/P&gt;
&lt;P&gt;From my perspective you can double check HW setup first. Here are some general pointers:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;For programming operation, by default the i.MX RT10xx uses SWD&amp;nbsp; to use JTAG you need to burn a fuse.&amp;nbsp;&lt;/LI&gt;
&lt;LI&gt;Double check the JTAG_MOD, this pin should be pulled low to enable programming.&lt;/LI&gt;
&lt;LI&gt;Ensure that debugger has access to the reset_b pin.&lt;/LI&gt;
&lt;LI&gt;Check the boot mode and boot config pins. The internal boot from flash requires&amp;nbsp; to leave boot mode pins to 0b10 and all boot config pins to zero.&lt;/LI&gt;
&lt;LI&gt;Sometimes&amp;nbsp; it is useful to set the MCU to boot in serial downloader (boot mode pins to 0b01) and then do a mass erase. If this succeeds, try to program one more time and set boot mode to internal boot. This is a common practice to regain debug access.&lt;/LI&gt;
&lt;LI&gt;Consider double checking your design against the latest version of our&amp;nbsp; Hardware Development guide * &lt;STRONG&gt;MIMXRT105060HDUG&lt;/STRONG&gt;) and i.MX RT1064 EVK.&amp;nbsp;&lt;/LI&gt;
&lt;LI&gt;Debugging is always simpler when no fuse has been burned. Because fuses can alter the boot mode, boot config, security state, debug interface etc.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;All the best,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Diego&lt;/P&gt;
&lt;P&gt;.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 24 Oct 2023 16:53:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/J-Flash-Error-on-MIMXRT1064-Verification-of-RAMCode-failed/m-p/1745364#M214631</guid>
      <dc:creator>diego_charles</dc:creator>
      <dc:date>2023-10-24T16:53:59Z</dc:date>
    </item>
  </channel>
</rss>