<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: IMX8MP and TC358743</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-and-TC358743/m-p/1742868#M214420</link>
    <description>&lt;P&gt;Hi Gary,&lt;/P&gt;&lt;P&gt;Thank you for your answer.&lt;/P&gt;&lt;P&gt;I made a connection board between EVK carrier and TC358743 daughter board, so I can use the Basler-compliant connector. IRQ and Reset is connected via J31 connector of EVK carrier board (pins 17 and 19).&lt;/P&gt;&lt;P&gt;I used the .dts file for ENC carrier which you mentioned as a template.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;</description>
    <pubDate>Thu, 19 Oct 2023 10:54:24 GMT</pubDate>
    <dc:creator>David24</dc:creator>
    <dc:date>2023-10-19T10:54:24Z</dc:date>
    <item>
      <title>IMX8MP and TC358743</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-and-TC358743/m-p/1737433#M213863</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I need to connect Toshiba TC358743 HDMI to CSI bridge to IMX8M Plus. I use Nitrogen 8M Plus module (Boundary devices) and their carrier board. NIT8MP_EVK. TC358743 is connected to csi1 and doesn't work, no frames captured. Basler camera is connected to csi0 and works well. Boundary Yocto&amp;nbsp;&lt;SPAN&gt;kirkstone-5.15.71-2.2.0 Linux.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;My .dts is attached.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;root@nitrogen8mp:~# media-ctl -p&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;Media controller API version 5.15.71&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Media device information&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;------------------------&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;driver mxc-md&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;model FSL Capture Media Device&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;serial&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;bus info&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;hw revision 0x0&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;driver version 5.15.71&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Device topology&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;- entity 1: mxc_isi.1 (16 pads, 2 links)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;type V4L2 subdev subtype Unknown flags 0&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad0: Sink&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad1: Sink&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad2: Sink&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad3: Sink&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad4: Sink&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;&amp;lt;- "mxc-mipi-csi2.1":4 [ENABLED]&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad5: Sink&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad6: Sink&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad7: Sink&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad8: Sink&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad9: Sink&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad10: Sink&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad11: Sink&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad12: Source&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;-&amp;gt; "mxc_isi.1.capture":0 [ENABLED]&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad13: Source&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad14: Source&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad15: Sink&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;- entity 18: mxc_isi.1.capture (1 pad, 1 link)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;type Node subtype V4L flags 0&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;device node name /dev/video2&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad0: Sink&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;&amp;lt;- "mxc_isi.1":12 [ENABLED]&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;- entity 22: mxc-mipi-csi2.0 (8 pads, 1 link)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;type Node subtype V4L flags 0&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;device node name /dev/v4l-subdev0&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad0: Sink&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;&amp;lt;- "basler-camera-vvcam 7-0036":0 [ENABLED,IMMUTABLE]&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad1: Sink&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad2: Sink&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad3: Sink&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad4: Source&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad5: Source&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad6: Source&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad7: Source&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;- entity 31: mxc-mipi-csi2.1 (8 pads, 2 links)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;type Node subtype V4L flags 0&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;device node name /dev/v4l-subdev1&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad0: Sink&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;&amp;lt;- "tc358743 8-000f":0 [ENABLED,IMMUTABLE]&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad1: Sink&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad2: Sink&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad3: Sink&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad4: Source&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;-&amp;gt; "mxc_isi.1":4 [ENABLED]&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad5: Source&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad6: Source&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad7: Source&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;- entity 40: basler-camera-vvcam 7-0036 (1 pad, 1 link)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;type V4L2 subdev subtype Sensor flags 0&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;device node name /dev/v4l-subdev2&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad0: Source&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;-&amp;gt; "mxc-mipi-csi2.0":0 [ENABLED,IMMUTABLE]&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;- entity 42: tc358743 8-000f (1 pad, 1 link)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;type V4L2 subdev subtype Unknown flags 0&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;device node name /dev/v4l-subdev3&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;pad0: Source&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[fmt:UYVY8_2X8/1280x720 field:none colorspace:smpte170m]&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[dv.caps:BT.656/1120 min:640x350@13000000 max:1920x1200@165000000 stds:CEA-861,DMT,CVT,GTF caps:progressive,reduced-blanking,custom]&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[dv.detect:BT.656/1120 1280x720p60 (1650x750) stds: flags:]&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[dv.current:BT.656/1120 1280x720p60 (1650x750) stds: flags:]&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;-&amp;gt; "mxc-mipi-csi2.1":0 [ENABLED,IMMUTABLE]&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="4"&gt;status of TC358743:&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="4"&gt;&lt;FONT size="2"&gt;[ 8320.421906] tc358743 8-000f: -----Chip status-----&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.427589] tc358743 8-000f: Chip ID: 0x00&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.432509] tc358743 8-000f: Chip revision: 0x00&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.437141] tc358743 8-000f: Reset: IR: 1, CEC: 0, CSI TX: 0, HDMI: 0&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.443607] tc358743 8-000f: Sleep mode: off&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.447892] tc358743 8-000f: Cable detected (+5V power): yes&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.454300] tc358743 8-000f: DDC lines enabled: yes&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.459940] tc358743 8-000f: Hotplug enabled: yes&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.465466] tc358743 8-000f: CEC enabled: no&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.469741] tc358743 8-000f: -----Signal status-----&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.474714] tc358743 8-000f: TMDS signal detected: yes&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.479858] tc358743 8-000f: Stable sync signal: yes&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.484828] tc358743 8-000f: PHY PLL locked: yes&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.489452] tc358743 8-000f: PHY DE detected: yes&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.503359] tc358743 8-000f: Detected format: 1280x720p60.00 (1650x750)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.510039] tc358743 8-000f: horizontal: fp = 0, -sync = 370, bp = 0&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.516420] tc358743 8-000f: vertical: fp = 0, -sync = 30, bp = 0&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.522536] tc358743 8-000f: pixelclock: 74250000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.527259] tc358743 8-000f: flags (0x0):&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.531287] tc358743 8-000f: standards (0x0):&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.535657] tc358743 8-000f: Configured format: 1280x720p60.00 (1650x750)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.542452] tc358743 8-000f: horizontal: fp = 0, -sync = 370, bp = 0&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.548812] tc358743 8-000f: vertical: fp = 0, -sync = 30, bp = 0&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.554910] tc358743 8-000f: pixelclock: 74250000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.559620] tc358743 8-000f: flags (0x0):&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.563637] tc358743 8-000f: standards (0x0):&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.567999] tc358743 8-000f: -----CSI-TX status-----&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.572969] tc358743 8-000f: Lanes needed: 2&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.577243] tc358743 8-000f: Lanes in use: 2&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.582334] tc358743 8-000f: Waiting for particular sync signal: no&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.589428] tc358743 8-000f: Transmit mode: yes&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.594769] tc358743 8-000f: Receive mode: no&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.599945] tc358743 8-000f: Stopped: no&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.603880] tc358743 8-000f: Color space: YCbCr 422 2x8-bit&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.610172] tc358743 8-000f: -----DVI-D status-----&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.615063] tc358743 8-000f: HDCP encrypted content: no&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 8320.620298] tc358743 8-000f: Input color space: RGB full range&lt;/FONT&gt;&lt;BR /&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="4"&gt;CSI registers:&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="4"&gt;&lt;FONT size="2"&gt;[ 330.076909] mxc-mipi-csi2.1: --- mipi_csis_s_stream ---&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 330.076916] mxc-mipi-csi2.1: CSIS_VERSION[0]: 0x03060301&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 330.076922] mxc-mipi-csi2.1: CSIS_CMN_CTRL[4]: 0x00004905&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 330.076927] mxc-mipi-csi2.1: CSIS_CLK_CTRL[8]: 0x000f0000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 330.076933] mxc-mipi-csi2.1: CSIS_INTMSK[10]: 0x0fffff1f&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 330.076940] mxc-mipi-csi2.1: CSIS_INTSRC[14]: 0x00000000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 330.076946] mxc-mipi-csi2.1: CSIS_DPHYSTATUS[20]: 0x000000c2&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 330.076951] mxc-mipi-csi2.1: CSIS_DPHYCTRL[24]: 0x06000007&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 330.076958] mxc-mipi-csi2.1: CSIS_DPHYBCTRL_L[30]: 0x000001f4&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 330.076964] mxc-mipi-csi2.1: CSIS_DPHYBCTRL_H[34]: 0x00000000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 330.076969] mxc-mipi-csi2.1: CSIS_DPHYSCTRL_L[38]: 0x00000000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 330.076975] mxc-mipi-csi2.1: CSIS_DPHYSCTRL_H[3c]: 0x00000000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 330.076980] mxc-mipi-csi2.1: CSIS_ISPCONFIG_CH0[40]: 0x00001078&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 330.076985] mxc-mipi-csi2.1: CSIS_ISPCONFIG_CH1[50]: 0x000008fd&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 330.076992] mxc-mipi-csi2.1: CSIS_ISPCONFIG_CH2[60]: 0x000008fe&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 330.076997] mxc-mipi-csi2.1: CSIS_ISPCONFIG_CH3[70]: 0x000008ff&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 330.077002] mxc-mipi-csi2.1: CSIS_ISPRESOL_CH0[44]: 0x02d00500&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 330.077009] mxc-mipi-csi2.1: CSIS_ISPRESOL_CH1[54]: 0x80008000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 330.077015] mxc-mipi-csi2.1: CSIS_ISPRESOL_CH2[64]: 0x80008000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 330.077020] mxc-mipi-csi2.1: CSIS_ISPRESOL_CH3[74]: 0x80008000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 330.077025] mxc-mipi-csi2.1: CSIS_ISPSYNC_CH0[48]: 0x00000000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 330.077030] mxc-mipi-csi2.1: CSIS_ISPSYNC_CH1[58]: 0x00000000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 330.077037] mxc-mipi-csi2.1: CSIS_ISPSYNC_CH2[68]: 0x00000000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 330.077043] mxc-mipi-csi2.1: CSIS_ISPSYNC_CH3[78]: 0x00000000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 330.077050] mxc-mipi-csi2.1: --- mipi_csis_s_stream ---&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 330.077054] mxc-mipi-csi2.1: GPR_GASKET_0_CTRL[60]: 0xffff8000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 330.077059] mxc-mipi-csi2.1: GPR_GASKET_0_HSIZE[64]: 0xffff8000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;[ 330.077064] mxc-mipi-csi2.1: GPR_GASKET_0_VSIZE[68]: 0xffff8000&lt;/FONT&gt;&lt;BR /&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="4"&gt;It seems like a clock lane is stopped and in ULPS. I don't know why. HS-settle and CLK-settle should be correct. Data lanes are alive. I checked it by an oscilloscope. Could anybody help, please?&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="4"&gt;David&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 11 Oct 2023 11:24:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-and-TC358743/m-p/1737433#M213863</guid>
      <dc:creator>David24</dc:creator>
      <dc:date>2023-10-11T11:24:12Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP and TC358743</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-and-TC358743/m-p/1737592#M213875</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You may have added the driver for it since M8MP does not have the driver for it, maybe&amp;nbsp;@boundary can help&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 11 Oct 2023 14:36:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-and-TC358743/m-p/1737592#M213875</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2023-10-11T14:36:33Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP and TC358743</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-and-TC358743/m-p/1738552#M213940</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;TC358743 driver is part of Boundary system image.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 12 Oct 2023 10:20:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-and-TC358743/m-p/1738552#M213940</guid>
      <dc:creator>David24</dc:creator>
      <dc:date>2023-10-12T10:20:32Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP and TC358743</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-and-TC358743/m-p/1739272#M214004</link>
      <description>&lt;P&gt;The driver mentioned above seems to work. I think the problem is in the ISI module. I don't know if it needs to be configured somehow.&lt;/P&gt;</description>
      <pubDate>Fri, 13 Oct 2023 07:51:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-and-TC358743/m-p/1739272#M214004</guid>
      <dc:creator>David24</dc:creator>
      <dc:date>2023-10-13T07:51:25Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP and TC358743</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-and-TC358743/m-p/1742836#M214416</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;There's already a device tree for TC358743:&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/boundarydevices/linux/blob/boundary-imx_6.1.y/arch/arm64/boot/dts/freescale/imx8mp-nitrogen8mp-enc-tc358743.dts" target="_blank"&gt;https://github.com/boundarydevices/linux/blob/boundary-imx_6.1.y/arch/arm64/boot/dts/freescale/imx8mp-nitrogen8mp-enc-tc358743.dts&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Note that you can only connect our TC358743 daughter to the ENC carrier which is tied to CSI1.&lt;/P&gt;&lt;P&gt;The EVK carrier only includes Basler-compliant connectors.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gary&lt;/P&gt;</description>
      <pubDate>Thu, 19 Oct 2023 09:44:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-and-TC358743/m-p/1742836#M214416</guid>
      <dc:creator>gary_bisson</dc:creator>
      <dc:date>2023-10-19T09:44:05Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP and TC358743</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-and-TC358743/m-p/1742868#M214420</link>
      <description>&lt;P&gt;Hi Gary,&lt;/P&gt;&lt;P&gt;Thank you for your answer.&lt;/P&gt;&lt;P&gt;I made a connection board between EVK carrier and TC358743 daughter board, so I can use the Basler-compliant connector. IRQ and Reset is connected via J31 connector of EVK carrier board (pins 17 and 19).&lt;/P&gt;&lt;P&gt;I used the .dts file for ENC carrier which you mentioned as a template.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;</description>
      <pubDate>Thu, 19 Oct 2023 10:54:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-and-TC358743/m-p/1742868#M214420</guid>
      <dc:creator>David24</dc:creator>
      <dc:date>2023-10-19T10:54:24Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP and TC358743</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-and-TC358743/m-p/1756814#M215685</link>
      <description>&lt;P&gt;A problem is in a function enable_stream() in tc358743.c. IMX8M Plus CSI2 DPHY needs non-continuous clock or at least one transition LP11-&amp;gt;HS at the beginning of stream. TC358743 is initialized according to device tree settings (clock non-continuous) and then the function changes the clock settings to continuous. It tries to do the LP11-&amp;gt;HS transition but a receiver doesn't get it and clock lane stays in stop state. Solution is to remove a part of a code which does the transition (i2c_wr32(sd, TXOPTIONCNTRL, 0);&amp;nbsp;i2c_wr32(sd, TXOPTIONCNTRL, MASK_CONTCLKMODE);).&lt;/P&gt;</description>
      <pubDate>Tue, 14 Nov 2023 09:32:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-and-TC358743/m-p/1756814#M215685</guid>
      <dc:creator>David24</dc:creator>
      <dc:date>2023-11-14T09:32:41Z</dc:date>
    </item>
  </channel>
</rss>