<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックBuild Linux from scratch for Coral devkit</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Build-Linux-from-scratch-for-Coral-devkit/m-p/1356008#M214329</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I want to learn how to build Linux (and maybe Android) for embedded devices. The main goal is to write drivers. I've already worked with Cortex-M microcontrollers, so I think using an i.MX8 with auxilliary M4 core is a nice add-on. While searching for an appropriate platform, I came across the Coral devkit which is additionally interesting because of the Edge TPU and the board doesn't cost much.&lt;BR /&gt;&lt;BR /&gt;I wonder what would be needed to build Linux from scratch for this board? For the first steps I'd use the Coral Mendel distribution, but later I want to build the system by myself. The "getting started with Mendel Linux" guide describes how to do it by using several tools like Gerrit, Docker, etc. but I don't want to be fixed to them. I also want to be able to try other approaches as well. Looking at Raspberry PI where it seems that there are multiple ways to build a Linux system for it, I assume it should also be possible for the i.MX8 and the Coral devkit. For example, the i.MX8 documentation uses YOCTO to build Linux for the i.MX8 devices.&lt;BR /&gt;So, for example, if I decide to use YOCTO, how would Linux be build for the Coral devkit? What would be needed? Has anyone already build a 'non-Mendel' Linux for the Coral devkit?&lt;BR /&gt;&lt;BR /&gt;Regards&lt;/P&gt;</description>
    <pubDate>Tue, 17 Oct 2023 22:28:47 GMT</pubDate>
    <dc:creator>RA1981</dc:creator>
    <dc:date>2023-10-17T22:28:47Z</dc:date>
    <item>
      <title>Build Linux from scratch for Coral devkit</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Build-Linux-from-scratch-for-Coral-devkit/m-p/1356008#M214329</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I want to learn how to build Linux (and maybe Android) for embedded devices. The main goal is to write drivers. I've already worked with Cortex-M microcontrollers, so I think using an i.MX8 with auxilliary M4 core is a nice add-on. While searching for an appropriate platform, I came across the Coral devkit which is additionally interesting because of the Edge TPU and the board doesn't cost much.&lt;BR /&gt;&lt;BR /&gt;I wonder what would be needed to build Linux from scratch for this board? For the first steps I'd use the Coral Mendel distribution, but later I want to build the system by myself. The "getting started with Mendel Linux" guide describes how to do it by using several tools like Gerrit, Docker, etc. but I don't want to be fixed to them. I also want to be able to try other approaches as well. Looking at Raspberry PI where it seems that there are multiple ways to build a Linux system for it, I assume it should also be possible for the i.MX8 and the Coral devkit. For example, the i.MX8 documentation uses YOCTO to build Linux for the i.MX8 devices.&lt;BR /&gt;So, for example, if I decide to use YOCTO, how would Linux be build for the Coral devkit? What would be needed? Has anyone already build a 'non-Mendel' Linux for the Coral devkit?&lt;BR /&gt;&lt;BR /&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 17 Oct 2023 22:28:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Build-Linux-from-scratch-for-Coral-devkit/m-p/1356008#M214329</guid>
      <dc:creator>RA1981</dc:creator>
      <dc:date>2023-10-17T22:28:47Z</dc:date>
    </item>
  </channel>
</rss>