<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX8M PLUS UART1 not working in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-PLUS-UART1-not-working/m-p/1739823#M214043</link>
    <description>&lt;P&gt;My memory is a bit vague but I think we worked around the issue by building the SDMA as a module instead of built-in to kernel.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sun, 15 Oct 2023 06:38:28 GMT</pubDate>
    <dc:creator>tamo2</dc:creator>
    <dc:date>2023-10-15T06:38:28Z</dc:date>
    <item>
      <title>iMX8M PLUS UART1 not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-PLUS-UART1-not-working/m-p/1418833#M187448</link>
      <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I am working on custom board based on iMX8M Plus processor and I want to use UART1 as a communication uart between 2 boards. But I am unable to receive anything on that uart1. Do I need to change anything in .dts file?&lt;/P&gt;&lt;P&gt;I wrote a sample code (application) to receive through uart1.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am getting "imx-uart 30860000.serial: We cannot prepare for the RX slave dma!" this type of error while running the application.&lt;/P&gt;&lt;P&gt;I changed&amp;nbsp;CONFIG_IMX_SDMA=y to&amp;nbsp;CONFIG_IMX_SDMA=m still it not work.&lt;/P&gt;&lt;P&gt;can anyone please help me here?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 24 Feb 2022 06:28:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-PLUS-UART1-not-working/m-p/1418833#M187448</guid>
      <dc:creator>swapnilturambekar</dc:creator>
      <dc:date>2022-02-24T06:28:28Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M PLUS UART1 not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-PLUS-UART1-not-working/m-p/1630758#M203965</link>
      <description>&lt;P&gt;I am getting the exact same error "We cannot prepare for the RX slave dma" built using Kirkstone.&amp;nbsp; Have you been able to solve the issue?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 10 Apr 2023 22:47:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-PLUS-UART1-not-working/m-p/1630758#M203965</guid>
      <dc:creator>tamo2</dc:creator>
      <dc:date>2023-04-10T22:47:43Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M PLUS UART1 not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-PLUS-UART1-not-working/m-p/1739814#M214041</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/195580"&gt;@tamo2&lt;/a&gt;&amp;nbsp;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/191259"&gt;@swapnilturambekar&lt;/a&gt;&amp;nbsp;, I'm am getting the exact same error on Kirkstone on an imx8mm. It seems to be generate when we get framing errors while using the DMA. Have you fix the issue?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 14 Oct 2023 19:28:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-PLUS-UART1-not-working/m-p/1739814#M214041</guid>
      <dc:creator>Olivier_B</dc:creator>
      <dc:date>2023-10-14T19:28:03Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M PLUS UART1 not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-PLUS-UART1-not-working/m-p/1739823#M214043</link>
      <description>&lt;P&gt;My memory is a bit vague but I think we worked around the issue by building the SDMA as a module instead of built-in to kernel.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 15 Oct 2023 06:38:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-PLUS-UART1-not-working/m-p/1739823#M214043</guid>
      <dc:creator>tamo2</dc:creator>
      <dc:date>2023-10-15T06:38:28Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M PLUS UART1 not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-PLUS-UART1-not-working/m-p/1796024#M219243</link>
      <description>which kernel version is/was based your project?</description>
      <pubDate>Fri, 26 Jan 2024 10:45:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-PLUS-UART1-not-working/m-p/1796024#M219243</guid>
      <dc:creator>gigli_korg</dc:creator>
      <dc:date>2024-01-26T10:45:13Z</dc:date>
    </item>
  </channel>
</rss>