<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX8M Nano eMMC boot options in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Nano-eMMC-boot-options/m-p/1738864#M213970</link>
    <description>&lt;P&gt;Hello,&amp;nbsp; We have developed a custom i.MX8M Nano application bd.&amp;nbsp; We are currently booting from NOR but would like to have the option to boot from eMMC as well.&amp;nbsp; Looking through the flash controller documentation it seems feasible to wire this to the SD1 interface. The question we have is regarding boot.&amp;nbsp; The default from Boot_Mode[1] is from USHDC3 (the SD3) interface.&amp;nbsp; However according to the RM we can boot from any SD port using fuses.&lt;/P&gt;&lt;P&gt;If we wanted to boot from USDHC1 we need to write 01(b) to bits 10:9 of fuses at 0x470.&amp;nbsp; Is our understanding that doing this would allow us to boot from eMMC on SD1?&amp;nbsp; Specifically if we set fuses as per above and used resistor select 0010 basically setting Boot_Mode_[1].&amp;nbsp;&amp;nbsp; The fuse selection in this case would allow the i.MX8MN to overide USDHC3.&amp;nbsp;&lt;/P&gt;&lt;P&gt;If we have misunderstood or this is not possible, any clarification would be greatly appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JHT_0-1697134727762.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/244868i0B2622FC86599220/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JHT_0-1697134727762.png" alt="JHT_0-1697134727762.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JHT_1-1697134809158.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/244869i761AA4BF82DC2A83/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JHT_1-1697134809158.png" alt="JHT_1-1697134809158.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 12 Oct 2023 18:31:25 GMT</pubDate>
    <dc:creator>JHT</dc:creator>
    <dc:date>2023-10-12T18:31:25Z</dc:date>
    <item>
      <title>i.MX8M Nano eMMC boot options</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Nano-eMMC-boot-options/m-p/1738864#M213970</link>
      <description>&lt;P&gt;Hello,&amp;nbsp; We have developed a custom i.MX8M Nano application bd.&amp;nbsp; We are currently booting from NOR but would like to have the option to boot from eMMC as well.&amp;nbsp; Looking through the flash controller documentation it seems feasible to wire this to the SD1 interface. The question we have is regarding boot.&amp;nbsp; The default from Boot_Mode[1] is from USHDC3 (the SD3) interface.&amp;nbsp; However according to the RM we can boot from any SD port using fuses.&lt;/P&gt;&lt;P&gt;If we wanted to boot from USDHC1 we need to write 01(b) to bits 10:9 of fuses at 0x470.&amp;nbsp; Is our understanding that doing this would allow us to boot from eMMC on SD1?&amp;nbsp; Specifically if we set fuses as per above and used resistor select 0010 basically setting Boot_Mode_[1].&amp;nbsp;&amp;nbsp; The fuse selection in this case would allow the i.MX8MN to overide USDHC3.&amp;nbsp;&lt;/P&gt;&lt;P&gt;If we have misunderstood or this is not possible, any clarification would be greatly appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JHT_0-1697134727762.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/244868i0B2622FC86599220/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JHT_0-1697134727762.png" alt="JHT_0-1697134727762.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JHT_1-1697134809158.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/244869i761AA4BF82DC2A83/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JHT_1-1697134809158.png" alt="JHT_1-1697134809158.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 12 Oct 2023 18:31:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Nano-eMMC-boot-options/m-p/1738864#M213970</guid>
      <dc:creator>JHT</dc:creator>
      <dc:date>2023-10-12T18:31:25Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M Nano eMMC boot options</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Nano-eMMC-boot-options/m-p/1738922#M213981</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products.&lt;/P&gt;
&lt;P&gt;Your understanding is correct, you can refer to &lt;SPAN class="fontstyle0"&gt;6.1.5.4.1 Expansion device eFUSE configuration.&lt;/SPAN&gt;&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;SPAN class="fontstyle0"&gt;11 - 9: Select which SDHC module and what flash you will use but you need to override.&lt;/SPAN&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;SPAN class="fontstyle0"&gt;15 - 12: You also need to tell the fuses to boot from emmc.&lt;/SPAN&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;SPAN class="fontstyle0"&gt;And you need to tell the device to boot from fuses either from pins to 0000 or the override pins fuse.&lt;/SPAN&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 12 Oct 2023 20:42:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Nano-eMMC-boot-options/m-p/1738922#M213981</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2023-10-12T20:42:32Z</dc:date>
    </item>
  </channel>
</rss>