<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRT1176 wakeup though CAN</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RT1176-wakeup-though-CAN/m-p/1738398#M213928</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are using IMXRT1176 controller for our instrument cluster application.&lt;/P&gt;&lt;P&gt;MCU will be in sleep mode when our vehicle is not operated.&lt;/P&gt;&lt;P&gt;Wakeup should be done through CAN bus.&lt;/P&gt;&lt;P&gt;CAN transceiver : supports a low-power&lt;BR /&gt;standby mode and wake over CAN which is compliant&lt;BR /&gt;to the ISO 11898-2:2016 defined wake-up pattern&lt;BR /&gt;(WUP).&lt;/P&gt;&lt;P&gt;The low-power receiver and bus monitor circuits are enabled to allow for RXD wake-up requests via the CAN bus. A wake-up request is output to RXD . The MCU RT1176 CAN protocol controller should monitor RXD for transitions (high-to-low) and reactivate the device to normal mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Whether our MCU RT1176 is capable of monitoring the CAN RXD pin in sleep mode and can wake up the entire system?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 12 Oct 2023 08:15:11 GMT</pubDate>
    <dc:creator>Chethanbg</dc:creator>
    <dc:date>2023-10-12T08:15:11Z</dc:date>
    <item>
      <title>RT1176 wakeup though CAN</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1176-wakeup-though-CAN/m-p/1738398#M213928</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are using IMXRT1176 controller for our instrument cluster application.&lt;/P&gt;&lt;P&gt;MCU will be in sleep mode when our vehicle is not operated.&lt;/P&gt;&lt;P&gt;Wakeup should be done through CAN bus.&lt;/P&gt;&lt;P&gt;CAN transceiver : supports a low-power&lt;BR /&gt;standby mode and wake over CAN which is compliant&lt;BR /&gt;to the ISO 11898-2:2016 defined wake-up pattern&lt;BR /&gt;(WUP).&lt;/P&gt;&lt;P&gt;The low-power receiver and bus monitor circuits are enabled to allow for RXD wake-up requests via the CAN bus. A wake-up request is output to RXD . The MCU RT1176 CAN protocol controller should monitor RXD for transitions (high-to-low) and reactivate the device to normal mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Whether our MCU RT1176 is capable of monitoring the CAN RXD pin in sleep mode and can wake up the entire system?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 12 Oct 2023 08:15:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1176-wakeup-though-CAN/m-p/1738398#M213928</guid>
      <dc:creator>Chethanbg</dc:creator>
      <dc:date>2023-10-12T08:15:11Z</dc:date>
    </item>
    <item>
      <title>Re: RT1176 wakeup though CAN</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1176-wakeup-though-CAN/m-p/1740682#M214129</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;The FlexCAN module of i.MX RT1170 has two modes for low-power operation (&lt;EM&gt;Doze&lt;/EM&gt; and &lt;EM&gt;Stop&lt;/EM&gt; modes) that support a &lt;EM&gt;Self Wake Up mechanism&lt;/EM&gt;. (Please refer to &lt;EM&gt;66.3.1 Modes of operation&lt;/EM&gt; section fo reference manual).&lt;/P&gt;
&lt;P&gt;Hope it helps you.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Mon, 16 Oct 2023 22:29:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1176-wakeup-though-CAN/m-p/1740682#M214129</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2023-10-16T22:29:06Z</dc:date>
    </item>
  </channel>
</rss>