<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX8MP Custom Board LVDS Display</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Custom-Board-LVDS-Display/m-p/1735692#M213730</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206842"&gt;@Wobaffet&lt;/a&gt;,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I hope you are doing well.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can you follow this link and check by running the command described in the link?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A href="https://github.com/nxp-imx/weston-imx" target="_blank"&gt;https://github.com/nxp-imx/weston-imx&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Please also follow this link in order to start the Weston, Please apply these changes and check.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/How-to-start-Weston-in-fsl-image-validation-imx-image/td-p/866716" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/How-to-start-Weston-in-fsl-image-validation-imx-image/td-p/866716&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;DIV&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/Unable-to-start-weston-wayland-on-imx8mm/m-p/1658344" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/Unable-to-start-weston-wayland-on-imx8mm/m-p/1658344&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;It will be helpful.&lt;BR /&gt;&lt;BR /&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Sanket Parekh&lt;/DIV&gt;</description>
    <pubDate>Mon, 09 Oct 2023 09:43:41 GMT</pubDate>
    <dc:creator>Sanket_Parekh</dc:creator>
    <dc:date>2023-10-09T09:43:41Z</dc:date>
    <item>
      <title>i.MX8MP Custom Board LVDS Display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Custom-Board-LVDS-Display/m-p/1728885#M213102</link>
      <description>&lt;P&gt;Hello, We are trying to bring up our LVDS display with our custom board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;we've patched the device tree imx8mp-evk.dts for the kernel as follows:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;  lvds_backlight: lvds_backlight {
                compatible = "pwm-backlight";
                pwms = &amp;lt;&amp;amp;pwm2 0 100000 0&amp;gt;;
                status = "okay";

                brightness-levels = &amp;lt; 0  1  2  3  4  5  6  7  8  9
                                     10 11 12 13 14 15 16 17 18 19
                                     20 21 22 23 24 25 26 27 28 29
                                     30 31 32 33 34 35 36 37 38 39
                                     40 41 42 43 44 45 46 47 48 49
                                     50 51 52 53 54 55 56 57 58 59
                                     60 61 62 63 64 65 66 67 68 69
                                     70 71 72 73 74 75 76 77 78 79
                                     80 81 82 83 84 85 86 87 88 89
                                     90 91 92 93 94 95 96 97 98 99
                                    100&amp;gt;;
                default-brightness-level = &amp;lt;80&amp;gt;;
        };
        lvds_panel0 {
                compatible = "dlc,dlc1010gig";
                backlight = &amp;lt;&amp;amp;lvds_backlight&amp;gt;;

                        port{
                                panel_lvds0_in: endpoint {
                                remote-endpoint=&amp;lt;&amp;amp;lvds_out&amp;gt;;
                                };
                         };
        };
lvds_bridge: lvds-to-hdmi-bridge@4c {
                compatible = "ite,it6263";
                reg = &amp;lt;0x4c&amp;gt;;
                reset-gpios = &amp;lt;&amp;amp;gpio1 10 GPIO_ACTIVE_LOW&amp;gt;;
                status = "disabled";
                port {
                        it6263_in: endpoint {
                                remote-endpoint = &amp;lt;&amp;amp;lvds_out&amp;gt;;
                        };
                };
        };
&amp;amp;ldb {
        status = "okay";

        lvds-channel@0 {
                fsl,data-mapping = "jeida";
                fsl,data-width = &amp;lt;24&amp;gt;;
                status = "okay";

                port@1{
                        reg=&amp;lt;1&amp;gt;;
                        lvds_out: endpoint{
                                remote-endpoint = &amp;lt;&amp;amp;panel_lvds0_in&amp;gt;;
                        };

                };
        };
};

&amp;amp;ldb_phy {
        status = "okay";
};&lt;/LI-CODE&gt;&lt;P&gt;We've built the imx-image-core to test out the LVDS, but at the start-up we get the following log:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;[FAILED] Failed to start Weston, a …mpositor, as a system service.
See 'systemctl status weston.service' for details.&lt;/LI-CODE&gt;&lt;P&gt;Then for the&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@imx8mp-lpddr4-evk:/# weston info
Date: 2022-11-08 UTC
[14:14:37.442] weston 11.0.1
               https://wayland.freedesktop.org
               Bug reports to: https://gitlab.freedesktop.org/wayland/weston/issues/
               Build: lf-6.1.1-1.0.0+
[14:14:37.443] Command line: weston info
[14:14:37.443] OS: Linux, 6.1.1+g32c8c4ce7e52, #1 SMP PREEMPT Thu Mar  2 14:54:17 UTC 2023, aarch64
[14:14:37.443] Flight recorder: enabled
[14:14:37.443] Using config file '/etc/xdg/weston/weston.ini'
[14:14:37.443] Output repaint window is 16 ms maximum.
[14:14:37.443] Loading module '/usr/lib/libweston-11/wayland-backend.so'
[14:14:37.443] Failed to load module: /usr/lib/libweston-11/wayland-backend.so: cannot open shared object file: No such file or directory
[14:14:37.443] fatal: failed to create compositor backend&lt;/LI-CODE&gt;&lt;LI-CODE lang="markup"&gt;root@imx8mp-lpddr4-evk:/# systemctl status weston.service
x weston.service - Weston, a Wayland compositor, as a system service
     Loaded: loaded (/lib/systemd/system/weston.service; enabled; preset: enabled)
     Active: failed (Result: exit-code) since Tue 2022-11-08 14:17:34 UTC; 1min 21s ago
TriggeredBy: * weston.socket
       Docs: man:weston(1)
             man:weston.ini(5)
             http://wayland.freedesktop.org/
    Process: 603 ExecStart=/usr/bin/weston --log=${XDG_RUNTIME_DIR}/weston.log --modules=systemd-notify.&amp;gt;
   Main PID: 603 (code=exited, status=1/FAILURE)

Nov 08 14:17:34 imx8mp-lpddr4-evk systemd[1]: Starting Weston, a Wayland compositor, as a system service&amp;gt;
Nov 08 14:17:34 imx8mp-lpddr4-evk systemd[1]: weston.service: Main process exited, code=exited, status=1&amp;gt;
Nov 08 14:17:34 imx8mp-lpddr4-evk systemd[1]: weston.service: Failed with result 'exit-code'.
Nov 08 14:17:34 imx8mp-lpddr4-evk systemd[1]: Failed to start Weston, a Wayland compositor, as a system &amp;gt;&lt;/LI-CODE&gt;&lt;LI-CODE lang="markup"&gt;root@imx8mp-lpddr4-evk:/# journalctl -xeu weston.service
-- 
-- A start job for unit weston.service has begun execution.
-- 
-- The job identifier is 118.
Nov 08 14:00:22 imx8mp-lpddr4-evk systemd[1]: weston.service: Main process exited, code=exited, status=1&amp;gt;
-- Subject: Unit process exited
-- Defined-By: systemd
-- Support: https://lists.freedesktop.org/mailman/listinfo/systemd-devel
-- 
-- An ExecStart= process belonging to unit weston.service has exited.
-- 
-- The process' exit code is 'exited' and its exit status is 1.
Nov 08 14:00:22 imx8mp-lpddr4-evk systemd[1]: weston.service: Failed with result 'exit-code'.
-- Subject: Unit failed
-- Defined-By: systemd
-- Support: https://lists.freedesktop.org/mailman/listinfo/systemd-devel
-- 
-- The unit weston.service has entered the 'failed' state with result 'exit-code'.
Nov 08 14:00:22 imx8mp-lpddr4-evk systemd[1]: Failed to start Weston, a Wayland compositor, as a system &amp;gt;
-- Subject: A start job for unit weston.service has failed
-- Defined-By: systemd
-- Support: https://lists.freedesktop.org/mailman/listinfo/systemd-devel
-- 
-- A start job for unit weston.service has finished with a failure.
-- 
-- The job identifier is 118 and the job result is failed.
Nov 08 14:17:34 imx8mp-lpddr4-evk systemd[1]: Starting Weston, a Wayland compositor, as a system service&amp;gt;
-- Subject: A start job for unit weston.service has begun execution
-- Defined-By: systemd
-- Support: https://lists.freedesktop.org/mailman/listinfo/systemd-devel
-- 
-- A start job for unit weston.service has begun execution.
-- 
-- The job identifier is 548.
Nov 08 14:17:34 imx8mp-lpddr4-evk systemd[1]: weston.service: Main process exited, code=exited, status=1&amp;gt;
-- Subject: Unit process exited
-- Defined-By: systemd
-- Support: https://lists.freedesktop.org/mailman/listinfo/systemd-devel
-- 
-- An ExecStart= process belonging to unit weston.service has exited.
-- 
-- The process' exit code is 'exited' and its exit status is 1.
Nov 08 14:17:34 imx8mp-lpddr4-evk systemd[1]: weston.service: Failed with result 'exit-code'.
-- Subject: Unit failed
-- Defined-By: systemd
-- Support: https://lists.freedesktop.org/mailman/listinfo/systemd-devel
-- 
-- The unit weston.service has entered the 'failed' state with result 'exit-code'.
Nov 08 14:17:34 imx8mp-lpddr4-evk systemd[1]: Failed to start Weston, a Wayland compositor, as a system &amp;gt;
-- Subject: A start job for unit weston.service has failed
-- Defined-By: systemd
-- Support: https://lists.freedesktop.org/mailman/listinfo/systemd-devel
-- 
-- A start job for unit weston.service has finished with a failure.
-- 
-- The job identifier is 548 and the job result is failed.
lines 5-60/60 (END)&lt;/LI-CODE&gt;&lt;P&gt;What could be wrong in our position. Thank you in advance!&lt;/P&gt;&lt;P&gt;Best Regards.&lt;/P&gt;</description>
      <pubDate>Mon, 25 Sep 2023 11:20:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Custom-Board-LVDS-Display/m-p/1728885#M213102</guid>
      <dc:creator>Wobaffet</dc:creator>
      <dc:date>2023-09-25T11:20:18Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8MP Custom Board LVDS Display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Custom-Board-LVDS-Display/m-p/1730141#M213220</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206842"&gt;@Wobaffet&lt;/a&gt;,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I hope you are doing well.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Please refer to the example of the device tree given in the below link.&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="https://community.toradex.com/t/imx8mp-lvds-display-lvds-channel-0/17389/5" target="_blank" rel="noopener" data-saferedirecturl="https://www.google.com/url?q=https://community.toradex.com/t/imx8mp-lvds-display-lvds-channel-0/17389/5&amp;amp;source=gmail&amp;amp;ust=1695876954039000&amp;amp;usg=AOvVaw1zmyZJByiq_EMZGAY2Woj-"&gt;https://community.toradex.com/&lt;WBR /&gt;t/imx8mp-lvds-display-lvds-&lt;WBR /&gt;channel-0/17389/5&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://community.toradex.com/t/imx8mp-lvds-display-settings/17401/2" target="_blank" rel="noopener" data-saferedirecturl="https://www.google.com/url?q=https://community.toradex.com/t/imx8mp-lvds-display-settings/17401/2&amp;amp;source=gmail&amp;amp;ust=1695876954039000&amp;amp;usg=AOvVaw0tuvPFx4QXANQEzzIW1qCK"&gt;https://community.toradex.com/&lt;WBR /&gt;t/imx8mp-lvds-display-&lt;WBR /&gt;settings/17401/2&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Please apply those changes and check.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Further If you want to use the lvds dual channel then please follow the below link.&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="https://github.com/varigit/uboot-imx/issues/9" target="_blank" rel="noopener" data-saferedirecturl="https://www.google.com/url?q=https://github.com/varigit/uboot-imx/issues/9&amp;amp;source=gmail&amp;amp;ust=1695876954039000&amp;amp;usg=AOvVaw3TCc4wCOGbuWJ0H_prgLrm"&gt;https://github.com/varigit/&lt;WBR /&gt;uboot-imx/issues/9&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;"[FAILED] Failed to start Weston, a …mpositor, as a system service."&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-&amp;gt;Please follow the below-given link for references and apply those changes and check.&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-failed-to-run-weston-service/m-p/1088208" target="_blank" rel="noopener" data-saferedirecturl="https://www.google.com/url?q=https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-failed-to-run-weston-service/m-p/1088208&amp;amp;source=gmail&amp;amp;ust=1695876954039000&amp;amp;usg=AOvVaw3pj4Hq74eQBiAwVqVhCZsO"&gt;https://community.nxp.com/t5/&lt;WBR /&gt;i-MX-Processors/IMX8MQ-failed-&lt;WBR /&gt;to-run-weston-service/m-p/&lt;WBR /&gt;1088208&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/Unable-to-start-weston-wayland-on-imx8mm/m-p/1658344" target="_blank" rel="noopener" data-saferedirecturl="https://www.google.com/url?q=https://community.nxp.com/t5/i-MX-Processors/Unable-to-start-weston-wayland-on-imx8mm/m-p/1658344&amp;amp;source=gmail&amp;amp;ust=1695876954039000&amp;amp;usg=AOvVaw0UIScUY99nqC_a5rsUYpHS"&gt;https://community.nxp.com/t5/&lt;WBR /&gt;i-MX-Processors/Unable-to-&lt;WBR /&gt;start-weston-wayland-on-&lt;WBR /&gt;imx8mm/m-p/1658344&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;To get a detailed idea on starting the service, Please refer to the below link.&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="https://wayland.pages.freedesktop.org/weston/toc/running-weston.html#running-weston-from-a-systemd-service" target="_blank" rel="noopener" data-saferedirecturl="https://www.google.com/url?q=https://wayland.pages.freedesktop.org/weston/toc/running-weston.html%23running-weston-from-a-systemd-service&amp;amp;source=gmail&amp;amp;ust=1695876954039000&amp;amp;usg=AOvVaw2lczMiLSm--1wmfuFO7crk"&gt;https://wayland.pages.&lt;WBR /&gt;freedesktop.org/weston/toc/&lt;WBR /&gt;running-weston.html#running-&lt;WBR /&gt;weston-from-a-systemd-service&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It will help!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks &amp;amp; Regards,&lt;/SPAN&gt;&lt;BR /&gt;Sanket Parekh&lt;/P&gt;</description>
      <pubDate>Wed, 27 Sep 2023 05:20:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Custom-Board-LVDS-Display/m-p/1730141#M213220</guid>
      <dc:creator>Sanket_Parekh</dc:creator>
      <dc:date>2023-09-27T05:20:38Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8MP Custom Board LVDS Display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Custom-Board-LVDS-Display/m-p/1734902#M213666</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I've configured my DT as follows. But weston does not start. Logs still are like above. What could be the problem here?&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;#include "imx8mp-evk.dts"&lt;/P&gt;&lt;P&gt;/ {&lt;BR /&gt;lvds0_panel {&lt;BR /&gt;compatible = "dlc,dlc1010gig";&lt;BR /&gt;fsl,data-mapping="spwg";&lt;BR /&gt;width-mm=&amp;lt;216&amp;gt;;&lt;BR /&gt;height-mm=&amp;lt;135&amp;gt;;&lt;BR /&gt;pinctrl-names = "default";&lt;BR /&gt;pinctrl-0 = &amp;lt;&amp;amp;pinctrl_lvds&amp;gt;;&lt;BR /&gt;gpio = &amp;lt;&amp;amp;gpio1 10 GPIO_ACTIVE_HIGH&lt;BR /&gt;&amp;amp;gpio1 11 GPIO_ACTIVE_HIGH&amp;gt;;&lt;BR /&gt;panel-timing{&lt;BR /&gt;clock-frequency=&amp;lt;74250000&amp;gt;;&lt;BR /&gt;hactive=&amp;lt;1280&amp;gt;;&lt;BR /&gt;vactive=&amp;lt;800&amp;gt;;&lt;BR /&gt;hfront-porch=&amp;lt;53&amp;gt;;&lt;BR /&gt;hback-porch=&amp;lt;53&amp;gt;;&lt;BR /&gt;hsync-len=&amp;lt;54&amp;gt;;&lt;BR /&gt;vfront-porch=&amp;lt;8&amp;gt;;&lt;BR /&gt;vback-porch=&amp;lt;8&amp;gt;;&lt;BR /&gt;vsync-len=&amp;lt;7&amp;gt;;&lt;BR /&gt;de-active=&amp;lt;1&amp;gt;;&lt;BR /&gt;};&lt;BR /&gt;port {&lt;BR /&gt;panel_lvds_in: endpoint {&lt;BR /&gt;remote-endpoint = &amp;lt;&amp;amp;lvds_out&amp;gt;;&lt;BR /&gt;};&lt;BR /&gt;};&lt;BR /&gt;};&lt;BR /&gt;};&lt;BR /&gt;/delete-node/ &amp;amp;lvds_bridge;&lt;BR /&gt;/delete-node/ &amp;amp;pwm2;&lt;BR /&gt;/delete-node/ &amp;amp;lvds_backlight;&lt;BR /&gt;&amp;amp;ldb {&lt;BR /&gt;status = "okay";&lt;BR /&gt;fsl,dual-channel;&lt;/P&gt;&lt;P&gt;lvds-channel@0 {&lt;BR /&gt;fsl,data-mapping = "spwg";&lt;BR /&gt;/delete-node/ port@1;&lt;/P&gt;&lt;P&gt;port@1 {&lt;BR /&gt;reg = &amp;lt;1&amp;gt;;&lt;/P&gt;&lt;P&gt;lvds_out: endpoint {&lt;BR /&gt;remote-endpoint = &amp;lt;&amp;amp;panel_lvds_in&amp;gt;;&lt;BR /&gt;};&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;};&lt;BR /&gt;};&lt;BR /&gt;&amp;amp;iomuxc{&lt;BR /&gt;pinctrl_lvds:lvdsgrp {&lt;BR /&gt;fsl,pins=&amp;lt;&lt;BR /&gt;MX8MP_IOMUXC_GPIO1_IO10__GPIO1_IO10 0x1c0&lt;BR /&gt;MX8MP_IOMUXC_GPIO1_IO11__GPIO1_IO11 0x1c0&lt;BR /&gt;&amp;gt;;&lt;BR /&gt;};&lt;BR /&gt;};&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;</description>
      <pubDate>Fri, 06 Oct 2023 14:29:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Custom-Board-LVDS-Display/m-p/1734902#M213666</guid>
      <dc:creator>Wobaffet</dc:creator>
      <dc:date>2023-10-06T14:29:54Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8MP Custom Board LVDS Display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Custom-Board-LVDS-Display/m-p/1735692#M213730</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206842"&gt;@Wobaffet&lt;/a&gt;,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I hope you are doing well.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can you follow this link and check by running the command described in the link?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A href="https://github.com/nxp-imx/weston-imx" target="_blank"&gt;https://github.com/nxp-imx/weston-imx&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Please also follow this link in order to start the Weston, Please apply these changes and check.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/How-to-start-Weston-in-fsl-image-validation-imx-image/td-p/866716" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/How-to-start-Weston-in-fsl-image-validation-imx-image/td-p/866716&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;DIV&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/Unable-to-start-weston-wayland-on-imx8mm/m-p/1658344" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/Unable-to-start-weston-wayland-on-imx8mm/m-p/1658344&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;It will be helpful.&lt;BR /&gt;&lt;BR /&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Sanket Parekh&lt;/DIV&gt;</description>
      <pubDate>Mon, 09 Oct 2023 09:43:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Custom-Board-LVDS-Display/m-p/1735692#M213730</guid>
      <dc:creator>Sanket_Parekh</dc:creator>
      <dc:date>2023-10-09T09:43:41Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8MP Custom Board LVDS Display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Custom-Board-LVDS-Display/m-p/1737518#M213868</link>
      <description>&lt;P&gt;I've the following issue that you've provided.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/Unable-to-start-weston-wayland-on-imx8mm/m-p/1658344" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/i-MX-Processors/Unable-to-start-weston-wayland-on-imx8mm/m-p/1658344&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;For this context, solution is solved with the correct configuration on the device tree, can you check our configuration for the lvds panel, we have direct connection to the boards lvds panel just like in the imx8mp-evk but we have configured backlight pwm as a gpio and it is always on, also display enable pin configured as always on, voltages are okay for these pins.&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;&lt;P&gt;best regards,&lt;/P&gt;</description>
      <pubDate>Wed, 11 Oct 2023 13:06:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Custom-Board-LVDS-Display/m-p/1737518#M213868</guid>
      <dc:creator>Wobaffet</dc:creator>
      <dc:date>2023-10-11T13:06:17Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8MP Custom Board LVDS Display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Custom-Board-LVDS-Display/m-p/1738351#M213923</link>
      <description>&lt;P&gt;Our problem still continues, we are stuck at the development. Below is the our weston.ini&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Wobaffet_0-1697093812271.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/244717i495737DC55F7F2BD/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Wobaffet_0-1697093812271.png" alt="Wobaffet_0-1697093812271.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;And here is our log when we try to launch weston with&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;weston -B drm-backend.so&lt;/LI-CODE&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Wobaffet_1-1697093915768.png" style="width: 538px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/244720i21799711B717E1B0/image-dimensions/538x273?v=v2" width="538" height="273" role="button" title="Wobaffet_1-1697093915768.png" alt="Wobaffet_1-1697093915768.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;We've tried to create rules for the weston which at first was not exist. And it can be seen below;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Wobaffet_2-1697094098892.png" style="width: 607px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/244722i30D855BB4286FB0A/image-dimensions/607x41?v=v2" width="607" height="41" role="button" title="Wobaffet_2-1697094098892.png" alt="Wobaffet_2-1697094098892.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Our DTS file for our custom board is attached.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Basically,&amp;nbsp;&amp;nbsp;&lt;STRONG&gt;logind&amp;nbsp;&lt;/STRONG&gt;can not launch. How can we eliminate this problem. Is our rules for the weston okay? Is this launch error related to DT configuration? We don't want to start weston as root. How should we configure? Can you help with these matters?&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;&lt;P&gt;Best Regards.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 12 Oct 2023 07:12:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Custom-Board-LVDS-Display/m-p/1738351#M213923</guid>
      <dc:creator>Wobaffet</dc:creator>
      <dc:date>2023-10-12T07:12:03Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8MP Custom Board LVDS Display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Custom-Board-LVDS-Display/m-p/1738525#M213935</link>
      <description>&lt;P&gt;&lt;SPAN class="im"&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206842"&gt;@Wobaffet&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;I hope you are doing well.&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;I have shared required properties one should include in the device tree below, Please find the same.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Required properties:&lt;/SPAN&gt;&lt;BR /&gt;&lt;STRONG&gt;- compatible: should be "dlc,dlc1010gig"&lt;BR /&gt;- power-supply: See simple-panel.txt&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Optional properties:&lt;/SPAN&gt;&lt;BR /&gt;&lt;STRONG&gt;- enable-gpios: See simple-panel.txt&lt;BR /&gt;- backlight: See simple-panel.txt&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This binding is compatible with the simple-panel binding, which is specified in simple-panel.txt in this directory.&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="https://github.com/OpenChannelSSD/linux/blob/master/Documentation/devicetree/bindings/display/panel/simple-panel.txt" target="_blank" rel="noopener" data-saferedirecturl="https://www.google.com/url?q=https://github.com/OpenChannelSSD/linux/blob/master/Documentation/devicetree/bindings/display/panel/simple-panel.txt&amp;amp;source=gmail&amp;amp;ust=1697190975374000&amp;amp;usg=AOvVaw2e7GSnn5KOXMeNOnipQgtN"&gt;https://github.com/&lt;WBR /&gt;OpenChannelSSD/linux/blob/&lt;WBR /&gt;master/Documentation/&lt;WBR /&gt;devicetree/bindings/display/&lt;WBR /&gt;panel/simple-panel.txt&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This will help you.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks &amp;amp; Regards,&lt;/SPAN&gt;&lt;BR /&gt;Sanket Parekh&lt;/P&gt;</description>
      <pubDate>Thu, 12 Oct 2023 09:57:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Custom-Board-LVDS-Display/m-p/1738525#M213935</guid>
      <dc:creator>Sanket_Parekh</dc:creator>
      <dc:date>2023-10-12T09:57:30Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8MP Custom Board LVDS Display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Custom-Board-LVDS-Display/m-p/1738752#M213965</link>
      <description>Hello @Sanketh_Parekh&lt;BR /&gt;I've tried the solutions you have suggested, but I still can't initialize my display and weston. Should I also patch DTS for u-boot? what does seat does in terms of weston? Thank you in advance!&lt;BR /&gt;Best Regards.&lt;BR /&gt;</description>
      <pubDate>Thu, 12 Oct 2023 15:06:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Custom-Board-LVDS-Display/m-p/1738752#M213965</guid>
      <dc:creator>Wobaffet</dc:creator>
      <dc:date>2023-10-12T15:06:05Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8MP Custom Board LVDS Display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Custom-Board-LVDS-Display/m-p/1740057#M214078</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206842"&gt;@Wobaffet&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;"Should I also patch DTS for u-boot? what does seat does in terms of weston?"&lt;BR /&gt;-&amp;gt;Yes, One should take reference from the below knowledge base link.&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Patch-to-support-uboot-logo-keep-from-uboot-to-kernel-for-NXP/ta-p/1120770" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Patch-to-support-uboot-logo-keep-from-uboot-to-kernel-for-NXP/ta-p/1120770&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;It will be helpful.&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Sanket Parekh&lt;/P&gt;</description>
      <pubDate>Mon, 16 Oct 2023 06:27:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Custom-Board-LVDS-Display/m-p/1740057#M214078</guid>
      <dc:creator>Sanket_Parekh</dc:creator>
      <dc:date>2023-10-16T06:27:54Z</dc:date>
    </item>
  </channel>
</rss>