<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic HDMI Module, iMx6 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-Module-iMx6/m-p/245799#M21373</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.. Can anyone confirm whether a fully initialised HDMI module is all that required initialising to produce a raster on a display?&amp;nbsp; If not, which is the minimum subset of modules (or functions...) that also need initialising before something can be detected on the display?.. nothing displayed in that display of course, just a blank synchronised display..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Jan 2014 09:29:30 GMT</pubDate>
    <dc:creator>johnballance</dc:creator>
    <dc:date>2014-01-21T09:29:30Z</dc:date>
    <item>
      <title>HDMI Module, iMx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-Module-iMx6/m-p/245799#M21373</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.. Can anyone confirm whether a fully initialised HDMI module is all that required initialising to produce a raster on a display?&amp;nbsp; If not, which is the minimum subset of modules (or functions...) that also need initialising before something can be detected on the display?.. nothing displayed in that display of course, just a blank synchronised display..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jan 2014 09:29:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HDMI-Module-iMx6/m-p/245799#M21373</guid>
      <dc:creator>johnballance</dc:creator>
      <dc:date>2014-01-21T09:29:30Z</dc:date>
    </item>
    <item>
      <title>Re: HDMI Module, iMx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-Module-iMx6/m-p/245800#M21374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Basically we can said that three different modules need to be initialized&amp;nbsp; the IOMUX for the pads to be used in the HDMI, the DMA / Memory Controller , and the PLL to provide the clock signal for the module, you can find a HDMI driver in bareboard in the Platform SDK that you can download from the following web page:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.freescale.com/webapp/Download?colCode=i.MX6_PLATFORM_SDK" title="https://www.freescale.com/webapp/Download?colCode=i.MX6_PLATFORM_SDK"&gt;https://www.freescale.com/webapp/Download?colCode=i.MX6_PLATFORM_SDK&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;saludos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Feb 2014 14:51:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HDMI-Module-iMx6/m-p/245800#M21374</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2014-02-04T14:51:01Z</dc:date>
    </item>
  </channel>
</rss>