<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Problem of ethernet connection with some ethernet switch</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1735575#M213722</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;Thank you for your replies.&lt;BR /&gt;I've tried the solution you sent me, meaning modifying the ssh_config file by adding the line&lt;/P&gt;&lt;P&gt;GSSAPIAuthentication yes&lt;/P&gt;&lt;DIV class=""&gt;&lt;P&gt;But unfortunatly it still doesn't work.&amp;nbsp;&lt;BR /&gt;Just to be sure the problem is well understood. The Imx6 is connected to the Ethernet switch by a simple Ethernet cable and it is the only cable connected to the switch. I don't think there is any key verification in this case as it not even recongnized by the switch (no led of presence nor speed). Every other devices I've tested are at least detected by the switch. The Imx6 is detected by smaller switches (5 or 8 ports) but not by this 16 ports switch.&lt;/P&gt;&lt;/DIV&gt;</description>
    <pubDate>Mon, 09 Oct 2023 07:36:38 GMT</pubDate>
    <dc:creator>LéoEaton</dc:creator>
    <dc:date>2023-10-09T07:36:38Z</dc:date>
    <item>
      <title>Problem of ethernet connection with some ethernet switch</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1727866#M213014</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are using an Imx6 DL card on which we run a linux kernel 4.19.288.&lt;/P&gt;&lt;P&gt;We encounter a problem when we try to go through a 16 ports ethernet switch (NetGear JGS516) the connection is not even detected (no leds on) just like nothing was connected. The same card on a 5 or 8 ports switch (GS 105 for example) works perfectly. Those switches are non programmable switches and the datasheets accept the same cables, same protocols and same speed.&lt;/P&gt;&lt;P&gt;The 16 ports switch works perfectly with other systems and devices.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I give you also the settings of my network obtained with the ethtool command on linux:&lt;/P&gt;&lt;P&gt;Settings for eth0:&lt;BR /&gt;Supported ports: [ TP MII ]&lt;BR /&gt;Supported link modes: 10baseT/Half 10baseT/Full&lt;BR /&gt;100baseT/Half 100baseT/Full&lt;BR /&gt;1000baseT/Full&lt;BR /&gt;Supported pause frame use: Symmetric&lt;BR /&gt;Supports auto-negotiation: Yes&lt;BR /&gt;Supported FEC modes: Not reported&lt;BR /&gt;Advertised link modes: 10baseT/Half 10baseT/Full&lt;BR /&gt;100baseT/Half 100baseT/Full&lt;BR /&gt;1000baseT/Full&lt;BR /&gt;Advertised pause frame use: Symmetric&lt;BR /&gt;Advertised auto-negotiation: Yes&lt;BR /&gt;Advertised FEC modes: Not reported&lt;BR /&gt;Link partner advertised link modes: 10baseT/Half 10baseT/Full&lt;BR /&gt;100baseT/Half 100baseT/Full&lt;BR /&gt;Link partner advertised pause frame use: Symmetric Receive-only&lt;BR /&gt;Link partner advertised auto-negotiation: Yes&lt;BR /&gt;Link partner advertised FEC modes: Not reported&lt;BR /&gt;Speed: 100Mb/s&lt;BR /&gt;Duplex: Full&lt;BR /&gt;Port: MII&lt;BR /&gt;PHYAD: 7&lt;BR /&gt;Transceiver: external&lt;BR /&gt;Auto-negotiation: on&lt;BR /&gt;Supports Wake-on: d&lt;BR /&gt;Wake-on: d&lt;BR /&gt;Link detected: yes&lt;/P&gt;&lt;P&gt;Besides the maximum speed is indicated in my kernel device-tree and set to 100Mb/s.&lt;/P&gt;&lt;P&gt;I have read on your forum that I seem not to be the only one concerned by this problem but I couldn't find any solutions.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could it be a power supply problem ? Or is there a setting to change I miss ?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 22 Sep 2023 08:42:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1727866#M213014</guid>
      <dc:creator>LéoEaton</dc:creator>
      <dc:date>2023-09-22T08:42:33Z</dc:date>
    </item>
    <item>
      <title>Re: Problem of ethernet connection with some ethernet switch</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1728851#M213098</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/223355"&gt;@LéoEaton&lt;/a&gt;,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I hope you are doing well.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Please share the dmesg logs to debug the issue with the help of the error logs.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Please make sure to check whether the auto-negotiation is disabled or not.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Please make sure to check the power supply is well-established.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Please check that there are no hardware damages.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks &amp;amp; Regards,&lt;/SPAN&gt;&lt;BR /&gt;Sanket Parekh&lt;/P&gt;</description>
      <pubDate>Mon, 25 Sep 2023 10:25:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1728851#M213098</guid>
      <dc:creator>Sanket_Parekh</dc:creator>
      <dc:date>2023-09-25T10:25:59Z</dc:date>
    </item>
    <item>
      <title>Re: Problem of ethernet connection with some ethernet switch</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1732441#M213429</link>
      <description>&lt;P&gt;I sent you an email with the dmesg logs did you receive it ?&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 02 Oct 2023 07:02:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1732441#M213429</guid>
      <dc:creator>LéoEaton</dc:creator>
      <dc:date>2023-10-02T07:02:37Z</dc:date>
    </item>
    <item>
      <title>Re: Problem of ethernet connection with some ethernet switch</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1733527#M213541</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/223355"&gt;@LéoEaton&lt;/a&gt;,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I hope you are doing well.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;3) As I showed you the output of the ethtool command, I see that auto-negotiation is on, if there is another way to confirm that please let me know&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-&amp;gt;Well one can see the output of the below given command to check the auto-negotiation-related details.&lt;/SPAN&gt;&lt;BR /&gt;&lt;STRONG&gt;ethtool &amp;lt;eth0&amp;gt;&lt;BR /&gt;&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;-&amp;gt;One can identify the&amp;nbsp;below things.&lt;/SPAN&gt;&lt;BR /&gt;&lt;STRONG&gt;Supports auto-negotiation: Yes&lt;BR /&gt;Advertised auto-negotiation: Yes&lt;BR /&gt;&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Can you check by trying the below-given solution below in the link provided?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A href="https://access.redhat.com/solutions/20057" target="_blank"&gt;https://access.redhat.com/solutions/20057&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Meantime I will try to narrow down the issue and will share If I find any.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks &amp;amp; Regards,&lt;/SPAN&gt;&lt;BR /&gt;Sanket Parekh&lt;/P&gt;</description>
      <pubDate>Wed, 04 Oct 2023 06:28:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1733527#M213541</guid>
      <dc:creator>Sanket_Parekh</dc:creator>
      <dc:date>2023-10-04T06:28:44Z</dc:date>
    </item>
    <item>
      <title>Re: Problem of ethernet connection with some ethernet switch</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1735575#M213722</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;Thank you for your replies.&lt;BR /&gt;I've tried the solution you sent me, meaning modifying the ssh_config file by adding the line&lt;/P&gt;&lt;P&gt;GSSAPIAuthentication yes&lt;/P&gt;&lt;DIV class=""&gt;&lt;P&gt;But unfortunatly it still doesn't work.&amp;nbsp;&lt;BR /&gt;Just to be sure the problem is well understood. The Imx6 is connected to the Ethernet switch by a simple Ethernet cable and it is the only cable connected to the switch. I don't think there is any key verification in this case as it not even recongnized by the switch (no led of presence nor speed). Every other devices I've tested are at least detected by the switch. The Imx6 is detected by smaller switches (5 or 8 ports) but not by this 16 ports switch.&lt;/P&gt;&lt;/DIV&gt;</description>
      <pubDate>Mon, 09 Oct 2023 07:36:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1735575#M213722</guid>
      <dc:creator>LéoEaton</dc:creator>
      <dc:date>2023-10-09T07:36:38Z</dc:date>
    </item>
    <item>
      <title>Re: Problem of ethernet connection with some ethernet switch</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1736251#M213759</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/223355"&gt;@LéoEaton&lt;/a&gt;,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I hope you are doing well.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a few queries to ask, Please find them below.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Have you checked the same using the latest BSP as it offers the latest drivers and firmware to work with, I suggest you please check it.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Please also share the device tree file to cross-check.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks &amp;amp; Regards,&lt;/SPAN&gt;&lt;BR /&gt;Sanket Parekh&lt;/P&gt;</description>
      <pubDate>Tue, 10 Oct 2023 05:43:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1736251#M213759</guid>
      <dc:creator>Sanket_Parekh</dc:creator>
      <dc:date>2023-10-10T05:43:57Z</dc:date>
    </item>
    <item>
      <title>Re: Problem of ethernet connection with some ethernet switch</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1737397#M213860</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I sent you an email with device tree files asked.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;</description>
      <pubDate>Wed, 11 Oct 2023 10:20:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1737397#M213860</guid>
      <dc:creator>LéoEaton</dc:creator>
      <dc:date>2023-10-11T10:20:57Z</dc:date>
    </item>
    <item>
      <title>Re: Problem of ethernet connection with some ethernet switch</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1738599#M213949</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/223355"&gt;@LéoEaton&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;Thanks for the device tree, I checked it, and It seems okay.&lt;BR /&gt;Can you share the connection diagram as well as the schematic for both failed and non-failed cases?&lt;BR /&gt;It will help us to narrow down the issue.&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Sanket Parekh&lt;/P&gt;</description>
      <pubDate>Thu, 12 Oct 2023 11:12:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1738599#M213949</guid>
      <dc:creator>Sanket_Parekh</dc:creator>
      <dc:date>2023-10-12T11:12:45Z</dc:date>
    </item>
    <item>
      <title>Re: Problem of ethernet connection with some ethernet switch</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1740025#M214074</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/223355"&gt;@LéoEaton&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;I hope you are doing well.&lt;BR /&gt;&lt;BR /&gt;Any updates from your side?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Sanket Parekh&lt;/P&gt;</description>
      <pubDate>Mon, 16 Oct 2023 05:43:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1740025#M214074</guid>
      <dc:creator>Sanket_Parekh</dc:creator>
      <dc:date>2023-10-16T05:43:25Z</dc:date>
    </item>
    <item>
      <title>Re: Problem of ethernet connection with some ethernet switch</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1743380#M214469</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/223355"&gt;@LéoEaton&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;Any updates from your side?&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Sanket Parekh&lt;/P&gt;</description>
      <pubDate>Fri, 20 Oct 2023 04:38:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1743380#M214469</guid>
      <dc:creator>Sanket_Parekh</dc:creator>
      <dc:date>2023-10-20T04:38:44Z</dc:date>
    </item>
    <item>
      <title>Re: Problem of ethernet connection with some ethernet switch</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1752838#M215306</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I shared with you the schematic as I understood your question by e-mail. Did you receive it ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;</description>
      <pubDate>Mon, 06 Nov 2023 12:53:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1752838#M215306</guid>
      <dc:creator>LéoEaton</dc:creator>
      <dc:date>2023-11-06T12:53:35Z</dc:date>
    </item>
    <item>
      <title>Re: Problem of ethernet connection with some ethernet switch</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1753321#M215348</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/223355"&gt;@LéoEaton&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;Thanks for the device tree, I checked it, and It appears okay.&lt;BR /&gt;Can you share the connection diagram as well as the schematic for both failed and non-failed cases?&lt;/P&gt;
&lt;P&gt;It will help us to narrow down the issue.&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Sanket Parekh&lt;/P&gt;</description>
      <pubDate>Tue, 07 Nov 2023 07:20:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1753321#M215348</guid>
      <dc:creator>Sanket_Parekh</dc:creator>
      <dc:date>2023-11-07T07:20:11Z</dc:date>
    </item>
    <item>
      <title>Re: Problem of ethernet connection with some ethernet switch</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1757631#M215761</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I shared with you the schematic as I understood your question by e-mail. Did you receive it ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;</description>
      <pubDate>Wed, 15 Nov 2023 12:56:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1757631#M215761</guid>
      <dc:creator>LéoEaton</dc:creator>
      <dc:date>2023-11-15T12:56:01Z</dc:date>
    </item>
    <item>
      <title>Re: Problem of ethernet connection with some ethernet switch</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1772360#M217162</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;Hi,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;For the schematic I'm not sure what you expect from me but I will try :&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;The following "schematic" doesn't work, the switch is not detecting the ethernet connection, just like the ethernet cable was not connected to the Imx6 :&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Imx6 ==Ethernet cable==&amp;gt; Switch netgear JGS516 (16 ports)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;The folowing "schematics" does work and the ethernet connection is established :&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Imx6 == Ethernet cable ==&amp;gt; Switch netgear GS105 (5 ports)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Imx6 == Ethernet cable ==&amp;gt; Switch netgear GS105 (5 ports) ==Ethernet cable==&amp;gt; Switch netgear JGS516 (16 ports)&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 11 Dec 2023 14:28:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1772360#M217162</guid>
      <dc:creator>LéoEaton</dc:creator>
      <dc:date>2023-12-11T14:28:14Z</dc:date>
    </item>
    <item>
      <title>Re: Problem of ethernet connection with some ethernet switch</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1773545#M217256</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/223355"&gt;@LéoEaton&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;"For the schematic, I'm not sure what you expect from me but I will try:"&lt;BR /&gt;-&amp;gt;No problem, I am sharing one example of a basic schematic with you for your reference, taking a reference from that you can have an idea regarding the schematic that is being used that may cause the problem, so one can share it with me to debug the issue further,&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/downloads/en/bsdl/IMX8MMINI-BSDL.bsdl" target="_blank" rel="noopener"&gt;https://www.nxp.com/downloads/en/bsdl/IMX8MMINI-BSDL.bsdl&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=8MMINILPD4-EVK-DESIGNFILES" target="_blank" rel="noopener"&gt;https://www.nxp.com/webapp/Download?colCode=8MMINILPD4-EVK-DESIGNFILES&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope this helps!&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Sanket Parekh&lt;/P&gt;</description>
      <pubDate>Wed, 13 Dec 2023 03:54:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-of-ethernet-connection-with-some-ethernet-switch/m-p/1773545#M217256</guid>
      <dc:creator>Sanket_Parekh</dc:creator>
      <dc:date>2023-12-13T03:54:26Z</dc:date>
    </item>
  </channel>
</rss>