<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Device Tree For the Custom Board i.MX8M Plus</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Device-Tree-For-the-Custom-Board-i-MX8M-Plus/m-p/1734591#M213636</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/221689"&gt;@rockerr&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Example of Solidrun would be a simple and good practicem but only for imX8MP : &lt;A href="https://github.com/SolidRun/meta-solidrun-arm-imx8" target="_blank"&gt;https://github.com/SolidRun/meta-solidrun-arm-imx8&lt;/A&gt;&lt;/P&gt;&lt;P&gt;There's also example form ext-Boundary Devices : &lt;A href="https://github.com/boundarydevices/meta-boundary" target="_blank"&gt;https://github.com/boundarydevices/meta-boundary&lt;/A&gt;&lt;/P&gt;&lt;P&gt;The main customized parts are u-Boot in the recipes-bsp/u-boot and Linux kernel in recipes-kernel/linux/.&lt;/P&gt;&lt;P&gt;The patches for your custom board are generated from the commits on top of NXP's official u-Boot and Linux. They will be included in .bbaapend files.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Khang&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 06 Oct 2023 05:51:16 GMT</pubDate>
    <dc:creator>khang_letruong</dc:creator>
    <dc:date>2023-10-06T05:51:16Z</dc:date>
    <item>
      <title>Device Tree For the Custom Board i.MX8M Plus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Device-Tree-For-the-Custom-Board-i-MX8M-Plus/m-p/1541977#M196693</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;What is the best efficient way to edit the device tree for our custom board with i.MX8MP MPU? Some components of our board will be same with the evaluation board so how should we proceed? Can you share your experiences?&lt;/P&gt;&lt;P&gt;Does Config Tools for i.MX create only pin_mux.dts file?&lt;/P&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;</description>
      <pubDate>Fri, 21 Oct 2022 12:48:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Device-Tree-For-the-Custom-Board-i-MX8M-Plus/m-p/1541977#M196693</guid>
      <dc:creator>Wobaffet</dc:creator>
      <dc:date>2022-10-21T12:48:52Z</dc:date>
    </item>
    <item>
      <title>Re: Device Tree For the Custom Board i.MX8M Plus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Device-Tree-For-the-Custom-Board-i-MX8M-Plus/m-p/1542196#M196710</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Once you have a build running on your custom board you can try the following.&lt;/P&gt;&lt;P&gt;First locate your correct device tree file(s), sometimes with Yocto and certain builds it may not be the files you think.. Then as a quick test comment out some obviously unused items and rebuild. Check you boot log to make sure the devices have disappeared or are no longer probed. You can trim down the device tree a fair bit if needed. Once you have worked out what can go, create some device tree patch file(s) and add these to your sources/meta-yours/recipes-kernel etc to make the changes permanent. This is fine if you want to work with modified EVK builds. You can remove unwanted drivers as well using bitbake linux-imx -c menuconfig thus having a similar effect as removing them from your device tree.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Just be aware if you tweak the actual device tree file(s) up in&amp;nbsp;/arch/arm64/boot/dts/freescale somewhere then do a kernel clean and build you will loose your changes. Do your changes after a kernel clean if you need to do one, creating patch files is a better practice so perhaps worth looking into sooner rather than later.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope it helps, it's a big learning curve.&lt;/P&gt;</description>
      <pubDate>Fri, 21 Oct 2022 23:28:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Device-Tree-For-the-Custom-Board-i-MX8M-Plus/m-p/1542196#M196710</guid>
      <dc:creator>edwardtyrrell</dc:creator>
      <dc:date>2022-10-21T23:28:46Z</dc:date>
    </item>
    <item>
      <title>Re: Device Tree For the Custom Board i.MX8M Plus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Device-Tree-For-the-Custom-Board-i-MX8M-Plus/m-p/1542271#M196726</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206842"&gt;@Wobaffet&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;There more than 1 way to do that. Either you can add your new device-tree files into the kernel repository (1) that is cloned from &lt;A href="https://source.codeaurora.org/external/imx/linux-imx/" target="_blank" rel="noopener"&gt;https://source.codeaurora.org/external/imx/linux-imx/&lt;/A&gt; or you can add them as patch(es) by the Yocto recipes (2).&lt;/P&gt;&lt;P&gt;Example of (1) :&lt;/P&gt;&lt;P&gt;a. Toradex with their verdin boards :&amp;nbsp;&lt;A href="https://git.toradex.com/cgit/linux-toradex.git/log/?h=toradex_5.4-2.3.x-imx" target="_blank" rel="noopener"&gt;https://git.toradex.com/cgit/linux-toradex.git/log/?h=toradex_5.4-2.3.x-imx&lt;/A&gt;&lt;/P&gt;&lt;P&gt;b. Phytec with their phycore boards: &lt;A href="https://github.com/phytec/linux-phytec-imx/tree/v5.4.70_2.3.2-phy" target="_blank" rel="noopener"&gt;https://github.com/phytec/linux-phytec-imx/tree/v5.4.70_2.3.2-phy&lt;/A&gt;&lt;/P&gt;&lt;P&gt;c. Variscite with their var-dart boards: &lt;A href="https://github.com/varigit/linux-imx/tree/5.4-2.3.x-imx_var01" target="_blank" rel="noopener"&gt;https://github.com/varigit/linux-imx/tree/5.4-2.3.x-imx_var01&lt;/A&gt;&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;Example of (2): SolidRun with their recipes to add their &lt;SPAN class=""&gt;Hummingboard&lt;/SPAN&gt; : &lt;A href="https://github.com/SolidRun/meta-solidrun-arm-imx8/blob/hardknott-imx8mp/recipes-kernel/linux/linux-imx/0010-ARM64-dts-imx8mp-Add-SolidRun-iMX8MP-SOM-based-platf.patch" target="_blank" rel="noopener"&gt;https://github.com/SolidRun/meta-solidrun-arm-imx8/blob/hardknott-imx8mp/recipes-kernel/linux/linux-imx/0010-ARM64-dts-imx8mp-Add-SolidRun-iMX8MP-SOM-based-platf.patch&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Also, my best practice would be including the &lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mp-evk.dts?h=imx_5.4.70_2.3.0" target="_self"&gt;imx8mp-evk.dts&lt;/A&gt; into the custom .dts and do the tweaking (add new nodes, removing unused nodes, overriding nodes with new properties, ...). Or you can completely add a new custom .dts by only including &lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mp.dtsi?h=imx_5.4.70_2.3.0" target="_self"&gt;imx8mp.dtsi&lt;/A&gt; which is crucial for any iMX8MP based board.&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;K.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 23 Oct 2022 05:04:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Device-Tree-For-the-Custom-Board-i-MX8M-Plus/m-p/1542271#M196726</guid>
      <dc:creator>khang_letruong</dc:creator>
      <dc:date>2022-10-23T05:04:42Z</dc:date>
    </item>
    <item>
      <title>Re: Device Tree For the Custom Board i.MX8M Plus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Device-Tree-For-the-Custom-Board-i-MX8M-Plus/m-p/1543226#M196808</link>
      <description>I have general knowledge of the concept but I am kind of lost on the job. For now, custom board will be again similar to evk so I should be fine patching it without creating a new machine? I've built a yocto image (imx-image-core) for the imx8mp evk. Eventually there are some dtb files at the /tmp/deploy/images/imx8mpevk for it. In this case If I take a look at the respective dts files and edit them w.r.t my use case and peripherals would that work? Editing will be done in my own layer with patching respective files.</description>
      <pubDate>Tue, 25 Oct 2022 08:12:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Device-Tree-For-the-Custom-Board-i-MX8M-Plus/m-p/1543226#M196808</guid>
      <dc:creator>Wobaffet</dc:creator>
      <dc:date>2022-10-25T08:12:43Z</dc:date>
    </item>
    <item>
      <title>Re: Device Tree For the Custom Board i.MX8M Plus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Device-Tree-For-the-Custom-Board-i-MX8M-Plus/m-p/1543344#M196821</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;EM&gt;For now, custom board will be again similar to evk so I should be fine patching it without creating a new machine?&lt;/EM&gt; Yes. Designers/developers often base a product on an EVK initially to hit the ground running, that takes care of the basic hardware and prevents all sorts of issues. It's not unusual&amp;nbsp;to develop on an EVK until you get the proper hardware in your hands.. So, if you have a custom board that is based on an EVK then you can boot and run a Yocto image even if your missing peripherals or have added more.&amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;EM&gt;Eventually there are some dtb files at the /tmp/deploy/images/imx8mpevk for it. In this case If I take a look at the respective dts files and edit them w.r.t my use case and peripherals would that work?&lt;/EM&gt; The dtb files you mentioned are objects that are built and are not editable, you need to edit/replace these at their source in a location like&amp;nbsp;/arch/arm64/boot/dts/freescale/imx8mm-evk.dtsi as you said.. Therefore editing the source files, adding and deleting peripherals&amp;nbsp;would work. Remember to enable new drivers in your menu config.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;As khang_letruong said, you can replace the dtsi file outright or do a custom file and include it.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 25 Oct 2022 10:09:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Device-Tree-For-the-Custom-Board-i-MX8M-Plus/m-p/1543344#M196821</guid>
      <dc:creator>edwardtyrrell</dc:creator>
      <dc:date>2022-10-25T10:09:04Z</dc:date>
    </item>
    <item>
      <title>Re: Device Tree For the Custom Board i.MX8M Plus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Device-Tree-For-the-Custom-Board-i-MX8M-Plus/m-p/1734151#M213598</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/147542"&gt;@khang_letruong&lt;/a&gt;&lt;/P&gt;&lt;P&gt;I'm working with iMX93 right now, my struggles are with this very problem where I have no idea how to enable my custom kernel DT in the Yocto configuration. Making patches to the default DT &lt;EM&gt;imx93-11x11-evk.dts&lt;/EM&gt; is optional, however rather painfull in the long run. I've taken a look at the toradex repository, they added a lot of their own configuration, so it wasn't clear to me how what are the best practices.&lt;/P&gt;&lt;P&gt;I cannot find any information in the official NXP guides on how to do it, have you maybe succeeded in that?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 05 Oct 2023 09:44:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Device-Tree-For-the-Custom-Board-i-MX8M-Plus/m-p/1734151#M213598</guid>
      <dc:creator>rockerr</dc:creator>
      <dc:date>2023-10-05T09:44:43Z</dc:date>
    </item>
    <item>
      <title>Re: Device Tree For the Custom Board i.MX8M Plus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Device-Tree-For-the-Custom-Board-i-MX8M-Plus/m-p/1734591#M213636</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/221689"&gt;@rockerr&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Example of Solidrun would be a simple and good practicem but only for imX8MP : &lt;A href="https://github.com/SolidRun/meta-solidrun-arm-imx8" target="_blank"&gt;https://github.com/SolidRun/meta-solidrun-arm-imx8&lt;/A&gt;&lt;/P&gt;&lt;P&gt;There's also example form ext-Boundary Devices : &lt;A href="https://github.com/boundarydevices/meta-boundary" target="_blank"&gt;https://github.com/boundarydevices/meta-boundary&lt;/A&gt;&lt;/P&gt;&lt;P&gt;The main customized parts are u-Boot in the recipes-bsp/u-boot and Linux kernel in recipes-kernel/linux/.&lt;/P&gt;&lt;P&gt;The patches for your custom board are generated from the commits on top of NXP's official u-Boot and Linux. They will be included in .bbaapend files.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Khang&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 06 Oct 2023 05:51:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Device-Tree-For-the-Custom-Board-i-MX8M-Plus/m-p/1734591#M213636</guid>
      <dc:creator>khang_letruong</dc:creator>
      <dc:date>2023-10-06T05:51:16Z</dc:date>
    </item>
  </channel>
</rss>