<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Pin Multiplexing in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Pin-Multiplexing/m-p/1734162#M213600</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/223880"&gt;@abhi_kr&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Since the tool allows the pin muxing, it won't affect each other's functionality.&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Ritesh M Patel&lt;/P&gt;</description>
    <pubDate>Thu, 05 Oct 2023 09:59:18 GMT</pubDate>
    <dc:creator>riteshmpatel</dc:creator>
    <dc:date>2023-10-05T09:59:18Z</dc:date>
    <item>
      <title>Pin Multiplexing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Pin-Multiplexing/m-p/1733681#M213559</link>
      <description>&lt;P&gt;I am using &lt;SPAN&gt;&lt;SPAN class=""&gt;MCIMX7D5EVM10SD for a project and want to utilize the EIM interface to communicate to FPGA,Also I want to use the two Ethernet port available.I am planning to use the First 8 AD lines from the EIM so that i can allocate the other pins for the two Ethernet. Is this possible.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 04 Oct 2023 10:23:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Pin-Multiplexing/m-p/1733681#M213559</guid>
      <dc:creator>abhi_kr</dc:creator>
      <dc:date>2023-10-04T10:23:42Z</dc:date>
    </item>
    <item>
      <title>Re: Pin Multiplexing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Pin-Multiplexing/m-p/1733706#M213563</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/223880"&gt;@abhi_kr&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P data-unlink="true"&gt;One can download the&amp;nbsp;&lt;A href="https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX" target="_self"&gt;Config Tools for i.MX Applications Processors&lt;/A&gt;&amp;nbsp;and perform the pin muxing and check if it can suffice one's requirement of the interfaces desired to be used.&lt;/P&gt;
&lt;P data-unlink="true"&gt;I hope it helps!&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Ritesh M Patel&lt;/P&gt;</description>
      <pubDate>Wed, 04 Oct 2023 11:49:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Pin-Multiplexing/m-p/1733706#M213563</guid>
      <dc:creator>riteshmpatel</dc:creator>
      <dc:date>2023-10-04T11:49:43Z</dc:date>
    </item>
    <item>
      <title>Re: Pin Multiplexing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Pin-Multiplexing/m-p/1734047#M213584</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201596"&gt;@riteshmpatel&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;I am using the Config tool only for the pin multiplexing .My concern is for example if we are having 20 pins for the EIM and i am using only 10 and the rest i had assigned for the two Ethernet related pins by the help of the tool,tool is supporting this.My question is if i am driving the Ethernet pins which was taken from the EIM pins will it affect the EIM operation,whether the opposite also will happen?&lt;/P&gt;</description>
      <pubDate>Thu, 05 Oct 2023 06:28:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Pin-Multiplexing/m-p/1734047#M213584</guid>
      <dc:creator>abhi_kr</dc:creator>
      <dc:date>2023-10-05T06:28:01Z</dc:date>
    </item>
    <item>
      <title>Re: Pin Multiplexing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Pin-Multiplexing/m-p/1734162#M213600</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/223880"&gt;@abhi_kr&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Since the tool allows the pin muxing, it won't affect each other's functionality.&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Ritesh M Patel&lt;/P&gt;</description>
      <pubDate>Thu, 05 Oct 2023 09:59:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Pin-Multiplexing/m-p/1734162#M213600</guid>
      <dc:creator>riteshmpatel</dc:creator>
      <dc:date>2023-10-05T09:59:18Z</dc:date>
    </item>
  </channel>
</rss>