<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Steps to add python packages into yocto build in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Steps-to-add-python-packages-into-yocto-build/m-p/1732906#M213483</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201299"&gt;@Dhruvit&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;I will check the recipes. Thanks for the information.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Sureshkumar R&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 03 Oct 2023 06:52:41 GMT</pubDate>
    <dc:creator>krsuresh</dc:creator>
    <dc:date>2023-10-03T06:52:41Z</dc:date>
    <item>
      <title>Steps to add python packages into yocto build</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Steps-to-add-python-packages-into-yocto-build/m-p/1731189#M213339</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;We would appreciate it if you could tell me how to build a core-minimal-image with following python packages,&lt;BR /&gt;&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;tflite-support&lt;BR /&gt;tensorstore&lt;BR /&gt;tflite-support-nightly&lt;BR /&gt;tensorflow-addons&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Sureshkumar R&lt;/P&gt;</description>
      <pubDate>Thu, 28 Sep 2023 09:31:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Steps-to-add-python-packages-into-yocto-build/m-p/1731189#M213339</guid>
      <dc:creator>krsuresh</dc:creator>
      <dc:date>2023-09-28T09:31:56Z</dc:date>
    </item>
    <item>
      <title>Re: Steps to add python packages into yocto build</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Steps-to-add-python-packages-into-yocto-build/m-p/1732886#M213478</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210184"&gt;@krsuresh&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;To add the above packes in the yocto build, one needs to have a bitbake recipe for the same.&lt;/P&gt;
&lt;P&gt;NXP Yocto BSP doesn't contain recipes for the same.&lt;/P&gt;
&lt;P&gt;Customer needs to create their own bitbake recipes to add above packages.&lt;/P&gt;
&lt;P&gt;One can refer to various recipes at&amp;nbsp;&lt;A href="https://github.com/nxp-imx/meta-imx/tree/mickledore-6.1.22-2.0.0/meta-ml/recipes-libraries/tensorflow-lite" target="_self"&gt;meta-imx/meta-ml/recipes-libraries&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://github.com/nxp-imx/meta-imx/tree/mickledore-6.1.22-2.0.0/meta-ml/recipes-libraries/tensorflow-lite" target="_self"&gt;/tensorflow-lite/&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Dhruvit Vasavada&lt;/P&gt;</description>
      <pubDate>Tue, 03 Oct 2023 06:22:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Steps-to-add-python-packages-into-yocto-build/m-p/1732886#M213478</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2023-10-03T06:22:59Z</dc:date>
    </item>
    <item>
      <title>Re: Steps to add python packages into yocto build</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Steps-to-add-python-packages-into-yocto-build/m-p/1732906#M213483</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201299"&gt;@Dhruvit&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;I will check the recipes. Thanks for the information.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Sureshkumar R&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Oct 2023 06:52:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Steps-to-add-python-packages-into-yocto-build/m-p/1732906#M213483</guid>
      <dc:creator>krsuresh</dc:creator>
      <dc:date>2023-10-03T06:52:41Z</dc:date>
    </item>
  </channel>
</rss>