<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: No bootable slots found</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/No-bootable-slots-found/m-p/1732870#M213477</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202155"&gt;@Sanket_Parekh&lt;/a&gt;I could find sdma-imx6q.bin and sdma-imx7d.bin files in /vendor/nxp/linux_firmware-imx/firmware/sdma path&lt;/P&gt;&lt;P&gt;After build is successful , i could find sdma-imx7d.bin file in /out/target/product/evk_8mm/vendor/firmware/imx/sdma path , But we are using imx8mm , this is the external firmware file for this processor ?&lt;/P&gt;</description>
    <pubDate>Tue, 03 Oct 2023 05:52:58 GMT</pubDate>
    <dc:creator>ramyashree1</dc:creator>
    <dc:date>2023-10-03T05:52:58Z</dc:date>
    <item>
      <title>No bootable slots found</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-bootable-slots-found/m-p/1730988#M213320</link>
      <description>&lt;P&gt;flash target is MMC:2&lt;BR /&gt;Net: No ethernet found.&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;Normal Boot&lt;BR /&gt;Autoboot disabled.&lt;BR /&gt;Hit any key to stop autoboot: 0 fsl_read_from_partition_multi: no boot partition&lt;BR /&gt;idx 0, ptn 0 name='gpt' start=0 len=2048&lt;BR /&gt;idx 1, ptn 0 name='' start=0 len=0&lt;BR /&gt;idx 2, ptn 0 name='mcu_os' start=10240 len=512&lt;BR /&gt;idx 3, ptn 0 name='all' start=0 len=244285440&lt;BR /&gt;idx 4, ptn 0 name='bootloader0' start=66 len=8192&lt;BR /&gt;idx 5, ptn 1 name='dtbo_a' start=16384 len=8192&lt;BR /&gt;idx 6, ptn 2 name='dtbo_b' start=24576 len=8192&lt;BR /&gt;idx 7, ptn 3 name='boot_a' start=32768 len=131072&lt;BR /&gt;idx 8, ptn 4 name='boot_b' start=163840 len=131072&lt;BR /&gt;idx 9, ptn 5 name='misc' start=294912 len=8192&lt;BR /&gt;idx 10, ptn 6 name='metadata' start=303104 len=4096&lt;BR /&gt;idx 11, ptn 7 name='presistdata' start=307200 len=2048&lt;BR /&gt;idx 12, ptn 8 name='super' start=311296 len=14680064&lt;BR /&gt;idx 13, ptn 9 name='userdata' start=14991360 len=12255232&lt;BR /&gt;idx 14, ptn 10 name='fbmisc' start=27246592 len=2048&lt;BR /&gt;idx 15, ptn 11 name='vbmeta_a' start=27250688 len=2048&lt;BR /&gt;idx 16, ptn 12 name='vbmeta_b' start=27254784 len=2048&lt;BR /&gt;boot load error!&lt;BR /&gt;No bootable slots found.&lt;BR /&gt;verify FAIL, state: LOCK&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;working on imx8mm board, flash is successful , but device is not booting , it is strucked in boot logo , after debugging got this failed error , please help me out what can be done&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;</description>
      <pubDate>Thu, 28 Sep 2023 05:24:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-bootable-slots-found/m-p/1730988#M213320</guid>
      <dc:creator>ramyashree1</dc:creator>
      <dc:date>2023-09-28T05:24:40Z</dc:date>
    </item>
    <item>
      <title>Re: No bootable slots found</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-bootable-slots-found/m-p/1732433#M213428</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/223664"&gt;@ramyashree1&lt;/a&gt;,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I hope you are doing well.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for sharing the logs, I checked it.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can you please also share the sequence of commands you run to debug the issue?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks &amp;amp; Regards,&lt;/SPAN&gt;&lt;BR /&gt;Sanket Parekh&lt;/P&gt;</description>
      <pubDate>Mon, 02 Oct 2023 06:38:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-bootable-slots-found/m-p/1732433#M213428</guid>
      <dc:creator>Sanket_Parekh</dc:creator>
      <dc:date>2023-10-02T06:38:21Z</dc:date>
    </item>
    <item>
      <title>Re: No bootable slots found</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-bootable-slots-found/m-p/1732865#M213476</link>
      <description>&lt;P&gt;Hi Sanket,&lt;/P&gt;&lt;P&gt;I'm using JTAG to debug&lt;/P&gt;&lt;P&gt;first i entered into sudo&lt;/P&gt;&lt;P&gt;gave the command "minicom -s -D /dev/ttyUSB0&lt;/P&gt;&lt;P&gt;enabled software flow and exit&lt;/P&gt;&lt;P&gt;ran the command "boot"&lt;/P&gt;&lt;P&gt;after this , while starting kernel , i'm getting this error&lt;/P&gt;</description>
      <pubDate>Tue, 03 Oct 2023 05:43:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-bootable-slots-found/m-p/1732865#M213476</guid>
      <dc:creator>ramyashree1</dc:creator>
      <dc:date>2023-10-03T05:43:48Z</dc:date>
    </item>
    <item>
      <title>Re: No bootable slots found</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-bootable-slots-found/m-p/1732870#M213477</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202155"&gt;@Sanket_Parekh&lt;/a&gt;I could find sdma-imx6q.bin and sdma-imx7d.bin files in /vendor/nxp/linux_firmware-imx/firmware/sdma path&lt;/P&gt;&lt;P&gt;After build is successful , i could find sdma-imx7d.bin file in /out/target/product/evk_8mm/vendor/firmware/imx/sdma path , But we are using imx8mm , this is the external firmware file for this processor ?&lt;/P&gt;</description>
      <pubDate>Tue, 03 Oct 2023 05:52:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-bootable-slots-found/m-p/1732870#M213477</guid>
      <dc:creator>ramyashree1</dc:creator>
      <dc:date>2023-10-03T05:52:58Z</dc:date>
    </item>
    <item>
      <title>Re: No bootable slots found</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-bootable-slots-found/m-p/1732889#M213479</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202155"&gt;@Sanket_Parekh&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now im getting this issue , Please check and let me know&lt;/P&gt;</description>
      <pubDate>Tue, 03 Oct 2023 06:23:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-bootable-slots-found/m-p/1732889#M213479</guid>
      <dc:creator>ramyashree1</dc:creator>
      <dc:date>2023-10-03T06:23:25Z</dc:date>
    </item>
    <item>
      <title>Re: No bootable slots found</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-bootable-slots-found/m-p/1733010#M213497</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/223664"&gt;@ramyashree1&lt;/a&gt;,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I hope you are doing well.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;"this is the external firmware file for this processor ?"&lt;BR /&gt;-&amp;gt;Yes, In the Linux source code there are several firmware files available for the various boards, Even one can find several dt files as well, One can select as per their requirements based on the board one is using one can choose it for the main purpose.&lt;/P&gt;
&lt;P&gt;Please refer to the IMX release notes for more details.&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/release-note/IMX_LINUX_RELEASE_NOTES.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/release-note/IMX_LINUX_RELEASE_NOTES.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I hope it answers your query.&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Sanket Parekh&lt;/P&gt;</description>
      <pubDate>Tue, 03 Oct 2023 09:09:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-bootable-slots-found/m-p/1733010#M213497</guid>
      <dc:creator>Sanket_Parekh</dc:creator>
      <dc:date>2023-10-03T09:09:58Z</dc:date>
    </item>
  </channel>
</rss>