<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックSensor boards with MIMXRT685-EVK</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Sensor-boards-with-MIMXRT685-EVK/m-p/1732737#M213465</link>
    <description>&lt;P&gt;I am trying to use the Makalu6 Evaluation application software with a P3T1085UK plugged into&amp;nbsp; a&amp;nbsp;MIMXRT685-EVK. Documentation for the P3T1085UK shows the module being recognized in the software. When I run the application nothing is recognized. I have tried connecting and disconnecting.&lt;/P&gt;&lt;P&gt;I have the module plugged in and the I3C cable plugged in.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 02 Oct 2023 19:00:31 GMT</pubDate>
    <dc:creator>jbn60</dc:creator>
    <dc:date>2023-10-02T19:00:31Z</dc:date>
    <item>
      <title>Sensor boards with MIMXRT685-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Sensor-boards-with-MIMXRT685-EVK/m-p/1732737#M213465</link>
      <description>&lt;P&gt;I am trying to use the Makalu6 Evaluation application software with a P3T1085UK plugged into&amp;nbsp; a&amp;nbsp;MIMXRT685-EVK. Documentation for the P3T1085UK shows the module being recognized in the software. When I run the application nothing is recognized. I have tried connecting and disconnecting.&lt;/P&gt;&lt;P&gt;I have the module plugged in and the I3C cable plugged in.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 02 Oct 2023 19:00:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Sensor-boards-with-MIMXRT685-EVK/m-p/1732737#M213465</guid>
      <dc:creator>jbn60</dc:creator>
      <dc:date>2023-10-02T19:00:31Z</dc:date>
    </item>
    <item>
      <title>Re: Sensor boards with MIMXRT685-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Sensor-boards-with-MIMXRT685-EVK/m-p/1735288#M213705</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/223799"&gt;@jbn60&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; Thanks for your interest in the NXP MIMXRT product, I would like to provide service for you.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; I am the RT engineer, so mainly familiar with the RT situation.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; Your side, also use the&amp;nbsp;&lt;SPAN&gt;P3T1085UK sensor, you mentioned it is working, but when connect with the RT685, not working.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; Do you do the correct configuration? Do you use ENTDAA or static address?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; You also can refer to this application note for the I3C and the code to do the communication, whether that works or not? an12796, or the SDK code.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;\SDK_2_14_0_MIMXRT685-AUD-EVK\boards\mimxrt685audevk\driver_examples\i3c&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; If still have issues, you can use the logic analyzer to check the I3C bus, where it is stopping.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;Also check the data send to the sensor is correct or not.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Kerry&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 08 Oct 2023 07:50:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Sensor-boards-with-MIMXRT685-EVK/m-p/1735288#M213705</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2023-10-08T07:50:05Z</dc:date>
    </item>
    <item>
      <title>Re: Sensor boards with MIMXRT685-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Sensor-boards-with-MIMXRT685-EVK/m-p/1764340#M216427</link>
      <description>&lt;P&gt;Following the instructions for the P3T1085 eval it shows after running the software the sensor board being detected by the Makalu6 application. See Instructions.png attachment. When I run the software the sensor board is never detected even after clicking the connect button. I have the I2C/I3C wires connected between the sensor board&amp;nbsp; into the and the MIMXRT685&amp;nbsp; and the sensor board plugged into the 685 eval board (see I3C_SensorSoftware.png). I am not sure what to do to get the sensor to work with the software&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 27 Nov 2023 23:34:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Sensor-boards-with-MIMXRT685-EVK/m-p/1764340#M216427</guid>
      <dc:creator>jbn60</dc:creator>
      <dc:date>2023-11-27T23:34:54Z</dc:date>
    </item>
  </channel>
</rss>