<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Confused about eFlexPWM disable in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Confused-about-eFlexPWM-disable/m-p/1732328#M213416</link>
    <description>&lt;P&gt;Thanks for you reply! And I want to confirm that is there other way to make it output low level when disable the pwm module. Can I use fault pins or force out function or use other low frequency pwm to have a trigger? I feel confused! Thank you!&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Iris&lt;/P&gt;</description>
    <pubDate>Sun, 01 Oct 2023 04:25:01 GMT</pubDate>
    <dc:creator>ahhhhhhhhhhh</dc:creator>
    <dc:date>2023-10-01T04:25:01Z</dc:date>
    <item>
      <title>Confused about eFlexPWM disable</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Confused-about-eFlexPWM-disable/m-p/1725831#M212814</link>
      <description>&lt;P&gt;Hi Community,&lt;/P&gt;&lt;P&gt;I have successfully generated a pair of complementary PWM using PWM1 submodule 0, but I cannot disable PWM output&amp;nbsp; through setting the OUTEN register. It always high after I setting the OUTEN for PWMA, even I setting the GPIO to internal pull-down. This submodule use GPIO_SD_B0_00 and GPIO_SD_B0_01 to output PWM, and for GPIO_SD_B0_00, it has an external pull-up resistor. And I also try to use submodule2(GPIO_SD_B0_04&amp;amp;05), it works, but these pins connect to TP27 and 28, it not easy to connect to other device, so I want to know how to disable submodule0 successfully.&lt;/P&gt;&lt;P&gt;Btw, I'm using RT1064 EVK.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ahhhhhhhhhhh_0-1695175845361.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/241693i4344F805D81115F9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ahhhhhhhhhhh_0-1695175845361.png" alt="ahhhhhhhhhhh_0-1695175845361.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ahhhhhhhhhhh_0-1695175845361.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 20 Sep 2023 02:21:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Confused-about-eFlexPWM-disable/m-p/1725831#M212814</guid>
      <dc:creator>ahhhhhhhhhhh</dc:creator>
      <dc:date>2023-09-20T02:21:38Z</dc:date>
    </item>
    <item>
      <title>Re: Confused about eFlexPWM disable</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Confused-about-eFlexPWM-disable/m-p/1729974#M213201</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;You are correct, the way to disable the submodules is with &lt;EM&gt;Output Enable Register (OUTEN)&lt;/EM&gt;, what you need to do is remove the pull-up resistors.&lt;/P&gt;
&lt;P&gt;Hope it helps you.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Wed, 27 Sep 2023 00:07:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Confused-about-eFlexPWM-disable/m-p/1729974#M213201</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2023-09-27T00:07:35Z</dc:date>
    </item>
    <item>
      <title>Re: Confused about eFlexPWM disable</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Confused-about-eFlexPWM-disable/m-p/1732328#M213416</link>
      <description>&lt;P&gt;Thanks for you reply! And I want to confirm that is there other way to make it output low level when disable the pwm module. Can I use fault pins or force out function or use other low frequency pwm to have a trigger? I feel confused! Thank you!&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Iris&lt;/P&gt;</description>
      <pubDate>Sun, 01 Oct 2023 04:25:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Confused-about-eFlexPWM-disable/m-p/1732328#M213416</guid>
      <dc:creator>ahhhhhhhhhhh</dc:creator>
      <dc:date>2023-10-01T04:25:01Z</dc:date>
    </item>
  </channel>
</rss>