<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Install Bitbake fsl-image-gui in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Install-Bitbake-fsl-image-gui/m-p/1731007#M213321</link>
    <description>&lt;P&gt;ERROR: fsl-image-gui-1.0-r0 do_rootfs: Unable to install packages. Command '/home/veeranagouda/iwg15-release-bsp/build_iwg15/tmp/sysroots/x86_64-linux/usr/bin/apt-get install --force-yes --allow-unauthenticated packagegroup-core-ssh-dropbear qt5nmapcarousedemo psplash packagegroup-core-tools-profile apt packagegroup-qt5-demos cinematicexperience packagegroup-fsl-tools-audio qtsmarthome packagegroup-fsl-tools-benchmark qtbase-examples quitindicators qt5nmapper quitbattery packagegroup-core-boot packagegroup-core-full-cmdline packagegroup-core-tools-testapps packagegroup-core-x11-base packagegroup-fsl-gstreamer1.0-full packagegroup-core-nfs-server qtdeclarative-examples iwtest qt3d-examples packagegroup-fsl-gstreamer1.0 packagegroup-fsl-tools-gpu packagegroup-fsl-tools-testapps run-postinsts packagegroup-fsl-tools-gpu-external packagegroup-core-tools-debug qt5ledscreen qt5everywheredemo packagegroup-qt5-toolchain-target qt5-demo-extrafiles packagegroup-tools-bluetooth packagegroup-base-extended packagegroup-core-x11-sato' returned 100:&lt;BR /&gt;Reading package lists...&lt;BR /&gt;Building dependency tree...&lt;BR /&gt;Reading state information...&lt;BR /&gt;Some packages could not be installed. This may mean that you have&lt;BR /&gt;requested an impossible situation or if you are using the unstable&lt;BR /&gt;distribution that some required packages have not yet been created&lt;BR /&gt;or been moved out of Incoming.&lt;BR /&gt;The following information may help to resolve the situation:&lt;/P&gt;&lt;P&gt;The following packages have unmet dependencies:&lt;BR /&gt;packagegroup-core-x11-base : Depends: packagegroup-core-x11-utils but it is not going to be installed&lt;BR /&gt;E: Unable to correct problems, you have held broken packages.&lt;/P&gt;&lt;P&gt;ERROR: fsl-image-gui-1.0-r0 do_rootfs: Function failed: do_rootfs&lt;BR /&gt;ERROR: Logfile of failure stored in: /home/veeranagouda/iwg15-release-bsp/build_iwg15/tmp/work/imx6qdl_iwg15_sm-poky-linux-gnueabi/fsl-image-gui/1.0-r0/temp/log.do_rootfs.29574&lt;BR /&gt;ERROR: Task 9 (/home/veeranagouda/iwg15-release-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-fsl/images/fsl-image-gui.bb, do_rootfs) failed with exit code '1'&lt;BR /&gt;NOTE: Tasks Summary: Attempted 8055 tasks of which 8054 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;how can i add apt package in the local.conf for used in putty&lt;/P&gt;</description>
    <pubDate>Thu, 28 Sep 2023 05:56:20 GMT</pubDate>
    <dc:creator>veeranagouda</dc:creator>
    <dc:date>2023-09-28T05:56:20Z</dc:date>
    <item>
      <title>Install Bitbake fsl-image-gui</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Install-Bitbake-fsl-image-gui/m-p/1726018#M212840</link>
      <description>&lt;P&gt;ERROR: Task 2761 (/home/veeranagouda/iwg15-release-bsp/sources/meta-openembedded/meta-oe/recipes-support/opencv/opencv_3.1.bb, do_compile) failed with exit code '1&lt;/P&gt;&lt;P&gt;when I'm installing Bitbake&amp;nbsp;&lt;STRONG&gt;fsl-image-gui I am getting error like this unable to solve&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 20 Sep 2023 07:17:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Install-Bitbake-fsl-image-gui/m-p/1726018#M212840</guid>
      <dc:creator>veeranagouda</dc:creator>
      <dc:date>2023-09-20T07:17:25Z</dc:date>
    </item>
    <item>
      <title>Re: Install Bitbake fsl-image-gui</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Install-Bitbake-fsl-image-gui/m-p/1726947#M212925</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/223235"&gt;@veeranagouda&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Can't really tell what the problem is only by the error.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;To check the compile error log can probably find logs for troubleshooting.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you have followed Yocto User Guide.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Thu, 21 Sep 2023 08:17:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Install-Bitbake-fsl-image-gui/m-p/1726947#M212925</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2023-09-21T08:17:35Z</dc:date>
    </item>
    <item>
      <title>Re: Install Bitbake fsl-image-gui</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Install-Bitbake-fsl-image-gui/m-p/1731007#M213321</link>
      <description>&lt;P&gt;ERROR: fsl-image-gui-1.0-r0 do_rootfs: Unable to install packages. Command '/home/veeranagouda/iwg15-release-bsp/build_iwg15/tmp/sysroots/x86_64-linux/usr/bin/apt-get install --force-yes --allow-unauthenticated packagegroup-core-ssh-dropbear qt5nmapcarousedemo psplash packagegroup-core-tools-profile apt packagegroup-qt5-demos cinematicexperience packagegroup-fsl-tools-audio qtsmarthome packagegroup-fsl-tools-benchmark qtbase-examples quitindicators qt5nmapper quitbattery packagegroup-core-boot packagegroup-core-full-cmdline packagegroup-core-tools-testapps packagegroup-core-x11-base packagegroup-fsl-gstreamer1.0-full packagegroup-core-nfs-server qtdeclarative-examples iwtest qt3d-examples packagegroup-fsl-gstreamer1.0 packagegroup-fsl-tools-gpu packagegroup-fsl-tools-testapps run-postinsts packagegroup-fsl-tools-gpu-external packagegroup-core-tools-debug qt5ledscreen qt5everywheredemo packagegroup-qt5-toolchain-target qt5-demo-extrafiles packagegroup-tools-bluetooth packagegroup-base-extended packagegroup-core-x11-sato' returned 100:&lt;BR /&gt;Reading package lists...&lt;BR /&gt;Building dependency tree...&lt;BR /&gt;Reading state information...&lt;BR /&gt;Some packages could not be installed. This may mean that you have&lt;BR /&gt;requested an impossible situation or if you are using the unstable&lt;BR /&gt;distribution that some required packages have not yet been created&lt;BR /&gt;or been moved out of Incoming.&lt;BR /&gt;The following information may help to resolve the situation:&lt;/P&gt;&lt;P&gt;The following packages have unmet dependencies:&lt;BR /&gt;packagegroup-core-x11-base : Depends: packagegroup-core-x11-utils but it is not going to be installed&lt;BR /&gt;E: Unable to correct problems, you have held broken packages.&lt;/P&gt;&lt;P&gt;ERROR: fsl-image-gui-1.0-r0 do_rootfs: Function failed: do_rootfs&lt;BR /&gt;ERROR: Logfile of failure stored in: /home/veeranagouda/iwg15-release-bsp/build_iwg15/tmp/work/imx6qdl_iwg15_sm-poky-linux-gnueabi/fsl-image-gui/1.0-r0/temp/log.do_rootfs.29574&lt;BR /&gt;ERROR: Task 9 (/home/veeranagouda/iwg15-release-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-fsl/images/fsl-image-gui.bb, do_rootfs) failed with exit code '1'&lt;BR /&gt;NOTE: Tasks Summary: Attempted 8055 tasks of which 8054 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;how can i add apt package in the local.conf for used in putty&lt;/P&gt;</description>
      <pubDate>Thu, 28 Sep 2023 05:56:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Install-Bitbake-fsl-image-gui/m-p/1731007#M213321</guid>
      <dc:creator>veeranagouda</dc:creator>
      <dc:date>2023-09-28T05:56:20Z</dc:date>
    </item>
    <item>
      <title>Re: Install Bitbake fsl-image-gui</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Install-Bitbake-fsl-image-gui/m-p/1731135#M213331</link>
      <description>&lt;P&gt;apt tool, by default, installed in image.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regard&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Thu, 28 Sep 2023 08:19:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Install-Bitbake-fsl-image-gui/m-p/1731135#M213331</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2023-09-28T08:19:45Z</dc:date>
    </item>
    <item>
      <title>Re: Install Bitbake fsl-image-gui</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Install-Bitbake-fsl-image-gui/m-p/1731185#M213338</link>
      <description>&lt;P&gt;but when im using in&amp;nbsp; sudo apt command in putty its showing apt command not found&lt;/P&gt;</description>
      <pubDate>Thu, 28 Sep 2023 09:26:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Install-Bitbake-fsl-image-gui/m-p/1731185#M213338</guid>
      <dc:creator>veeranagouda</dc:creator>
      <dc:date>2023-09-28T09:26:30Z</dc:date>
    </item>
    <item>
      <title>Re: Install Bitbake fsl-image-gui</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Install-Bitbake-fsl-image-gui/m-p/1731881#M213380</link>
      <description>&lt;P&gt;I haven't tried apt on&amp;nbsp;fsl-image-gui, anyhow, I believe the recipe for apt should be there /poky/meta/recipes-devtools/. so you can build it to your image.&amp;nbsp;&lt;/P&gt;&lt;P&gt;By the way, after you build apt into your image, you have to take care of the secure authentication for using apt tool.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Fri, 29 Sep 2023 08:43:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Install-Bitbake-fsl-image-gui/m-p/1731881#M213380</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2023-09-29T08:43:05Z</dc:date>
    </item>
  </channel>
</rss>