<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Guidelines - Unit testing and CI/CD in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Guidelines-Unit-testing-and-CI-CD/m-p/1730771#M213293</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm quite new to NXP and MCUxpresso and I was wondering what the possibilities are to setup up a CI/CD pipeline and unit testing (on the host).&lt;/P&gt;&lt;P&gt;Usually I setup github actions to run tests (using cppUtest or something) and compile the program using docker containers, but with the MCUxpresso IDE I'm a bit lost how I should approach this.&lt;/P&gt;&lt;P&gt;Are there some examples of unit testing and CI/CD pipelines?&lt;BR /&gt;Any tips &amp;amp; tricks are highly appreciated!&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Thx!&lt;/P&gt;</description>
    <pubDate>Wed, 27 Sep 2023 20:50:02 GMT</pubDate>
    <dc:creator>Geiger8759</dc:creator>
    <dc:date>2023-09-27T20:50:02Z</dc:date>
    <item>
      <title>Guidelines - Unit testing and CI/CD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Guidelines-Unit-testing-and-CI-CD/m-p/1730771#M213293</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm quite new to NXP and MCUxpresso and I was wondering what the possibilities are to setup up a CI/CD pipeline and unit testing (on the host).&lt;/P&gt;&lt;P&gt;Usually I setup github actions to run tests (using cppUtest or something) and compile the program using docker containers, but with the MCUxpresso IDE I'm a bit lost how I should approach this.&lt;/P&gt;&lt;P&gt;Are there some examples of unit testing and CI/CD pipelines?&lt;BR /&gt;Any tips &amp;amp; tricks are highly appreciated!&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Thx!&lt;/P&gt;</description>
      <pubDate>Wed, 27 Sep 2023 20:50:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Guidelines-Unit-testing-and-CI-CD/m-p/1730771#M213293</guid>
      <dc:creator>Geiger8759</dc:creator>
      <dc:date>2023-09-27T20:50:02Z</dc:date>
    </item>
    <item>
      <title>Re: Guidelines - Unit testing and CI/CD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Guidelines-Unit-testing-and-CI-CD/m-p/1732896#M213480</link>
      <description>&lt;P&gt;Erich Styger just posted an article about this:&amp;nbsp;&lt;A href="https://mcuoneclipse.com/2023/10/02/ci-cd-for-embedded-with-vs-code-docker-and-github-actions/" target="_blank"&gt;https://mcuoneclipse.com/2023/10/02/ci-cd-for-embedded-with-vs-code-docker-and-github-actions/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Many thanks Erich!&lt;/P&gt;</description>
      <pubDate>Tue, 03 Oct 2023 06:40:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Guidelines-Unit-testing-and-CI-CD/m-p/1732896#M213480</guid>
      <dc:creator>Geiger8759</dc:creator>
      <dc:date>2023-10-03T06:40:18Z</dc:date>
    </item>
  </channel>
</rss>