<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Boot IMX8MM using USB serial port</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Boot-IMX8MM-using-USB-serial-port/m-p/1728923#M213108</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/217485"&gt;@ajita02&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;Please make sure that you have used the correct commands. Please share the uuu commands that were used to flash the board and board schematics for further debugging.&lt;/P&gt;
&lt;P&gt;Please make sure that boot mode and CFG pins are set correctly.&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Dhruvit Vasavada&lt;/P&gt;</description>
    <pubDate>Mon, 25 Sep 2023 12:27:51 GMT</pubDate>
    <dc:creator>Dhruvit</dc:creator>
    <dc:date>2023-09-25T12:27:51Z</dc:date>
    <item>
      <title>Boot IMX8MM using USB serial port</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-IMX8MM-using-USB-serial-port/m-p/1728897#M213106</link>
      <description>&lt;P&gt;Hi all,&lt;BR /&gt;&lt;BR /&gt;We have a custom board which uses IMX8MM. I want to boot board using serial port. We dont have eMMC support on board. Also board is not booting through sd card slot.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ajita&lt;BR /&gt;&lt;LI-PRODUCT title="iMX8MMINI" id="iMX8MMINI"&gt;&lt;/LI-PRODUCT&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 25 Sep 2023 11:54:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-IMX8MM-using-USB-serial-port/m-p/1728897#M213106</guid>
      <dc:creator>ajita02</dc:creator>
      <dc:date>2023-09-25T11:54:23Z</dc:date>
    </item>
    <item>
      <title>Re: Boot IMX8MM using USB serial port</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-IMX8MM-using-USB-serial-port/m-p/1728923#M213108</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/217485"&gt;@ajita02&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;Please make sure that you have used the correct commands. Please share the uuu commands that were used to flash the board and board schematics for further debugging.&lt;/P&gt;
&lt;P&gt;Please make sure that boot mode and CFG pins are set correctly.&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Dhruvit Vasavada&lt;/P&gt;</description>
      <pubDate>Mon, 25 Sep 2023 12:27:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-IMX8MM-using-USB-serial-port/m-p/1728923#M213108</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2023-09-25T12:27:51Z</dc:date>
    </item>
    <item>
      <title>Re: Boot IMX8MM using USB serial port</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-IMX8MM-using-USB-serial-port/m-p/1729606#M213172</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201299"&gt;@Dhruvit&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Is it possible to boot kernel image through UUU? Our board dont have emmc support and our SD card is not booting. What can be done in this case?&lt;/P&gt;&lt;P&gt;I made bootmode switch as "1010xxxxxx". I have built "imx-image-full". The image has been tested with imx8mm evk board.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ajita&lt;/P&gt;</description>
      <pubDate>Tue, 26 Sep 2023 09:39:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-IMX8MM-using-USB-serial-port/m-p/1729606#M213172</guid>
      <dc:creator>ajita02</dc:creator>
      <dc:date>2023-09-26T09:39:02Z</dc:date>
    </item>
    <item>
      <title>Re: Boot IMX8MM using USB serial port</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-IMX8MM-using-USB-serial-port/m-p/1730240#M213232</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/217485"&gt;@ajita02&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;UUU can boot u-boot and can flash kernel image and rootfs.&lt;/P&gt;
&lt;P&gt;If emmc is not available, then one can flash kernel image and rootfs to sd card using uuu.&lt;/P&gt;
&lt;P&gt;Please change the DIP switches to serial download mode.&lt;/P&gt;
&lt;P&gt;Please use the below command.&lt;/P&gt;
&lt;P&gt;uuu -b sd_all &amp;lt;imx-boot-*&amp;gt; &amp;lt;rootfs/imx-image-full image&amp;gt;&lt;/P&gt;
&lt;P&gt;After flashing one can change DIP switches back to internal boot mode &amp;amp; SD card.&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Dhruvit Vasavada&lt;/P&gt;</description>
      <pubDate>Wed, 27 Sep 2023 07:16:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-IMX8MM-using-USB-serial-port/m-p/1730240#M213232</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2023-09-27T07:16:32Z</dc:date>
    </item>
  </channel>
</rss>