<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Communicating with external storage SSD with only using RX and TX line of the USB3.0</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Communicating-with-external-storage-SSD-with-only-using-RX-and/m-p/1728044#M213031</link>
    <description>&lt;P&gt;Hi Ritesh,&lt;BR /&gt;&lt;BR /&gt;Thank you for the clarification&lt;BR /&gt;&lt;BR /&gt;I need to confirm one thing , are there different&amp;nbsp; USB2.0 PHY and USB3.0 PHY ?or the single USB PHY which controlled both USB2.0 and USB3.0?&lt;BR /&gt;Basically i am uing USB2.0 for the flashing and debugging and USB3.0 Rx and Tx for the SSD , so whether both the things can run simultaneously&amp;nbsp; ?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Parag1_0-1695386829117.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/242263i8A0BD34174181B51/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Parag1_0-1695386829117.png" alt="Parag1_0-1695386829117.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Parag1_0-1695386829117.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;above image is from the imx8m reference manual . here they have mentionUSB2.0 PHy and USB3.0 PHY , so i think there will be different phy for the both ,So according to this i can use USB2.0 for flashing and debugging and USB3.0 for the SSD at the same time.&lt;BR /&gt;&lt;BR /&gt;Please let me know on this topic&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 22 Sep 2023 12:51:49 GMT</pubDate>
    <dc:creator>Parag1</dc:creator>
    <dc:date>2023-09-22T12:51:49Z</dc:date>
    <item>
      <title>Communicating with external storage SSD with only using RX and TX line of the USB3.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Communicating-with-external-storage-SSD-with-only-using-RX-and/m-p/1726920#M212923</link>
      <description>&lt;P&gt;Hello Team,&lt;BR /&gt;&lt;BR /&gt;I am using imx8m plus processor , and want to connect external storage SSD&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Parag1_0-1695282524402.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/241983i83357E1585E9B4D7/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Parag1_0-1695282524402.png" alt="Parag1_0-1695282524402.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Parag1_0-1695282524402.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Above is the block diagram of the IC i am going to use for the SSD Connection and Communication.&lt;BR /&gt;In this IC as you can see both USB3.0 and USB2.0 of the imx8m are connected to the SATA Gen1/2 .&lt;BR /&gt;But in my case USB2.0 will not be available we are using it for different application , so only TX and RX pins of the USB3.0 will be there . so will it possible to establish the connection with SSD using only TX and RX pins or do we required DP and DM ?&lt;BR /&gt;Please provide your response on this query.&lt;/P&gt;</description>
      <pubDate>Thu, 21 Sep 2023 07:54:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Communicating-with-external-storage-SSD-with-only-using-RX-and/m-p/1726920#M212923</guid>
      <dc:creator>Parag1</dc:creator>
      <dc:date>2023-09-21T07:54:17Z</dc:date>
    </item>
    <item>
      <title>Re: Communicating with external storage SSD with only using RX and TX line of the USB3.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Communicating-with-external-storage-SSD-with-only-using-RX-and/m-p/1727107#M212944</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/223283"&gt;@Parag1&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;DP and DM pins are necessary for USB enumeration and speed detection. So, they cannot be omitted from the USB 3.0 connections.&lt;/P&gt;
&lt;P&gt;I hope it helps!&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Ritesh M Patel&lt;/P&gt;</description>
      <pubDate>Thu, 21 Sep 2023 11:21:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Communicating-with-external-storage-SSD-with-only-using-RX-and/m-p/1727107#M212944</guid>
      <dc:creator>riteshmpatel</dc:creator>
      <dc:date>2023-09-21T11:21:22Z</dc:date>
    </item>
    <item>
      <title>Re: Communicating with external storage SSD with only using RX and TX line of the USB3.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Communicating-with-external-storage-SSD-with-only-using-RX-and/m-p/1727697#M212992</link>
      <description>&lt;P&gt;Hello Ritesh,&lt;BR /&gt;&lt;BR /&gt;Thank you or the Response,&lt;BR /&gt;&lt;BR /&gt;What i think USB3.0 will Use Rx and TX first for the USB &lt;SPAN&gt;enumeration and speed detection, then it will switch to DP and DM if RX and Tx are busy .So it may possible to communicate with Rx and Tx lines of USB3.0 between imx8m and SSD.&lt;BR /&gt;Please let me know if i am wrong&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 22 Sep 2023 06:28:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Communicating-with-external-storage-SSD-with-only-using-RX-and/m-p/1727697#M212992</guid>
      <dc:creator>Parag1</dc:creator>
      <dc:date>2023-09-22T06:28:49Z</dc:date>
    </item>
    <item>
      <title>Re: Communicating with external storage SSD with only using RX and TX line of the USB3.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Communicating-with-external-storage-SSD-with-only-using-RX-and/m-p/1727975#M213024</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/223283"&gt;@Parag1&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Apologies for the inconvenience caused.&lt;BR /&gt;I discussed this with my internal team. Please see the response below:&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class="ui-provider axg axh ava axi axj axk axl axm axn axo axp axq axr axs axt axu axv axw axx axy axz aya ayb ayc ayd aye ayf ayg ayh ayi ayj ayk ayl aym ayn"&gt;DP/DM is used for USB 2.0. Normally, to make it compatible with USB 2.0. DP/DM, SS_Txp/Txn, and SS_Rxp/Rxn will be connected to the same port.&amp;nbsp;That is DP/DM is not used in super-speed communication.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class="ui-provider axg axh ava axi axj axk axl axm axn axo axp axq axr axs axt axu axv axw axx axy axz aya ayb ayc ayd aye ayf ayg ayh ayi ayj ayk ayl aym ayn"&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Ritesh M Patel&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 22 Sep 2023 10:46:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Communicating-with-external-storage-SSD-with-only-using-RX-and/m-p/1727975#M213024</guid>
      <dc:creator>riteshmpatel</dc:creator>
      <dc:date>2023-09-22T10:46:29Z</dc:date>
    </item>
    <item>
      <title>Re: Communicating with external storage SSD with only using RX and TX line of the USB3.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Communicating-with-external-storage-SSD-with-only-using-RX-and/m-p/1728044#M213031</link>
      <description>&lt;P&gt;Hi Ritesh,&lt;BR /&gt;&lt;BR /&gt;Thank you for the clarification&lt;BR /&gt;&lt;BR /&gt;I need to confirm one thing , are there different&amp;nbsp; USB2.0 PHY and USB3.0 PHY ?or the single USB PHY which controlled both USB2.0 and USB3.0?&lt;BR /&gt;Basically i am uing USB2.0 for the flashing and debugging and USB3.0 Rx and Tx for the SSD , so whether both the things can run simultaneously&amp;nbsp; ?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Parag1_0-1695386829117.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/242263i8A0BD34174181B51/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Parag1_0-1695386829117.png" alt="Parag1_0-1695386829117.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Parag1_0-1695386829117.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;above image is from the imx8m reference manual . here they have mentionUSB2.0 PHy and USB3.0 PHY , so i think there will be different phy for the both ,So according to this i can use USB2.0 for flashing and debugging and USB3.0 for the SSD at the same time.&lt;BR /&gt;&lt;BR /&gt;Please let me know on this topic&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 22 Sep 2023 12:51:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Communicating-with-external-storage-SSD-with-only-using-RX-and/m-p/1728044#M213031</guid>
      <dc:creator>Parag1</dc:creator>
      <dc:date>2023-09-22T12:51:49Z</dc:date>
    </item>
    <item>
      <title>Re: Communicating with external storage SSD with only using RX and TX line of the USB3.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Communicating-with-external-storage-SSD-with-only-using-RX-and/m-p/1728622#M213084</link>
      <description>&lt;P&gt;Hi Ritesh,&lt;BR /&gt;&lt;BR /&gt;Can you please quickly update here&lt;BR /&gt;&lt;BR /&gt;Thank you for your support&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 25 Sep 2023 07:11:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Communicating-with-external-storage-SSD-with-only-using-RX-and/m-p/1728622#M213084</guid>
      <dc:creator>Parag1</dc:creator>
      <dc:date>2023-09-25T07:11:41Z</dc:date>
    </item>
    <item>
      <title>Re: Communicating with external storage SSD with only using RX and TX line of the USB3.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Communicating-with-external-storage-SSD-with-only-using-RX-and/m-p/1729584#M213171</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/223283"&gt;@Parag1&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;USB port cannot be used for debugging. For debugging, one can use the UART port as mentioned in the Reference Manual.&lt;/P&gt;
&lt;P&gt;In addition to that, flashing via USB 2.0 and using RX &amp;amp; TX for USB 3.0 cannot happen at the same time, since while flashing the processor, only ROM code will run.&lt;/P&gt;
&lt;P&gt;I hope it helps!&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Ritesh M Patel&lt;/P&gt;</description>
      <pubDate>Tue, 26 Sep 2023 09:21:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Communicating-with-external-storage-SSD-with-only-using-RX-and/m-p/1729584#M213171</guid>
      <dc:creator>riteshmpatel</dc:creator>
      <dc:date>2023-09-26T09:21:19Z</dc:date>
    </item>
  </channel>
</rss>