<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: About the resistance value of the internal pull-up resistor of the PMIC_ON_REQ of the imx6ull ch in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/About-the-resistance-value-of-the-internal-pull-up-resistor-of/m-p/1726209#M212861</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/222605"&gt;@hyw666&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Just find the macro that muxing this pin in dts, and then modify the PAD driver capability.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Harvey&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 20 Sep 2023 09:40:48 GMT</pubDate>
    <dc:creator>Harvey021</dc:creator>
    <dc:date>2023-09-20T09:40:48Z</dc:date>
    <item>
      <title>About the resistance value of the internal pull-up resistor of the PMIC_ON_REQ of the imx6ull chip</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-the-resistance-value-of-the-internal-pull-up-resistor-of/m-p/1724087#M212672</link>
      <description>&lt;P&gt;I have noticed that imx6ull chip PMIC_ON_REQ internal 100k pull-up, but now I need to increase the drive capability of the IO, can I modify its internal pull-up resistance?On my development board, due to the insufficient driving ability of PMIC_ON_REQ signal, after ONOFF shutdown, the PMIC ON REQ still has 1.8-2v voltage, resulting in 3.3 and 5v peripheral voltage still, which is a fake shutdown.&lt;/P&gt;&lt;P&gt;I check the manual and find SW_PAD_CTL_PAD_SNVS_PMIC_ON_REQ SW PAD Control Register can configure the electrical properties of PMIC_ON_REQ as follows:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="1.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/241238i3EFA25C340A5881F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="2.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/241239i3E4977962EA60C25/image-size/medium?v=v2&amp;amp;px=400" role="button" title="2.png" alt="2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I tried to change the register value to 0001 1111 0000 1011 1000, i.e. 0x1F0B8, 22k Pull up, I added the address of the register on the uboot source code, changed the register to Ox1FOB8, in the kernel part, I wrote the character device driver to set the register to Ox1FOB8, So that after uboot boot and kernel boot, the value of the register is Ox1FOB8.&lt;/P&gt;&lt;P&gt;However, I found that PMIC_ON_REQ still has 1.8-2v voltage after shutdown, I only modified the SW_PAD register because I did not know the clock of the signal, and it did not have the multiplexing register, the I/O mode register, the level configuration register.&lt;/P&gt;&lt;P&gt;I think PMIC_ON_REQ's pin clock is turned on by default. Is this correct? Do I only need to modify the SW_PAD register to configure the electrical properties of PMIC_ON_REQ to achieve 22k pull-up?&lt;/P&gt;&lt;P&gt;Wish you all the best.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 15 Sep 2023 18:22:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-the-resistance-value-of-the-internal-pull-up-resistor-of/m-p/1724087#M212672</guid>
      <dc:creator>hyw666</dc:creator>
      <dc:date>2023-09-15T18:22:55Z</dc:date>
    </item>
    <item>
      <title>Re: About the resistance value of the internal pull-up resistor of the PMIC_ON_REQ of the imx6ull ch</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-the-resistance-value-of-the-internal-pull-up-resistor-of/m-p/1726209#M212861</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/222605"&gt;@hyw666&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Just find the macro that muxing this pin in dts, and then modify the PAD driver capability.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Harvey&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 20 Sep 2023 09:40:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-the-resistance-value-of-the-internal-pull-up-resistor-of/m-p/1726209#M212861</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2023-09-20T09:40:48Z</dc:date>
    </item>
  </channel>
</rss>