<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using spi and i2c protocols in imxrt1176 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-spi-and-i2c-protocols-in-imxrt1176/m-p/1725711#M212808</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;To use SPI and I2C you have two options. The first is through LPSPI or LPI2C, respectively. The second is with the FlexIO module, which is capable of supporting a wide range of protocols, among them SPI and I2C.&lt;/P&gt;
&lt;P&gt;In the SDK you will find examples of LPSPI, LPI2C, as well as SPI and I2C with FlexIO. I also recommend consulting &lt;EM&gt;Table 11-1. Muxing Options&lt;/EM&gt; from reference manual.&lt;/P&gt;
&lt;P&gt;Hope it helps you.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
    <pubDate>Tue, 19 Sep 2023 18:43:11 GMT</pubDate>
    <dc:creator>_Leo_</dc:creator>
    <dc:date>2023-09-19T18:43:11Z</dc:date>
    <item>
      <title>Using spi and i2c protocols in imxrt1176</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-spi-and-i2c-protocols-in-imxrt1176/m-p/1720825#M212410</link>
      <description>&lt;P&gt;I wanted to use spi and i2c communication protocols in the evaluation board, mimxrt1170 -&amp;nbsp; evk. When I am going through datasheet I found out that spi and i2c can be configured through flexio pins. But I want to know that is there any dedicated spi and i2c pins are there in imxrt1176 chip.Every example code I found also use flexio. Can anyone clarify to me.&lt;/P&gt;</description>
      <pubDate>Tue, 12 Sep 2023 05:13:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-spi-and-i2c-protocols-in-imxrt1176/m-p/1720825#M212410</guid>
      <dc:creator>Shehan_Janidu</dc:creator>
      <dc:date>2023-09-12T05:13:38Z</dc:date>
    </item>
    <item>
      <title>Re: Using spi and i2c protocols in imxrt1176</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-spi-and-i2c-protocols-in-imxrt1176/m-p/1725711#M212808</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;To use SPI and I2C you have two options. The first is through LPSPI or LPI2C, respectively. The second is with the FlexIO module, which is capable of supporting a wide range of protocols, among them SPI and I2C.&lt;/P&gt;
&lt;P&gt;In the SDK you will find examples of LPSPI, LPI2C, as well as SPI and I2C with FlexIO. I also recommend consulting &lt;EM&gt;Table 11-1. Muxing Options&lt;/EM&gt; from reference manual.&lt;/P&gt;
&lt;P&gt;Hope it helps you.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Tue, 19 Sep 2023 18:43:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-spi-and-i2c-protocols-in-imxrt1176/m-p/1725711#M212808</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2023-09-19T18:43:11Z</dc:date>
    </item>
  </channel>
</rss>