<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Config PWM in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Config-PWM/m-p/1724964#M212756</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;That pins corresponds to &lt;EM&gt;PWM_X&lt;/EM&gt; signals, which can output a third PWM signal from each submodule. However, the SDK does not include support for &lt;EM&gt;PWM_X&lt;/EM&gt; functionality other than input capture.&lt;/P&gt;
&lt;P&gt;If you refer to the &lt;EM&gt;50.3.2.4 PWM Generation&lt;/EM&gt; section of reference manual, the &lt;EM&gt;VAL0&lt;/EM&gt; and &lt;EM&gt;VAL1&lt;/EM&gt; comparators can be used to set frequency and duty cycle, based on the incoming clock to the counter.&lt;/P&gt;
&lt;P&gt;Hope it helps you.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
    <pubDate>Mon, 18 Sep 2023 21:01:44 GMT</pubDate>
    <dc:creator>_Leo_</dc:creator>
    <dc:date>2023-09-18T21:01:44Z</dc:date>
    <item>
      <title>Config PWM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Config-PWM/m-p/1722011#M212538</link>
      <description>&lt;P&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;How to configure 7 and 4 pins to output PWM signals respectively? [i.MX RT 1020 ]&lt;/P&gt;</description>
      <pubDate>Wed, 13 Sep 2023 11:30:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Config-PWM/m-p/1722011#M212538</guid>
      <dc:creator>IanBrand</dc:creator>
      <dc:date>2023-09-13T11:30:56Z</dc:date>
    </item>
    <item>
      <title>Re: Config PWM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Config-PWM/m-p/1724964#M212756</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;That pins corresponds to &lt;EM&gt;PWM_X&lt;/EM&gt; signals, which can output a third PWM signal from each submodule. However, the SDK does not include support for &lt;EM&gt;PWM_X&lt;/EM&gt; functionality other than input capture.&lt;/P&gt;
&lt;P&gt;If you refer to the &lt;EM&gt;50.3.2.4 PWM Generation&lt;/EM&gt; section of reference manual, the &lt;EM&gt;VAL0&lt;/EM&gt; and &lt;EM&gt;VAL1&lt;/EM&gt; comparators can be used to set frequency and duty cycle, based on the incoming clock to the counter.&lt;/P&gt;
&lt;P&gt;Hope it helps you.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Mon, 18 Sep 2023 21:01:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Config-PWM/m-p/1724964#M212756</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2023-09-18T21:01:44Z</dc:date>
    </item>
  </channel>
</rss>