<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Interrupt geneartion between Cortex-A53 &amp;amp; Cortex-M4 in imx8mm in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Interrupt-geneartion-between-Cortex-A53-amp-Cortex-M4-in-imx8mm/m-p/1723607#M212632</link>
    <description>&lt;P&gt;I too have similar question!!, what is the purpose of keeping M4 along with Cortex -A53 in imx8mmini or so? What are the best examples&lt;/P&gt;&lt;P&gt;which have been already implemented using these cores ?&lt;/P&gt;&lt;P&gt;I was going though Reference manual of imx8m Message Unit Section, explains about so many concepts, but are there any examples to verify those? I want to send an interrupt from M4 to A53 or vice versa by making use of below concepts. I could find very few examples in mcuexpress sdk that too simple messaging examples.... is OpenAmp supported on imx8m platform? or only RPmsglite works?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;4.3.2.7.1 Interrupts to the Processors&lt;BR /&gt;There are 12 interrupt sources from the MU to the Processors:&lt;BR /&gt;• Four receive interrupts (asserted when the Processors receive full bits are set and&lt;BR /&gt;enabled in the xCR register) for each of the receive registers&lt;BR /&gt;• Four transmit interrupts (asserted when the Processor transmit empty bits are set and&lt;BR /&gt;enabled in the xCR register) for each of the transmit registers&lt;BR /&gt;• Four general purpose interrupts (asserted when the GIP bits are set and enabled in the&lt;BR /&gt;xCR register)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;kindly update&lt;/P&gt;</description>
    <pubDate>Fri, 15 Sep 2023 04:44:14 GMT</pubDate>
    <dc:creator>prasannakulkarni</dc:creator>
    <dc:date>2023-09-15T04:44:14Z</dc:date>
    <item>
      <title>Interrupt geneartion between Cortex-A53 &amp; Cortex-M4 in imx8mm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Interrupt-geneartion-between-Cortex-A53-amp-Cortex-M4-in-imx8mm/m-p/1723607#M212632</link>
      <description>&lt;P&gt;I too have similar question!!, what is the purpose of keeping M4 along with Cortex -A53 in imx8mmini or so? What are the best examples&lt;/P&gt;&lt;P&gt;which have been already implemented using these cores ?&lt;/P&gt;&lt;P&gt;I was going though Reference manual of imx8m Message Unit Section, explains about so many concepts, but are there any examples to verify those? I want to send an interrupt from M4 to A53 or vice versa by making use of below concepts. I could find very few examples in mcuexpress sdk that too simple messaging examples.... is OpenAmp supported on imx8m platform? or only RPmsglite works?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;4.3.2.7.1 Interrupts to the Processors&lt;BR /&gt;There are 12 interrupt sources from the MU to the Processors:&lt;BR /&gt;• Four receive interrupts (asserted when the Processors receive full bits are set and&lt;BR /&gt;enabled in the xCR register) for each of the receive registers&lt;BR /&gt;• Four transmit interrupts (asserted when the Processor transmit empty bits are set and&lt;BR /&gt;enabled in the xCR register) for each of the transmit registers&lt;BR /&gt;• Four general purpose interrupts (asserted when the GIP bits are set and enabled in the&lt;BR /&gt;xCR register)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;kindly update&lt;/P&gt;</description>
      <pubDate>Fri, 15 Sep 2023 04:44:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Interrupt-geneartion-between-Cortex-A53-amp-Cortex-M4-in-imx8mm/m-p/1723607#M212632</guid>
      <dc:creator>prasannakulkarni</dc:creator>
      <dc:date>2023-09-15T04:44:14Z</dc:date>
    </item>
    <item>
      <title>Re: Interrupt geneartion between Cortex-A53 &amp; Cortex-M4 in imx8mm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Interrupt-geneartion-between-Cortex-A53-amp-Cortex-M4-in-imx8mm/m-p/1725850#M212818</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The Linux side will call&amp;nbsp;&lt;SPAN&gt;&lt;STRONG&gt;imx_rproc_xtr_mbox_init&lt;/STRONG&gt;-&amp;gt;&lt;/SPAN&gt;&lt;SPAN&gt;mbox_request_channel_byname-&amp;gt;&lt;/SPAN&gt;&lt;SPAN&gt;mbox_request_channel-&amp;gt;&lt;/SPAN&gt;&lt;SPAN&gt;imx_mu_dcfg to realize RX/TX message, but the mailbox driver miss the code for Generic interrupt, you can refer this case :&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/imx8mm-Wake-Linux-from-M4-core/m-p/1492800" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/i-MX-Processors/imx8mm-Wake-Linux-from-M4-core/m-p/1492800&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 20 Sep 2023 02:46:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Interrupt-geneartion-between-Cortex-A53-amp-Cortex-M4-in-imx8mm/m-p/1725850#M212818</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2023-09-20T02:46:07Z</dc:date>
    </item>
  </channel>
</rss>