<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MIMXRT1176AVM8A internal dc dc operating frequency in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1176AVM8A-internal-dc-dc-operating-frequency/m-p/1722442#M212569</link>
    <description>&lt;P&gt;The on-chip DC-DC regulator of the processor is suitable for consumer and industrial applications up to 105 °C. The part that you are using is for automotive applications, in this case, the core platform power consumption may exceed the internal DC-DC capacity as the Tj is increased to 125 °C. In such cases, use RT1170 with NXP PF5020 PMIC.&lt;/P&gt;</description>
    <pubDate>Wed, 13 Sep 2023 22:14:18 GMT</pubDate>
    <dc:creator>_Leo_</dc:creator>
    <dc:date>2023-09-13T22:14:18Z</dc:date>
    <item>
      <title>MIMXRT1176AVM8A internal dc dc operating frequency</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1176AVM8A-internal-dc-dc-operating-frequency/m-p/1716995#M212031</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;I will use internal dc dc of MIMXRT1176AVM8A without PMIC.&lt;/P&gt;&lt;P&gt;8 in the processor code and as far as I understood from the datasheet, the nominal core frequency of the 800 Mhz processor..&lt;/P&gt;&lt;P&gt;Can I go to higher frequencies if I need it?&lt;/P&gt;&lt;P&gt;Can I use this processor in a 1 Ghz application(Automotive)? If I can, what would be the differences in terms of temperature?&lt;/P&gt;</description>
      <pubDate>Tue, 05 Sep 2023 08:35:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1176AVM8A-internal-dc-dc-operating-frequency/m-p/1716995#M212031</guid>
      <dc:creator>EMertCakir</dc:creator>
      <dc:date>2023-09-05T08:35:53Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1176AVM8A internal dc dc operating frequency</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1176AVM8A-internal-dc-dc-operating-frequency/m-p/1719078#M212222</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;The part that you mention can only operate up to 800 MHz.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Thu, 07 Sep 2023 23:16:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1176AVM8A-internal-dc-dc-operating-frequency/m-p/1719078#M212222</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2023-09-07T23:16:36Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1176AVM8A internal dc dc operating frequency</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1176AVM8A-internal-dc-dc-operating-frequency/m-p/1719351#M212248</link>
      <description>&lt;P&gt;hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/199320"&gt;@_Leo_&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is the frequency you are talking about internal dc dc operating frequency?&lt;/P&gt;&lt;P&gt;Can I run internal dc dc with 800 mhz?&lt;/P&gt;</description>
      <pubDate>Fri, 08 Sep 2023 08:12:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1176AVM8A-internal-dc-dc-operating-frequency/m-p/1719351#M212248</guid>
      <dc:creator>EMertCakir</dc:creator>
      <dc:date>2023-09-08T08:12:12Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1176AVM8A internal dc dc operating frequency</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1176AVM8A-internal-dc-dc-operating-frequency/m-p/1721140#M212458</link>
      <description>&lt;P&gt;Hi&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/199320"&gt;@_Leo_&lt;/a&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 12 Sep 2023 10:56:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1176AVM8A-internal-dc-dc-operating-frequency/m-p/1721140#M212458</guid>
      <dc:creator>EMertCakir</dc:creator>
      <dc:date>2023-09-12T10:56:25Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1176AVM8A internal dc dc operating frequency</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1176AVM8A-internal-dc-dc-operating-frequency/m-p/1722442#M212569</link>
      <description>&lt;P&gt;The on-chip DC-DC regulator of the processor is suitable for consumer and industrial applications up to 105 °C. The part that you are using is for automotive applications, in this case, the core platform power consumption may exceed the internal DC-DC capacity as the Tj is increased to 125 °C. In such cases, use RT1170 with NXP PF5020 PMIC.&lt;/P&gt;</description>
      <pubDate>Wed, 13 Sep 2023 22:14:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1176AVM8A-internal-dc-dc-operating-frequency/m-p/1722442#M212569</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2023-09-13T22:14:18Z</dc:date>
    </item>
  </channel>
</rss>