<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: RAM Test using UUU</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RAM-Test-using-UUU/m-p/1721133#M212456</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/188620"&gt;@ankitpanchal167&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;I hope you are doing well.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Yes, As per the uuu script I tried to run the command to read and write in the memory but it skipped the command and jumped to the SDPU command sequence.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The SDP commands will only be run when the machine is i.MX6/7/8MM/8MQ.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Dhruvit Vasavada&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 12 Sep 2023 10:51:16 GMT</pubDate>
    <dc:creator>Dhruvit</dc:creator>
    <dc:date>2023-09-12T10:51:16Z</dc:date>
    <item>
      <title>RAM Test using UUU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RAM-Test-using-UUU/m-p/1720256#M212350</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I want to perform a RAM test on imx8mp using UUU utility. Can you please provide any references to meet our expectations?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have already tested the imx6ull&amp;nbsp;processer and we found some options to test 'rdmem' and 'wrmem' commands in UUU to test RAM memory but for the imx8mp it is not available.&lt;/P&gt;&lt;P&gt;UUU version :&amp;nbsp;1.4.193&lt;BR /&gt;Uboot-imx version : 2021.0&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 11 Sep 2023 09:37:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RAM-Test-using-UUU/m-p/1720256#M212350</guid>
      <dc:creator>ankitpanchal167</dc:creator>
      <dc:date>2023-09-11T09:37:34Z</dc:date>
    </item>
    <item>
      <title>Re: RAM Test using UUU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RAM-Test-using-UUU/m-p/1721133#M212456</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/188620"&gt;@ankitpanchal167&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;I hope you are doing well.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Yes, As per the uuu script I tried to run the command to read and write in the memory but it skipped the command and jumped to the SDPU command sequence.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The SDP commands will only be run when the machine is i.MX6/7/8MM/8MQ.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Dhruvit Vasavada&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 12 Sep 2023 10:51:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RAM-Test-using-UUU/m-p/1721133#M212456</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2023-09-12T10:51:16Z</dc:date>
    </item>
    <item>
      <title>Re: RAM Test using UUU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RAM-Test-using-UUU/m-p/1721200#M212466</link>
      <description>Yes, right SDP commands are not working with imx8mp. I want to test RAM memory using UUU.&lt;BR /&gt;Is there any way to test RAM memory using UUU?&lt;BR /&gt;Like, push some binary on board. And test RAM and give the results.</description>
      <pubDate>Tue, 12 Sep 2023 12:01:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RAM-Test-using-UUU/m-p/1721200#M212466</guid>
      <dc:creator>ankitpanchal167</dc:creator>
      <dc:date>2023-09-12T12:01:28Z</dc:date>
    </item>
    <item>
      <title>Re: RAM Test using UUU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RAM-Test-using-UUU/m-p/1721782#M212513</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/188620"&gt;@ankitpanchal167&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="im"&gt;&lt;BR /&gt;I hope you are doing well.&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;It appears there is no way as the support is not given itself in i.MX8MP.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I suggest using DDR tool for i.MX8mp with that one can do RAM testing along with calibration, and stress test.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Please find it in the below link.&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467" target="_blank" rel="noopener" data-saferedirecturl="https://www.google.com/url?q=https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467&amp;amp;source=gmail&amp;amp;ust=1694671073147000&amp;amp;usg=AOvVaw3fPGkgCqKGvCyx4oJHueD4"&gt;https://community.nxp.com/t5/&lt;WBR /&gt;i-MX-Processors-Knowledge-&lt;WBR /&gt;Base/i-MX-8M-Family-DDR-Tool-&lt;WBR /&gt;Release/ta-p/1104467&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It will be helpful.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Dhruvit Vasavada&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Sep 2023 07:30:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RAM-Test-using-UUU/m-p/1721782#M212513</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2023-09-13T07:30:06Z</dc:date>
    </item>
  </channel>
</rss>