<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX8 Plus pm-suspend problem</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8-Plus-pm-suspend-problem/m-p/1721024#M212438</link>
    <description>&lt;P&gt;refer to your description, these bsp isn't nxp official released version, do you mind testing on nxp official bsp version? if still has the similar issue, pls tell me the reproduce steps&lt;/P&gt;
&lt;P&gt;"&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX&lt;/A&gt;"&lt;/P&gt;</description>
    <pubDate>Tue, 12 Sep 2023 08:50:29 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2023-09-12T08:50:29Z</dc:date>
    <item>
      <title>IMX8 Plus pm-suspend problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8-Plus-pm-suspend-problem/m-p/1720890#M212417</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have some troubles with pm-suspend command, executed on my IMX8 Plus board if some conditions are met:&lt;BR /&gt;The system is going to sleep if I execute pm-suspend command even if some processes are working in background. But if I start gstreamer, reading from video source - for example CMOS sensor with data processed by the MIPI-&amp;gt;ISP or from sensor with already processed data through MIPI-&amp;gt;ISI - there is a problem. Usually the pm-suspend script fails at line 297, exit code 128 - resource busy, the video stream to the HDMI output is still alive, the console is also active.&lt;BR /&gt;Similar setup on IMX6 Quad executes pm-suspend without problem even if the gstreamer is active and reading from video device over MIPI-&amp;gt;IPU, the IMX6 successfully enters sleep mode and wake-up on button.&lt;/P&gt;&lt;P&gt;Please note that I prefer not to stop the gstreamer pipe, which is already in operation - this logic works fine with IMX6, but fails with IMX8. My setup is based on FSLC 5.15-2.0.x-imx, kernel 5.15.60, yocto kirkstone.&lt;BR /&gt;&lt;BR /&gt;Is there some bug in this release, or the problem is the MIPI-&amp;gt;ISP/ISI peripherals preventing the system to go to sleep mode and if so - what is the workaround? Except to stop the gstreamer obviously..&lt;/P&gt;</description>
      <pubDate>Tue, 12 Sep 2023 06:49:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8-Plus-pm-suspend-problem/m-p/1720890#M212417</guid>
      <dc:creator>imsOPX</dc:creator>
      <dc:date>2023-09-12T06:49:57Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8 Plus pm-suspend problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8-Plus-pm-suspend-problem/m-p/1721024#M212438</link>
      <description>&lt;P&gt;refer to your description, these bsp isn't nxp official released version, do you mind testing on nxp official bsp version? if still has the similar issue, pls tell me the reproduce steps&lt;/P&gt;
&lt;P&gt;"&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX&lt;/A&gt;"&lt;/P&gt;</description>
      <pubDate>Tue, 12 Sep 2023 08:50:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8-Plus-pm-suspend-problem/m-p/1721024#M212438</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-09-12T08:50:29Z</dc:date>
    </item>
  </channel>
</rss>