<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic RDC: inconsistent values between SDK and manual in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RDC-inconsistent-values-between-SDK-and-manual/m-p/1719480#M212263</link>
    <description>&lt;P&gt;For iMXRT1176, the SDK and the reference manual do not agree about the RDC peripheral numbering.&lt;BR /&gt;RDC has 128 PDAP registers, each of which contains settings for a peripheral or group of peripherals.&lt;BR /&gt;The peripheral indices are specified in the reference manual (IMXRT1170RM Rev. 2, 06/2023), §42.5.2 Peripheral Mapping.&lt;BR /&gt;They are also defined in the SDK (v2.14.0; file "SDK_2_14_0_MIMXRT1170-EVK\devices\MIMXRT1176\MIMXRT1176_cm7.h", enum rdc_periph_t).&lt;BR /&gt;The two do not agree on a number of indices.&lt;BR /&gt;Below, I list the number (the index in the PDAP register array), then the peripheral indicated by the reference manual, then the peripheral indicated by the SDK; the unlisted values are consistent between RM and SDK.&lt;/P&gt;&lt;P&gt;0: Reserved / MTR&lt;BR /&gt;6: FLEXRAM / CM7_IMXRT&lt;BR /&gt;16: Reserved / TSC_DIG&lt;BR /&gt;60: DEC1 / ENC1&lt;BR /&gt;61: DEC2 / ENC2&lt;BR /&gt;62: DEC3 / ENC3&lt;BR /&gt;63: DEC4 / ENC4&lt;BR /&gt;111: XRDC2_MGR_D1 / SEMA1&lt;BR /&gt;114: ANALOG/ANADIG / ANATOP&lt;/P&gt;&lt;P&gt;What do these indices actually correspond to?&lt;/P&gt;&lt;P&gt;Also, what are MTR and TSC_DIG, which are never explained in the reference manual?&lt;/P&gt;</description>
    <pubDate>Fri, 08 Sep 2023 10:24:12 GMT</pubDate>
    <dc:creator>stefano-quantic</dc:creator>
    <dc:date>2023-09-08T10:24:12Z</dc:date>
    <item>
      <title>RDC: inconsistent values between SDK and manual</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RDC-inconsistent-values-between-SDK-and-manual/m-p/1719480#M212263</link>
      <description>&lt;P&gt;For iMXRT1176, the SDK and the reference manual do not agree about the RDC peripheral numbering.&lt;BR /&gt;RDC has 128 PDAP registers, each of which contains settings for a peripheral or group of peripherals.&lt;BR /&gt;The peripheral indices are specified in the reference manual (IMXRT1170RM Rev. 2, 06/2023), §42.5.2 Peripheral Mapping.&lt;BR /&gt;They are also defined in the SDK (v2.14.0; file "SDK_2_14_0_MIMXRT1170-EVK\devices\MIMXRT1176\MIMXRT1176_cm7.h", enum rdc_periph_t).&lt;BR /&gt;The two do not agree on a number of indices.&lt;BR /&gt;Below, I list the number (the index in the PDAP register array), then the peripheral indicated by the reference manual, then the peripheral indicated by the SDK; the unlisted values are consistent between RM and SDK.&lt;/P&gt;&lt;P&gt;0: Reserved / MTR&lt;BR /&gt;6: FLEXRAM / CM7_IMXRT&lt;BR /&gt;16: Reserved / TSC_DIG&lt;BR /&gt;60: DEC1 / ENC1&lt;BR /&gt;61: DEC2 / ENC2&lt;BR /&gt;62: DEC3 / ENC3&lt;BR /&gt;63: DEC4 / ENC4&lt;BR /&gt;111: XRDC2_MGR_D1 / SEMA1&lt;BR /&gt;114: ANALOG/ANADIG / ANATOP&lt;/P&gt;&lt;P&gt;What do these indices actually correspond to?&lt;/P&gt;&lt;P&gt;Also, what are MTR and TSC_DIG, which are never explained in the reference manual?&lt;/P&gt;</description>
      <pubDate>Fri, 08 Sep 2023 10:24:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RDC-inconsistent-values-between-SDK-and-manual/m-p/1719480#M212263</guid>
      <dc:creator>stefano-quantic</dc:creator>
      <dc:date>2023-09-08T10:24:12Z</dc:date>
    </item>
  </channel>
</rss>