<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: imx6q bmode usb</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6q-bmode-usb/m-p/1719028#M212216</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Could you share the uboot version that you are using?&lt;BR /&gt;Please note that this is enabled by default in our BSP&lt;BR /&gt;&lt;A href="https://github.com/nxp-imx/uboot-imx/blob/lf_v2022.04/configs/mx6dlsabresd_defconfig" target="_blank"&gt;https://github.com/nxp-imx/uboot-imx/blob/lf_v2022.04/configs/mx6dlsabresd_defconfig&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Also, please share how you are trying to connect by using UUU&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
    <pubDate>Thu, 07 Sep 2023 20:24:53 GMT</pubDate>
    <dc:creator>AldoG</dc:creator>
    <dc:date>2023-09-07T20:24:53Z</dc:date>
    <item>
      <title>imx6q bmode usb</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6q-bmode-usb/m-p/1718210#M212140</link>
      <description>&lt;P&gt;I have an imx6q-based board, and when running "bmode usb" with a micro-B cable plugged in, the board doesn't go into USB download mode. Instead, it just restarts normally and boots from MMC. Why would this happen?&lt;/P&gt;&lt;P&gt;P.S. There is a physical jumper that can put the board into download mode without issue, I am just tryting to do it from software. I can also run "sdp 0" to put the board into download mode, but then the uuu tool doesn't work.&lt;/P&gt;</description>
      <pubDate>Wed, 06 Sep 2023 18:48:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6q-bmode-usb/m-p/1718210#M212140</guid>
      <dc:creator>user123412</dc:creator>
      <dc:date>2023-09-06T18:48:38Z</dc:date>
    </item>
    <item>
      <title>Re: imx6q bmode usb</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6q-bmode-usb/m-p/1719028#M212216</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Could you share the uboot version that you are using?&lt;BR /&gt;Please note that this is enabled by default in our BSP&lt;BR /&gt;&lt;A href="https://github.com/nxp-imx/uboot-imx/blob/lf_v2022.04/configs/mx6dlsabresd_defconfig" target="_blank"&gt;https://github.com/nxp-imx/uboot-imx/blob/lf_v2022.04/configs/mx6dlsabresd_defconfig&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Also, please share how you are trying to connect by using UUU&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Thu, 07 Sep 2023 20:24:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6q-bmode-usb/m-p/1719028#M212216</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2023-09-07T20:24:53Z</dc:date>
    </item>
  </channel>
</rss>