<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックCoresight On-Chip Debugging i.MX 93 - Base Addresses</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Coresight-On-Chip-Debugging-i-MX-93-Base-Addresses/m-p/1718433#M212162</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;for a project I want to use on-chip debugging on my imx93 (EVK). For setting up the Coresight Access Library and accessing the tracing capabilities I need the addresses for the components like ETM, ETR, ETF,... Unfortunately I cannot find them in the official documentation. Also, I am not sure if I have to set the system in a debugging state before or how I would do that. As a sidenote: I want to do the tracing in the secure world of trustzone, do I need to do any additional configuration for that?&lt;/P&gt;&lt;P&gt;I would be very happy about any help&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;</description>
    <pubDate>Thu, 07 Sep 2023 06:03:37 GMT</pubDate>
    <dc:creator>silicolino</dc:creator>
    <dc:date>2023-09-07T06:03:37Z</dc:date>
    <item>
      <title>Coresight On-Chip Debugging i.MX 93 - Base Addresses</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Coresight-On-Chip-Debugging-i-MX-93-Base-Addresses/m-p/1718433#M212162</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;for a project I want to use on-chip debugging on my imx93 (EVK). For setting up the Coresight Access Library and accessing the tracing capabilities I need the addresses for the components like ETM, ETR, ETF,... Unfortunately I cannot find them in the official documentation. Also, I am not sure if I have to set the system in a debugging state before or how I would do that. As a sidenote: I want to do the tracing in the secure world of trustzone, do I need to do any additional configuration for that?&lt;/P&gt;&lt;P&gt;I would be very happy about any help&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;</description>
      <pubDate>Thu, 07 Sep 2023 06:03:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Coresight-On-Chip-Debugging-i-MX-93-Base-Addresses/m-p/1718433#M212162</guid>
      <dc:creator>silicolino</dc:creator>
      <dc:date>2023-09-07T06:03:37Z</dc:date>
    </item>
  </channel>
</rss>