<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: GStreamer gst-launch faces latency issues.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/GStreamer-gst-launch-faces-latency-issues/m-p/1717950#M212109</link>
    <description>&lt;P&gt;I'm just posting this here because I think it will be helpful to someone.&lt;BR /&gt;So, the issue was with the pipeline. When I changed the pipeline, the issue has been solved.&lt;BR /&gt;&lt;BR /&gt;The pipeline which worked is&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;gst-launch-1.0 filesrc location=&amp;lt;filename.mp4&amp;gt; ! qtdemux name=d d.video_0 ! queue ! h264parse ! v4l2h264dec ! imxvideoconvert_g2d ! queue ! waylandsink&lt;/P&gt;&lt;/BLOCKQUOTE&gt;</description>
    <pubDate>Wed, 06 Sep 2023 09:53:17 GMT</pubDate>
    <dc:creator>donjacobvellathottam</dc:creator>
    <dc:date>2023-09-06T09:53:17Z</dc:date>
    <item>
      <title>GStreamer gst-launch faces latency issues.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GStreamer-gst-launch-faces-latency-issues/m-p/1716203#M211928</link>
      <description>&lt;P&gt;I'm using an i.MX 8 board. I have tried to play a video file using gst-play-1.0, but the video playback is getting stuck at various points. below is the warning message shown:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;Redistribute latency...
Redistribute latency...
Redistribute latency...     
WARNING A lot of buffers are being dropped.
WARNING debug information: ../git/libs/gst/base/gstbasesink.c(3143): gst_base_sink_is_too_late (): /GstPlayBin:playbin/GstPlaySink:playsink/GstBin:vbin/GstWaylandSink:waylandsink0:&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using yocto builds to run the board. The issue with GStreamer is only faced in linux 5.15 and it works perfectly in linux 5.4&amp;nbsp;&lt;/P&gt;&lt;P&gt;But I need to implement it in 5.15 what may be the reason to this&lt;/P&gt;</description>
      <pubDate>Mon, 04 Sep 2023 05:47:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GStreamer-gst-launch-faces-latency-issues/m-p/1716203#M211928</guid>
      <dc:creator>donjacobvellathottam</dc:creator>
      <dc:date>2023-09-04T05:47:50Z</dc:date>
    </item>
    <item>
      <title>Re: GStreamer gst-launch faces latency issues.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GStreamer-gst-launch-faces-latency-issues/m-p/1717950#M212109</link>
      <description>&lt;P&gt;I'm just posting this here because I think it will be helpful to someone.&lt;BR /&gt;So, the issue was with the pipeline. When I changed the pipeline, the issue has been solved.&lt;BR /&gt;&lt;BR /&gt;The pipeline which worked is&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;gst-launch-1.0 filesrc location=&amp;lt;filename.mp4&amp;gt; ! qtdemux name=d d.video_0 ! queue ! h264parse ! v4l2h264dec ! imxvideoconvert_g2d ! queue ! waylandsink&lt;/P&gt;&lt;/BLOCKQUOTE&gt;</description>
      <pubDate>Wed, 06 Sep 2023 09:53:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GStreamer-gst-launch-faces-latency-issues/m-p/1717950#M212109</guid>
      <dc:creator>donjacobvellathottam</dc:creator>
      <dc:date>2023-09-06T09:53:17Z</dc:date>
    </item>
  </channel>
</rss>