<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 How can add ntp module</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-can-add-ntp-module/m-p/1717577#M212070</link>
    <description>&lt;P&gt;I want to synchronize time from ntp server.&lt;/P&gt;&lt;P&gt;So, when building yocto, I added ntpdate as shown below and built it, but an error occurred.&lt;/P&gt;&lt;P&gt;Also ntpd error.&lt;/P&gt;&lt;P&gt;How can I add ntp to rootfs?&lt;/P&gt;&lt;P&gt;1. Change local.conf file&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; IMAGE_INSTALL:append = " ntpdate"&lt;/P&gt;&lt;P&gt;2. Yocto version and build script&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; version : 6.1.22_2.0.0&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; build : bitbake -f core-image-base&lt;/P&gt;&lt;P&gt;3. error&amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;vrtrnd@vrtrnd-14ZD960-GX7BK:~/dscan3-yocto-bsp/build_dscan3$ bitbake -f core-image-base&lt;BR /&gt;Loading cache: 100% | | ETA: --:--:--&lt;BR /&gt;Loaded 0 entries from dependency cache.&lt;BR /&gt;Parsing recipes: 100% |##########################################| Time: 0:03:22&lt;BR /&gt;Parsing of 3444 .bb files complete (0 cached, 3444 parsed). 5307 targets, 593 skipped, 17 masked, 0 errors.&lt;BR /&gt;NOTE: Resolving any missing task queue dependencies&lt;BR /&gt;ERROR: Nothing RPROVIDES 'ntpdate' (but /home/vrtrnd/dscan3-yocto-bsp/sources/poky/meta/recipes-core/images/core-image-base.bb RDEPENDS on or otherwise requires it)&lt;BR /&gt;NOTE: Runtime target 'ntpdate' is unbuildable, removing...&lt;BR /&gt;Missing or unbuildable dependency chain was: ['ntpdate']&lt;BR /&gt;ERROR: Required build target 'core-image-base' has no buildable providers.&lt;BR /&gt;Missing or unbuildable dependency chain was: ['core-image-base', 'ntpdate']&lt;/P&gt;&lt;P&gt;Summary: There were 2 ERROR messages, returning a non-zero exit code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 06 Sep 2023 02:13:52 GMT</pubDate>
    <dc:creator>dskim2</dc:creator>
    <dc:date>2023-09-06T02:13:52Z</dc:date>
    <item>
      <title>How can add ntp module</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-can-add-ntp-module/m-p/1717577#M212070</link>
      <description>&lt;P&gt;I want to synchronize time from ntp server.&lt;/P&gt;&lt;P&gt;So, when building yocto, I added ntpdate as shown below and built it, but an error occurred.&lt;/P&gt;&lt;P&gt;Also ntpd error.&lt;/P&gt;&lt;P&gt;How can I add ntp to rootfs?&lt;/P&gt;&lt;P&gt;1. Change local.conf file&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; IMAGE_INSTALL:append = " ntpdate"&lt;/P&gt;&lt;P&gt;2. Yocto version and build script&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; version : 6.1.22_2.0.0&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; build : bitbake -f core-image-base&lt;/P&gt;&lt;P&gt;3. error&amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;vrtrnd@vrtrnd-14ZD960-GX7BK:~/dscan3-yocto-bsp/build_dscan3$ bitbake -f core-image-base&lt;BR /&gt;Loading cache: 100% | | ETA: --:--:--&lt;BR /&gt;Loaded 0 entries from dependency cache.&lt;BR /&gt;Parsing recipes: 100% |##########################################| Time: 0:03:22&lt;BR /&gt;Parsing of 3444 .bb files complete (0 cached, 3444 parsed). 5307 targets, 593 skipped, 17 masked, 0 errors.&lt;BR /&gt;NOTE: Resolving any missing task queue dependencies&lt;BR /&gt;ERROR: Nothing RPROVIDES 'ntpdate' (but /home/vrtrnd/dscan3-yocto-bsp/sources/poky/meta/recipes-core/images/core-image-base.bb RDEPENDS on or otherwise requires it)&lt;BR /&gt;NOTE: Runtime target 'ntpdate' is unbuildable, removing...&lt;BR /&gt;Missing or unbuildable dependency chain was: ['ntpdate']&lt;BR /&gt;ERROR: Required build target 'core-image-base' has no buildable providers.&lt;BR /&gt;Missing or unbuildable dependency chain was: ['core-image-base', 'ntpdate']&lt;/P&gt;&lt;P&gt;Summary: There were 2 ERROR messages, returning a non-zero exit code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 06 Sep 2023 02:13:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-can-add-ntp-module/m-p/1717577#M212070</guid>
      <dc:creator>dskim2</dc:creator>
      <dc:date>2023-09-06T02:13:52Z</dc:date>
    </item>
    <item>
      <title>Re: How can add ntp module</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-can-add-ntp-module/m-p/1718718#M212185</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/209213"&gt;@dskim2&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I think that the one for its recipe that you build should be ntp instead of ntpdate.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Thu, 07 Sep 2023 10:23:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-can-add-ntp-module/m-p/1718718#M212185</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2023-09-07T10:23:06Z</dc:date>
    </item>
    <item>
      <title>Re: How can add ntp module</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-can-add-ntp-module/m-p/1722577#M212570</link>
      <description>&lt;P&gt;I added ntp-utils and installed ntpdate.&lt;/P&gt;</description>
      <pubDate>Thu, 14 Sep 2023 00:00:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-can-add-ntp-module/m-p/1722577#M212570</guid>
      <dc:creator>dskim2</dc:creator>
      <dc:date>2023-09-14T00:00:06Z</dc:date>
    </item>
  </channel>
</rss>