<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Preempt-RT in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Preempt-RT/m-p/1716852#M212010</link>
    <description>&lt;P&gt;1)the owner doesn't update to the latest bsp version, maybe customer needs to change the new bsp source code according to the patches based on 4.1478&lt;/P&gt;
&lt;P&gt;2) refer to the readme, these patches are for kernel, customer just needs to change the kernel image, they just replace the new kernel image only&lt;/P&gt;</description>
    <pubDate>Tue, 05 Sep 2023 06:27:01 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2023-09-05T06:27:01Z</dc:date>
    <item>
      <title>Preempt-RT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Preempt-RT/m-p/1716097#M211919</link>
      <description>&lt;P&gt;1. I'm looking for the patches that 'Only' enables the "Preemt-RT" feature.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; refer to&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &lt;A href="https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/Enable-Linux-RT-PREEMPT-on-i-MX8M-Products/ta-p/1300117" target="_blank"&gt;https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/Enable-Linux-RT-PREEMPT-on-i-MX8M-Products/ta-p/1300117&lt;/A&gt;&lt;/P&gt;&lt;P&gt;But I don't know how get the patches for kernel 5.10.72 and 6.1.1x.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2.&amp;nbsp;&amp;nbsp;Per customer's request, we have to replace the original rootfs with other version.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; If we do so, will the "Preempt RT" feature keep available?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; (in other words, the preempt rt patches impact kernel image only or also including the roots?)&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 04 Sep 2023 01:32:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Preempt-RT/m-p/1716097#M211919</guid>
      <dc:creator>ChrisChang1234</dc:creator>
      <dc:date>2023-09-04T01:32:04Z</dc:date>
    </item>
    <item>
      <title>Re: Preempt-RT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Preempt-RT/m-p/1716852#M212010</link>
      <description>&lt;P&gt;1)the owner doesn't update to the latest bsp version, maybe customer needs to change the new bsp source code according to the patches based on 4.1478&lt;/P&gt;
&lt;P&gt;2) refer to the readme, these patches are for kernel, customer just needs to change the kernel image, they just replace the new kernel image only&lt;/P&gt;</description>
      <pubDate>Tue, 05 Sep 2023 06:27:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Preempt-RT/m-p/1716852#M212010</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-09-05T06:27:01Z</dc:date>
    </item>
    <item>
      <title>Re: Preempt-RT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Preempt-RT/m-p/1716931#M212026</link>
      <description>&lt;P&gt;Got it, thanks&lt;/P&gt;</description>
      <pubDate>Tue, 05 Sep 2023 07:47:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Preempt-RT/m-p/1716931#M212026</guid>
      <dc:creator>ChrisChang1234</dc:creator>
      <dc:date>2023-09-05T07:47:01Z</dc:date>
    </item>
  </channel>
</rss>