<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: kernel 6.4.8 infinite rootwait</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/kernel-6-4-8-infinite-rootwait/m-p/1716557#M211977</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You can check the 6.1v kernel BSP version since this is the latest official for MX6Q:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 04 Sep 2023 14:53:16 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2023-09-04T14:53:16Z</dc:date>
    <item>
      <title>kernel 6.4.8 infinite rootwait</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/kernel-6-4-8-infinite-rootwait/m-p/1716033#M211904</link>
      <description>&lt;P&gt;Hello, I'm updating the Linux kernel of an i.MX6Q-based SBC to kernel 6.4.8 (Debian distribution).&lt;BR /&gt;However, I'm encountering an infinite rootwait.&lt;BR /&gt;The SD card is not mounted in the /dev folder (I checked from the initramfs console).&lt;BR /&gt;I'm also seeing a lot of 'not linking [...] might never become dev' errors starting from 1.755544s. The errors are as follows:&lt;/P&gt;&lt;P&gt;[ 1.736203][ T1] /soc/bus@2000000/gpc@20dc000: Relaxing link with /soc/bus@2000000/clock-controller@20c4000&lt;BR /&gt;[ 1.746272][ T1] /soc/bus@2000000/gpc@20dc000: Relaxing link with /soc/interrupt-controller@a01000&lt;BR /&gt;[ 1.755544][ T1] /soc: Relaxing link with /soc/bus@2000000/gpc@20dc000&lt;/P&gt;&lt;P&gt;I think it's a DTS/DTB problem, but I haven't found anything specific yet...&lt;/P&gt;&lt;P&gt;Please find below/in attachement :&lt;BR /&gt;- the boot logs&lt;BR /&gt;- kernel .config file&lt;BR /&gt;- dts, dtsi files&lt;BR /&gt;&lt;BR /&gt;Thank you for your time,&lt;BR /&gt;&lt;BR /&gt;Cécile Janin&lt;/P&gt;</description>
      <pubDate>Sat, 02 Sep 2023 11:09:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/kernel-6-4-8-infinite-rootwait/m-p/1716033#M211904</guid>
      <dc:creator>Cécile</dc:creator>
      <dc:date>2023-09-02T11:09:26Z</dc:date>
    </item>
    <item>
      <title>Re: kernel 6.4.8 infinite rootwait</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/kernel-6-4-8-infinite-rootwait/m-p/1716557#M211977</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You can check the 6.1v kernel BSP version since this is the latest official for MX6Q:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 04 Sep 2023 14:53:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/kernel-6-4-8-infinite-rootwait/m-p/1716557#M211977</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2023-09-04T14:53:16Z</dc:date>
    </item>
    <item>
      <title>Re: kernel 6.4.8 infinite rootwait</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/kernel-6-4-8-infinite-rootwait/m-p/1717350#M212058</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;To be sure:&lt;BR /&gt;Can I compile a kernel for imx6 only with the code downloaded from kernel.org ? Or should I add non-free binaries?&lt;/P&gt;</description>
      <pubDate>Tue, 05 Sep 2023 17:06:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/kernel-6-4-8-infinite-rootwait/m-p/1717350#M212058</guid>
      <dc:creator>Cécile</dc:creator>
      <dc:date>2023-09-05T17:06:34Z</dc:date>
    </item>
  </channel>
</rss>