<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: MIMXRT1176AVM8A  RGB(R0,R1....R7-G0,G1......) equivalents of GPIO_DISP pins</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1176AVM8A-RGB-R0-R1-R7-G0-G1-equivalents-of-GPIO-DISP-pins/m-p/1716528#M211973</link>
    <description>&lt;P&gt;Hİ&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186731"&gt;@EdwinHz&lt;/a&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186731"&gt;@EdwinHz&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There was no information about this in the datasheet. We connected it directly. (We are not sure any shift each pins?)&lt;/P&gt;&lt;P&gt;Is the link in the picture suitable for 24-bit use?Is that true?&lt;/P&gt;&lt;P&gt;thank you&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 04 Sep 2023 13:39:57 GMT</pubDate>
    <dc:creator>EMertCakir</dc:creator>
    <dc:date>2023-09-04T13:39:57Z</dc:date>
    <item>
      <title>MIMXRT1176AVM8A  RGB(R0,R1....R7-G0,G1......) equivalents of GPIO_DISP pins</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1176AVM8A-RGB-R0-R1-R7-G0-G1-equivalents-of-GPIO-DISP-pins/m-p/1705589#M210890</link>
      <description>&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;I connected display data to GPIO_DISP_B1_XX and GPIO_DISP_B2_XX pins. I read manuel that I have to connect data 0 to GPIO_DISP_B1_04, but is it GPIO_DISP_B1_04&amp;nbsp; &amp;nbsp; R0 ? Im not sure that.&amp;nbsp; R0...R7 ,B0...B7,G0....G7 should I connect the data of GPIO_DISP_B1_XX to these pins in order. Is there a document about this subject? Thank you&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 16 Aug 2023 08:34:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1176AVM8A-RGB-R0-R1-R7-G0-G1-equivalents-of-GPIO-DISP-pins/m-p/1705589#M210890</guid>
      <dc:creator>EMertCakir</dc:creator>
      <dc:date>2023-08-16T08:34:26Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1176AVM8A  RGB(R0,R1....R7-G0,G1......) equivalents of GPIO_DISP pins</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1176AVM8A-RGB-R0-R1-R7-G0-G1-equivalents-of-GPIO-DISP-pins/m-p/1705991#M210933</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/221526"&gt;@EMertCakir&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Please look into the following application note (&lt;A href="https://www.nxp.com/docs/en/application-note/AN12302.pdf" target="_blank"&gt;AN12302&lt;/A&gt;), specifically "Figure 6. 24-bit RGB888 eLCDIF interface to 18bpp LCD panel". I believe it will prove very useful for your inquiry.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Wed, 16 Aug 2023 18:55:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1176AVM8A-RGB-R0-R1-R7-G0-G1-equivalents-of-GPIO-DISP-pins/m-p/1705991#M210933</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2023-08-16T18:55:46Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1176AVM8A  RGB(R0,R1....R7-G0,G1......) equivalents of GPIO_DISP pins</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1176AVM8A-RGB-R0-R1-R7-G0-G1-equivalents-of-GPIO-DISP-pins/m-p/1706542#M210988</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186731"&gt;@EdwinHz&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is the meaning of pins D17,D16,D9,D8,D0,D1 in Table 6?&lt;BR /&gt;Where do I connect the R6,7-G6,7-B6,7 pins to?&lt;/P&gt;</description>
      <pubDate>Thu, 17 Aug 2023 10:17:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1176AVM8A-RGB-R0-R1-R7-G0-G1-equivalents-of-GPIO-DISP-pins/m-p/1706542#M210988</guid>
      <dc:creator>EMertCakir</dc:creator>
      <dc:date>2023-08-17T10:17:42Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1176AVM8A  RGB(R0,R1....R7-G0,G1......) equivalents of GPIO_DISP pins</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1176AVM8A-RGB-R0-R1-R7-G0-G1-equivalents-of-GPIO-DISP-pins/m-p/1706941#M211013</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/221526"&gt;@EMertCakir&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Table 6 shows the connection of a 18 bit per pixel LCD. In that case,&amp;nbsp;&lt;SPAN&gt;pins D17, D16, D9, D8, D1 and D0 end up being left over.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;From what you mention, I believe you are using 24bpp, so the RGB connections would equate to the values shown on "Figure 1. Data for 1 pixel" (D7-0 Blue, D15-8 Green, D23-16 Red):&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="EdwinHz_0-1692300772914.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/236943iD49DBC6105F5A24D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="EdwinHz_0-1692300772914.png" alt="EdwinHz_0-1692300772914.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Thu, 17 Aug 2023 19:33:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1176AVM8A-RGB-R0-R1-R7-G0-G1-equivalents-of-GPIO-DISP-pins/m-p/1706941#M211013</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2023-08-17T19:33:45Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1176AVM8A  RGB(R0,R1....R7-G0,G1......) equivalents of GPIO_DISP pins</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1176AVM8A-RGB-R0-R1-R7-G0-G1-equivalents-of-GPIO-DISP-pins/m-p/1708145#M211127</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186731"&gt;@EdwinHz&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There was no information about this in the datasheet. We connected it directly. (We are not sure any shift each pins?)&lt;/P&gt;&lt;P&gt;Is the link in the picture suitable for 24-bit use?Is that true?&lt;/P&gt;&lt;P&gt;thank you&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Aug 2023 07:43:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1176AVM8A-RGB-R0-R1-R7-G0-G1-equivalents-of-GPIO-DISP-pins/m-p/1708145#M211127</guid>
      <dc:creator>EMertCakir</dc:creator>
      <dc:date>2023-08-21T07:43:50Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1176AVM8A  RGB(R0,R1....R7-G0,G1......) equivalents of GPIO_DISP pins</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1176AVM8A-RGB-R0-R1-R7-G0-G1-equivalents-of-GPIO-DISP-pins/m-p/1716528#M211973</link>
      <description>&lt;P&gt;Hİ&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186731"&gt;@EdwinHz&lt;/a&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186731"&gt;@EdwinHz&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There was no information about this in the datasheet. We connected it directly. (We are not sure any shift each pins?)&lt;/P&gt;&lt;P&gt;Is the link in the picture suitable for 24-bit use?Is that true?&lt;/P&gt;&lt;P&gt;thank you&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 04 Sep 2023 13:39:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1176AVM8A-RGB-R0-R1-R7-G0-G1-equivalents-of-GPIO-DISP-pins/m-p/1716528#M211973</guid>
      <dc:creator>EMertCakir</dc:creator>
      <dc:date>2023-09-04T13:39:57Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1176AVM8A  RGB(R0,R1....R7-G0,G1......) equivalents of GPIO_DISP pins</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1176AVM8A-RGB-R0-R1-R7-G0-G1-equivalents-of-GPIO-DISP-pins/m-p/1716529#M211974</link>
      <description>There was no information about this in the datasheet. We connected it directly. (We are not sure any shift each pins?)&lt;BR /&gt;&lt;BR /&gt;Is the link in the picture suitable for 24-bit use?Is that true?&lt;BR /&gt;&lt;BR /&gt;thank you</description>
      <pubDate>Mon, 04 Sep 2023 13:40:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1176AVM8A-RGB-R0-R1-R7-G0-G1-equivalents-of-GPIO-DISP-pins/m-p/1716529#M211974</guid>
      <dc:creator>EMertCakir</dc:creator>
      <dc:date>2023-09-04T13:40:43Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1176AVM8A  RGB(R0,R1....R7-G0,G1......) equivalents of GPIO_DISP pins</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1176AVM8A-RGB-R0-R1-R7-G0-G1-equivalents-of-GPIO-DISP-pins/m-p/1716599#M211982</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/221526"&gt;@EMertCakir&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Sorry for the delayed response. Yes, the image shown is suitable for 24-bit use. If your application follows this scheme, you can follow this image.&lt;/P&gt;&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Mon, 04 Sep 2023 16:42:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1176AVM8A-RGB-R0-R1-R7-G0-G1-equivalents-of-GPIO-DISP-pins/m-p/1716599#M211982</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2023-09-04T16:42:03Z</dc:date>
    </item>
  </channel>
</rss>