<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックiMX8 boot kernel from micro-sd having SDIO WP enabled</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8-boot-kernel-from-micro-sd-having-SDIO-WP-enabled/m-p/1716077#M211911</link>
    <description>&lt;P&gt;The boot from micro-sd having SDIO WP signal enabled hangs with error -30 "/dev/root: Can't open blockdev "&lt;/P&gt;&lt;P&gt;Why it is not possible to mount the root device with the write protection?&lt;/P&gt;&lt;P&gt;is there a work around? like enabling the "wp-gpios" after the boot?&lt;/P&gt;</description>
    <pubDate>Sun, 03 Sep 2023 20:20:49 GMT</pubDate>
    <dc:creator>Joomar</dc:creator>
    <dc:date>2023-09-03T20:20:49Z</dc:date>
    <item>
      <title>iMX8 boot kernel from micro-sd having SDIO WP enabled</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8-boot-kernel-from-micro-sd-having-SDIO-WP-enabled/m-p/1716077#M211911</link>
      <description>&lt;P&gt;The boot from micro-sd having SDIO WP signal enabled hangs with error -30 "/dev/root: Can't open blockdev "&lt;/P&gt;&lt;P&gt;Why it is not possible to mount the root device with the write protection?&lt;/P&gt;&lt;P&gt;is there a work around? like enabling the "wp-gpios" after the boot?&lt;/P&gt;</description>
      <pubDate>Sun, 03 Sep 2023 20:20:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8-boot-kernel-from-micro-sd-having-SDIO-WP-enabled/m-p/1716077#M211911</guid>
      <dc:creator>Joomar</dc:creator>
      <dc:date>2023-09-03T20:20:49Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8 boot kernel from micro-sd having SDIO WP enabled</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8-boot-kernel-from-micro-sd-having-SDIO-WP-enabled/m-p/1716567#M211979</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The kernel is protected so, the SD WP need to be non-write enable to work with it.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Mon, 04 Sep 2023 15:00:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8-boot-kernel-from-micro-sd-having-SDIO-WP-enabled/m-p/1716567#M211979</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2023-09-04T15:00:29Z</dc:date>
    </item>
  </channel>
</rss>