<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.mx93. Using parallel camera and display interface in one device simultaneously. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx93-Using-parallel-camera-and-display-interface-in-one-device/m-p/1715103#M211807</link>
    <description>&lt;P&gt;Hello, &lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I want to use i.mx93 series processor (&lt;SPAN class=""&gt;MIMX9352CVUXMAA&lt;/SPAN&gt;).&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I want to connect a camera to it via a parallel 8-bit interface and a display via a parallel 24-bit interface.&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN class=""&gt;&lt;SPAN class=""&gt;There was a problem that the processor pins used for the display and the camera intersect (example: Pin J21 using for cam_clk and for disp_clk).&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Whether correctly I understand, what at the same time these two interfaces cannot be used?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Is there some way around this problem?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;For example, remap display or camera pins to other pins?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 31 Aug 2023 13:21:34 GMT</pubDate>
    <dc:creator>Serg_mx6</dc:creator>
    <dc:date>2023-08-31T13:21:34Z</dc:date>
    <item>
      <title>i.mx93. Using parallel camera and display interface in one device simultaneously.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx93-Using-parallel-camera-and-display-interface-in-one-device/m-p/1715103#M211807</link>
      <description>&lt;P&gt;Hello, &lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I want to use i.mx93 series processor (&lt;SPAN class=""&gt;MIMX9352CVUXMAA&lt;/SPAN&gt;).&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I want to connect a camera to it via a parallel 8-bit interface and a display via a parallel 24-bit interface.&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN class=""&gt;&lt;SPAN class=""&gt;There was a problem that the processor pins used for the display and the camera intersect (example: Pin J21 using for cam_clk and for disp_clk).&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Whether correctly I understand, what at the same time these two interfaces cannot be used?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Is there some way around this problem?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;For example, remap display or camera pins to other pins?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 31 Aug 2023 13:21:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx93-Using-parallel-camera-and-display-interface-in-one-device/m-p/1715103#M211807</guid>
      <dc:creator>Serg_mx6</dc:creator>
      <dc:date>2023-08-31T13:21:34Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx93. Using parallel camera and display interface in one device simultaneously.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx93-Using-parallel-camera-and-display-interface-in-one-device/m-p/1715386#M211832</link>
      <description>&lt;P&gt;Hello, I hope you are doing well.&lt;/P&gt;
&lt;P&gt;The IOMUX and Pad Control Registers are able to change function of the pin and re-map them to another. For this particular case, MEDIAMIX_CAM_CLK and MEDIAMIX_DISP_CLK functions are only mapped to J21 pin.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Thu, 31 Aug 2023 21:47:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx93-Using-parallel-camera-and-display-interface-in-one-device/m-p/1715386#M211832</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2023-08-31T21:47:11Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx93. Using parallel camera and display interface in one device simultaneously.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx93-Using-parallel-camera-and-display-interface-in-one-device/m-p/1885738#M224846</link>
      <description>&lt;P&gt;Can anyone confirm still&amp;nbsp;&lt;STRONG&gt;MIMX9352CVUXMAA is this part number available in NXP, Digikey, Mouser and Arrow?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jun 2024 04:54:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx93-Using-parallel-camera-and-display-interface-in-one-device/m-p/1885738#M224846</guid>
      <dc:creator>rameshasp</dc:creator>
      <dc:date>2024-06-12T04:54:05Z</dc:date>
    </item>
  </channel>
</rss>