<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMXRT1176 - Slew rate and drive strength on SNVS pins in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMXRT1176-Slew-rate-and-drive-strength-on-SNVS-pins/m-p/1714179#M211760</link>
    <description>&lt;P class="lia-align-justify"&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/219981"&gt;@stefano-quantic&lt;/a&gt;,&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;First of all, we apologize for our delay.&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P class="lia-align-justify"&gt;&lt;EM&gt;Is it supported or not?&lt;/EM&gt;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P class="lia-align-justify"&gt;They&lt;EM&gt; are analog IO with limited function, and they do not support slew rate or drive strength configuration.&lt;/EM&gt;&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;The tool is going to be updated. Thanks for the feedback.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Best regards, Raul.&lt;/P&gt;</description>
    <pubDate>Wed, 30 Aug 2023 17:22:57 GMT</pubDate>
    <dc:creator>RaRo</dc:creator>
    <dc:date>2023-08-30T17:22:57Z</dc:date>
    <item>
      <title>iMXRT1176 - Slew rate and drive strength on SNVS pins</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMXRT1176-Slew-rate-and-drive-strength-on-SNVS-pins/m-p/1697661#M210139</link>
      <description>&lt;P&gt;The reference manual v2 (06/2023) says that SNVS pins do not have a slew rate option.&lt;BR /&gt;See section "12.4.2.21 SW_PAD_CTL_PAD_GPIO_SNVS_00_DIG SW PAD Control Register (SW_PAD_CTL_PAD_GPIO_SNVS_00_DIG)" and following.&lt;BR /&gt;Bit #0 is marked as "reserved" in this register.&lt;BR /&gt;For other pins, this bit is used for the slew rate setting SRE (e.g. see section "12.4.6.210 SW_PAD_CTL_PAD_GPIO_AD_00 SW PAD Control Register (SW_PAD_CTL_PAD_GPIO_AD_00)").&lt;/P&gt;&lt;P&gt;However, Config Tools let me select the slew rate for the SNVS pins too.&lt;/P&gt;&lt;P&gt;So, is the slew rate setting available on the SNVS pins?&lt;/P&gt;&lt;P&gt;Similarly for other pins whose registers are described in nearby sections:&lt;BR /&gt;SW_PAD_CTL_PAD_TEST_MODE_DIG&lt;BR /&gt;SW_PAD_CTL_PAD_POR_B_DIG&lt;BR /&gt;SW_PAD_CTL_PAD_ONOFF_DIG&lt;BR /&gt;SW_PAD_CTL_PAD_WAKEUP_DIG&lt;BR /&gt;SW_PAD_CTL_PAD_PMIC_ON_REQ_DIG&lt;BR /&gt;SW_PAD_CTL_PAD_PMIC_STBY_REQ_DIG&lt;/P&gt;&lt;P&gt;The same for the adjacent bit DSE (#1), for the drive strength: it's marked as reserved in the reference manual, but Config Tools let me configure it.&lt;/P&gt;&lt;P&gt;Is it supported or not?&lt;/P&gt;</description>
      <pubDate>Wed, 02 Aug 2023 13:15:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMXRT1176-Slew-rate-and-drive-strength-on-SNVS-pins/m-p/1697661#M210139</guid>
      <dc:creator>stefano-quantic</dc:creator>
      <dc:date>2023-08-02T13:15:34Z</dc:date>
    </item>
    <item>
      <title>Re: iMXRT1176 - Slew rate and drive strength on SNVS pins</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMXRT1176-Slew-rate-and-drive-strength-on-SNVS-pins/m-p/1698906#M210253</link>
      <description>&lt;P class="lia-align-justify"&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/219981"&gt;@stefano-quantic&lt;/a&gt;,&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Let us double check if DSE and SRE are not being supported in SNVS, PMIC, POR, ONOFF and WAKEUP as i.MX RT1170 Processor Reference Manual mentions to give you a proper answer.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;At the meantime, we are letting the team in charge to know about this.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Best regards, Raul.&lt;/P&gt;</description>
      <pubDate>Thu, 03 Aug 2023 21:43:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMXRT1176-Slew-rate-and-drive-strength-on-SNVS-pins/m-p/1698906#M210253</guid>
      <dc:creator>RaRo</dc:creator>
      <dc:date>2023-08-03T21:43:09Z</dc:date>
    </item>
    <item>
      <title>Re: iMXRT1176 - Slew rate and drive strength on SNVS pins</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMXRT1176-Slew-rate-and-drive-strength-on-SNVS-pins/m-p/1714179#M211760</link>
      <description>&lt;P class="lia-align-justify"&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/219981"&gt;@stefano-quantic&lt;/a&gt;,&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;First of all, we apologize for our delay.&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P class="lia-align-justify"&gt;&lt;EM&gt;Is it supported or not?&lt;/EM&gt;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P class="lia-align-justify"&gt;They&lt;EM&gt; are analog IO with limited function, and they do not support slew rate or drive strength configuration.&lt;/EM&gt;&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;The tool is going to be updated. Thanks for the feedback.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Best regards, Raul.&lt;/P&gt;</description>
      <pubDate>Wed, 30 Aug 2023 17:22:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMXRT1176-Slew-rate-and-drive-strength-on-SNVS-pins/m-p/1714179#M211760</guid>
      <dc:creator>RaRo</dc:creator>
      <dc:date>2023-08-30T17:22:57Z</dc:date>
    </item>
  </channel>
</rss>