<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: QSPI Flash through Flex SPI1 Interface using MIMXRT1176DVMAA</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/QSPI-Flash-through-Flex-SPI1-Interface-using-MIMXRT1176DVMAA/m-p/1711900#M211522</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/211253"&gt;@972794&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;You can refer to the MIMXRT1170-EVK QSPI flash design, the flexspi DQS pin should be float.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; Then, you can use the SDK code:&lt;/P&gt;
&lt;P&gt;\SDK_2_14_0_MIMXRT1170-EVK\boards\evkmimxrt1170\driver_examples\flexspi\nor\polling_transfer&lt;/P&gt;
&lt;P&gt;run it in internal RAM to test the QSPI flash communication, you need to enable the quad mode if you use the quad communication, so please run the above code to enable QE, check the erase, program, and read.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Wish it helps you!&lt;BR /&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 28 Aug 2023 04:53:02 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2023-08-28T04:53:02Z</dc:date>
    <item>
      <title>QSPI Flash through Flex SPI1 Interface using MIMXRT1176DVMAA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/QSPI-Flash-through-Flex-SPI1-Interface-using-MIMXRT1176DVMAA/m-p/1709731#M211279</link>
      <description>&lt;P&gt;I am using&amp;nbsp;MIMXRT1176CVM8A&amp;nbsp; and QSPI flash(IS25WP128-JKLE-TR) in our application&amp;nbsp;&lt;/P&gt;&lt;P&gt;We have issue with flashing we are able to send the data from processor but QSPI is not sending the information to the processor(MISO pin its loading) what could be issue&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 23 Aug 2023 08:50:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/QSPI-Flash-through-Flex-SPI1-Interface-using-MIMXRT1176DVMAA/m-p/1709731#M211279</guid>
      <dc:creator>972794</dc:creator>
      <dc:date>2023-08-23T08:50:43Z</dc:date>
    </item>
    <item>
      <title>Re: QSPI Flash through Flex SPI1 Interface using MIMXRT1176DVMAA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/QSPI-Flash-through-Flex-SPI1-Interface-using-MIMXRT1176DVMAA/m-p/1710677#M211367</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Check the wiring and connections between the processor and the QSPI flash. Make sure that the MISO pin is correctly connected.&lt;/P&gt;&lt;P&gt;Verify the configuration of the Flex SPI1 interface. Ensure that it's correctly set up to communicate with the QSPI flash.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 24 Aug 2023 11:44:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/QSPI-Flash-through-Flex-SPI1-Interface-using-MIMXRT1176DVMAA/m-p/1710677#M211367</guid>
      <dc:creator>ramprakash09</dc:creator>
      <dc:date>2023-08-24T11:44:57Z</dc:date>
    </item>
    <item>
      <title>Re: QSPI Flash through Flex SPI1 Interface using MIMXRT1176DVMAA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/QSPI-Flash-through-Flex-SPI1-Interface-using-MIMXRT1176DVMAA/m-p/1711900#M211522</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/211253"&gt;@972794&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;You can refer to the MIMXRT1170-EVK QSPI flash design, the flexspi DQS pin should be float.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; Then, you can use the SDK code:&lt;/P&gt;
&lt;P&gt;\SDK_2_14_0_MIMXRT1170-EVK\boards\evkmimxrt1170\driver_examples\flexspi\nor\polling_transfer&lt;/P&gt;
&lt;P&gt;run it in internal RAM to test the QSPI flash communication, you need to enable the quad mode if you use the quad communication, so please run the above code to enable QE, check the erase, program, and read.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Wish it helps you!&lt;BR /&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 28 Aug 2023 04:53:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/QSPI-Flash-through-Flex-SPI1-Interface-using-MIMXRT1176DVMAA/m-p/1711900#M211522</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2023-08-28T04:53:02Z</dc:date>
    </item>
  </channel>
</rss>