<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx8mp u-boot failed to run</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-u-boot-failed-to-run/m-p/1711791#M211497</link>
    <description>&lt;P&gt;Thank you&amp;nbsp;&lt;/P&gt;&lt;P&gt;I write&amp;nbsp;imx8mp-evk-revb4.dtb to board and&amp;nbsp;solved the problem.&lt;/P&gt;&lt;P&gt;The board does not have a multimedia device.&lt;/P&gt;&lt;P&gt;How can I run the board without imx8mp-evk-revb.dtb?&lt;/P&gt;</description>
    <pubDate>Mon, 28 Aug 2023 00:38:28 GMT</pubDate>
    <dc:creator>dskim2</dc:creator>
    <dc:date>2023-08-28T00:38:28Z</dc:date>
    <item>
      <title>imx8mp u-boot failed to run</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-u-boot-failed-to-run/m-p/1709830#M211287</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi! I make a custom board with iMX8MP and compile u-boot with yocto&amp;nbsp;6.1.22_2.0.0.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;but u-boot failed to run&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;How can I fixed it&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;This board is ok at yocto 5.10.72.2.2.0.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;below is board's log&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2023.04-lf_v2023.04+gaf7d004eaf (Jun 06 2023 - 14:59:40 +0000)&lt;/P&gt;&lt;P&gt;CPU: i.MX8MP[8] rev1.1 1600 MHz (running at 1200 MHz)&lt;BR /&gt;CPU: Industrial temperature grade (-40C to 105C) at 76C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: NXP i.MX8MPlus LPDDR4 EVK board&lt;BR /&gt;DRAM: 2 GiB&lt;BR /&gt;tcpc_init: Can't find bus&lt;BR /&gt;setup_typec: tcpc port2 init failed, err=-22&lt;BR /&gt;setup_pd_switch: Can't find device id=0x72&lt;BR /&gt;TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]&lt;BR /&gt;Core: 240 devices, 30 uclasses, devicetree: separate&lt;BR /&gt;MMC: FSL_SDHC: 1, FSL_SDHC: 2&lt;BR /&gt;Loading Environment from MMC... *** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;Fail to setup video link&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;SEC0: RNG instantiated&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc2(part 0) is current device&lt;BR /&gt;flash target is MMC:2&lt;BR /&gt;Net:&lt;BR /&gt;Warning: ethernet@30bf0000 (eth1) using random MAC address - 16:2a:a6:9c:df:15&lt;/P&gt;&lt;P&gt;Warning: ethernet@30be0000 (eth0) using random MAC address - b2:90:5b:8f:fb:ec&lt;BR /&gt;eth0: ethernet@30be0000, eth1: ethernet@30bf0000 [PRIME]&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 2 1 0&lt;BR /&gt;Working FDT set to 43000000&lt;BR /&gt;libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND&lt;BR /&gt;libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND&lt;BR /&gt;libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND&lt;BR /&gt;libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND&lt;BR /&gt;libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND&lt;BR /&gt;libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND&lt;BR /&gt;libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND&lt;BR /&gt;starting USB...&lt;BR /&gt;Bus usb@38100000: Failed to initialize board for imx8m USB&lt;BR /&gt;probe failed, error -1&lt;BR /&gt;Bus usb@38200000: Register 2000140 NbrPorts 2&lt;BR /&gt;Starting the controller&lt;BR /&gt;USB XHCI 1.10&lt;BR /&gt;scanning bus usb@38200000 for devices... 1 USB Device(s) found&lt;BR /&gt;scanning usb for storage devices... 0 Storage Device(s) found&lt;/P&gt;&lt;P&gt;Device 0: unknown device&lt;BR /&gt;MMC: no card present&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc2(part 0) is current device&lt;BR /&gt;Scanning mmc 2:1...&lt;BR /&gt;Working FDT set to 43000000&lt;BR /&gt;MMC: no card present&lt;BR /&gt;Unable to open OP-TEE session (err=-5)&lt;BR /&gt;mm_communicate failed!&lt;BR /&gt;Error: Cannot initialize UEFI sub-system, r = 3&lt;BR /&gt;Running BSP bootcmd ...&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc2(part 0) is current device&lt;BR /&gt;Failed to load 'boot.scr'&lt;BR /&gt;32121344 bytes read in 230 ms (133.2 MiB/s)&lt;BR /&gt;Booting from mmc ...&lt;BR /&gt;Failed to load 'imx8mp-evk-revb4.dtb'&lt;BR /&gt;WARN: Cannot load the DT&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 23 Aug 2023 10:27:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-u-boot-failed-to-run/m-p/1709830#M211287</guid>
      <dc:creator>dskim2</dc:creator>
      <dc:date>2023-08-23T10:27:31Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mp u-boot failed to run</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-u-boot-failed-to-run/m-p/1711220#M211429</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/209213"&gt;@dskim2&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;lt;Failed to load 'imx8mp-evk-revb4.dtb'&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WARN: Cannot load the DT&amp;gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Suggest to check the dtb files.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Fri, 25 Aug 2023 06:33:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-u-boot-failed-to-run/m-p/1711220#M211429</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2023-08-25T06:33:45Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mp u-boot failed to run</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-u-boot-failed-to-run/m-p/1711791#M211497</link>
      <description>&lt;P&gt;Thank you&amp;nbsp;&lt;/P&gt;&lt;P&gt;I write&amp;nbsp;imx8mp-evk-revb4.dtb to board and&amp;nbsp;solved the problem.&lt;/P&gt;&lt;P&gt;The board does not have a multimedia device.&lt;/P&gt;&lt;P&gt;How can I run the board without imx8mp-evk-revb.dtb?&lt;/P&gt;</description>
      <pubDate>Mon, 28 Aug 2023 00:38:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-u-boot-failed-to-run/m-p/1711791#M211497</guid>
      <dc:creator>dskim2</dc:creator>
      <dc:date>2023-08-28T00:38:28Z</dc:date>
    </item>
  </channel>
</rss>