<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックQueries regarding IMX233</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Queries-regarding-IMX233/m-p/244889#M21136</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We need to understand the following few things for choosing the right IC for reset. &lt;/P&gt;&lt;P&gt;1)We have two sources for input power to processor. one is 5V input from wall adapter or USB interface and second one is Li-ion battery.&lt;/P&gt;&lt;P&gt;Li-ion battery is charged from processor so if we need to charge the battery processor should be up and not in reset.&lt;/P&gt;&lt;P&gt;As we have two power sources 5V (at 4.3V) and battery (at 3.2V) which have different brownout so we need to take care both situations.&lt;/P&gt;&lt;P&gt;Case 1: when 5V is applied and battery voltage is above 3.2V:&amp;nbsp; No need to reset the processor as processor has sufficient input voltage from battery.&lt;/P&gt;&lt;P&gt;Case 2: when 5V is applied but battery voltage is less than 3.2V:&amp;nbsp; As battery voltage was low than threshold and reset need to be provided fro 5V source.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2)We also need to know if we need to physically disconnect the battery in case battery voltage goes below threshold and at what voltage.&lt;/P&gt;&lt;P&gt;3)what to do with the battery in case battery voltage goes below the threshold voltage ( if we need to disconnect it ). We can also discuss with him for probable battery disconnection circuit if it needed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Jyothi&lt;/P&gt;&lt;P&gt;HCI Technocrats&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 Sep 2013 06:49:55 GMT</pubDate>
    <dc:creator>veeramallajyoth</dc:creator>
    <dc:date>2013-09-23T06:49:55Z</dc:date>
    <item>
      <title>Queries regarding IMX233</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Queries-regarding-IMX233/m-p/244889#M21136</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We need to understand the following few things for choosing the right IC for reset. &lt;/P&gt;&lt;P&gt;1)We have two sources for input power to processor. one is 5V input from wall adapter or USB interface and second one is Li-ion battery.&lt;/P&gt;&lt;P&gt;Li-ion battery is charged from processor so if we need to charge the battery processor should be up and not in reset.&lt;/P&gt;&lt;P&gt;As we have two power sources 5V (at 4.3V) and battery (at 3.2V) which have different brownout so we need to take care both situations.&lt;/P&gt;&lt;P&gt;Case 1: when 5V is applied and battery voltage is above 3.2V:&amp;nbsp; No need to reset the processor as processor has sufficient input voltage from battery.&lt;/P&gt;&lt;P&gt;Case 2: when 5V is applied but battery voltage is less than 3.2V:&amp;nbsp; As battery voltage was low than threshold and reset need to be provided fro 5V source.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2)We also need to know if we need to physically disconnect the battery in case battery voltage goes below threshold and at what voltage.&lt;/P&gt;&lt;P&gt;3)what to do with the battery in case battery voltage goes below the threshold voltage ( if we need to disconnect it ). We can also discuss with him for probable battery disconnection circuit if it needed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Jyothi&lt;/P&gt;&lt;P&gt;HCI Technocrats&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Sep 2013 06:49:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Queries-regarding-IMX233/m-p/244889#M21136</guid>
      <dc:creator>veeramallajyoth</dc:creator>
      <dc:date>2013-09-23T06:49:55Z</dc:date>
    </item>
    <item>
      <title>Re: Queries regarding IMX233</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Queries-regarding-IMX233/m-p/244890#M21137</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Jyothi&lt;/SPAN&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;unfortunately I do not really know whats your question. Could you please rewrite your text using a interrogative form?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I try to give some answers by guessing the questions ;-)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Your system must be up and running to charge the battery.&lt;/P&gt;&lt;P&gt;- I see no need to &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;physically disconnect the battery. Could you please explain why you want to do this?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;There is a lot of battery/charger source code within the iMX233 Linux bootlets covering VBUSVALID detection, charging, linear regulators, 4P2, ect. In combination with the reference manual it will provide a great resource of information.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Kind regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Mike&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Sep 2013 08:08:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Queries-regarding-IMX233/m-p/244890#M21137</guid>
      <dc:creator>mbergmann</dc:creator>
      <dc:date>2013-09-23T08:08:22Z</dc:date>
    </item>
  </channel>
</rss>