<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Custom rules under /etc/udev/rules.d are not taking effect in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Custom-rules-under-etc-udev-rules-d-are-not-taking-effect/m-p/1710574#M211351</link>
    <description>&lt;P&gt;&lt;SPAN&gt;I have created a rule named "99-usb-mount.rules" in the rules.d directory, but it doesn't trigger the script. How can I resolve this issue?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;This is the rules：&lt;BR /&gt;ACTION=="add", SUBSYSTEM=="block", KERNEL=="sda1", RUN+="/bin/bash /etc/udev/scripts/mount.sh start"&lt;BR /&gt;&lt;BR /&gt;This is the script:&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;#!/bin/sh&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;udisksctl mount -b /dev/sda1&lt;BR /&gt;echo "111111111111111111111111111"&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 24 Aug 2023 09:46:26 GMT</pubDate>
    <dc:creator>logic887</dc:creator>
    <dc:date>2023-08-24T09:46:26Z</dc:date>
    <item>
      <title>Custom rules under /etc/udev/rules.d are not taking effect</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-rules-under-etc-udev-rules-d-are-not-taking-effect/m-p/1710574#M211351</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I have created a rule named "99-usb-mount.rules" in the rules.d directory, but it doesn't trigger the script. How can I resolve this issue?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;This is the rules：&lt;BR /&gt;ACTION=="add", SUBSYSTEM=="block", KERNEL=="sda1", RUN+="/bin/bash /etc/udev/scripts/mount.sh start"&lt;BR /&gt;&lt;BR /&gt;This is the script:&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;#!/bin/sh&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;udisksctl mount -b /dev/sda1&lt;BR /&gt;echo "111111111111111111111111111"&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 24 Aug 2023 09:46:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-rules-under-etc-udev-rules-d-are-not-taking-effect/m-p/1710574#M211351</guid>
      <dc:creator>logic887</dc:creator>
      <dc:date>2023-08-24T09:46:26Z</dc:date>
    </item>
    <item>
      <title>Re: Custom rules under /etc/udev/rules.d are not taking effect</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-rules-under-etc-udev-rules-d-are-not-taking-effect/m-p/1712254#M211560</link>
      <description>&lt;P&gt;Which product and which version BSP are you using?&lt;/P&gt;</description>
      <pubDate>Mon, 28 Aug 2023 09:18:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-rules-under-etc-udev-rules-d-are-not-taking-effect/m-p/1712254#M211560</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2023-08-28T09:18:40Z</dc:date>
    </item>
    <item>
      <title>Re: Custom rules under /etc/udev/rules.d are not taking effect</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Custom-rules-under-etc-udev-rules-d-are-not-taking-effect/m-p/1712723#M211612</link>
      <description>IMX8MP Platform &amp;amp;&amp;amp; ubuntu file system</description>
      <pubDate>Tue, 29 Aug 2023 03:53:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Custom-rules-under-etc-udev-rules-d-are-not-taking-effect/m-p/1712723#M211612</guid>
      <dc:creator>logic887</dc:creator>
      <dc:date>2023-08-29T03:53:11Z</dc:date>
    </item>
  </channel>
</rss>