<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: How to use BD71847 internal RTC with IMX8M-MINI controller</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-BD71847-internal-RTC-with-IMX8M-MINI-controller/m-p/1709087#M211230</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The SJA1110 switch does not inherently support STP or any of its variants like RSTP MSTP or ERPS . However, it does support 802.1CB, which is a standard for Frame Replication and Elimination for Reliability.&lt;/P&gt;&lt;P&gt;802.1CB can be used to prevent loops in a network by creating redundant paths and then eliminating duplicate frames.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Tue, 22 Aug 2023 11:55:01 GMT</pubDate>
    <dc:creator>ramprakash08</dc:creator>
    <dc:date>2023-08-22T11:55:01Z</dc:date>
    <item>
      <title>How to use BD71847 internal RTC with IMX8M-MINI controller</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-BD71847-internal-RTC-with-IMX8M-MINI-controller/m-p/1708760#M211194</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I do have IMX8M-MINI controller interfaced with BD71847 power management IC using yocto setup.&lt;/P&gt;&lt;P&gt;Can you provide me the solution on how to use internal RTC of BD71847 with IMX8M-mini controller.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="AMBh_0-1692683755826.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/237353i6E0876DA975E4277/image-size/medium?v=v2&amp;amp;px=400" role="button" title="AMBh_0-1692683755826.png" alt="AMBh_0-1692683755826.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Tue, 22 Aug 2023 05:56:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-use-BD71847-internal-RTC-with-IMX8M-MINI-controller/m-p/1708760#M211194</guid>
      <dc:creator>AMBh</dc:creator>
      <dc:date>2023-08-22T05:56:20Z</dc:date>
    </item>
    <item>
      <title>Re: How to use BD71847 internal RTC with IMX8M-MINI controller</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-BD71847-internal-RTC-with-IMX8M-MINI-controller/m-p/1709085#M211229</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;To use the internal RTC of BD71847 with the IMX8M-MINI controller, you will need to interface the two using the I2C protocol. The BD71847 power management IC has an inbuilt RTC which can be accessed via I2C.&lt;/P&gt;&lt;P&gt;Assuming you have already set up the I2C communication between the IMX8M-MINI and the BD71847, you can access the RTC registers of the BD71847 to set and get the time.&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Aug 2023 11:50:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-use-BD71847-internal-RTC-with-IMX8M-MINI-controller/m-p/1709085#M211229</guid>
      <dc:creator>ramprakash08</dc:creator>
      <dc:date>2023-08-22T11:50:53Z</dc:date>
    </item>
    <item>
      <title>Re: How to use BD71847 internal RTC with IMX8M-MINI controller</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-BD71847-internal-RTC-with-IMX8M-MINI-controller/m-p/1709087#M211230</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The SJA1110 switch does not inherently support STP or any of its variants like RSTP MSTP or ERPS . However, it does support 802.1CB, which is a standard for Frame Replication and Elimination for Reliability.&lt;/P&gt;&lt;P&gt;802.1CB can be used to prevent loops in a network by creating redundant paths and then eliminating duplicate frames.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 22 Aug 2023 11:55:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-use-BD71847-internal-RTC-with-IMX8M-MINI-controller/m-p/1709087#M211230</guid>
      <dc:creator>ramprakash08</dc:creator>
      <dc:date>2023-08-22T11:55:01Z</dc:date>
    </item>
    <item>
      <title>Re: How to use BD71847 internal RTC with IMX8M-MINI controller</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-BD71847-internal-RTC-with-IMX8M-MINI-controller/m-p/1710554#M211348</link>
      <description>&lt;P&gt;Thanks for sharing.&lt;/P&gt;</description>
      <pubDate>Thu, 24 Aug 2023 09:28:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-use-BD71847-internal-RTC-with-IMX8M-MINI-controller/m-p/1710554#M211348</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2023-08-24T09:28:50Z</dc:date>
    </item>
  </channel>
</rss>