<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Gpu performance on imx7ulp device in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Gpu-performance-on-imx7ulp-device/m-p/1708693#M211188</link>
    <description>&lt;P&gt;You are using the ethnaviv driver not the GPU driver we using, so we do not have test the performance for this driver.&lt;/P&gt;
&lt;P&gt;If you want to use the GPU of NXP, you can modify in the &lt;SPAN&gt;&lt;SPAN class="ui-provider fy b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;Menuconfig&lt;/SPAN&gt;&lt;/SPAN&gt;.&lt;/P&gt;
&lt;P&gt;You can refer to our i.MX_Graphics_User's_Guide.pdf document.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class="ui-provider fy b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;In menu configuration enable the following module for the GPU driver:&lt;BR /&gt;CONFIG_MXC_GPU_VIV is a configuration option for GPU driver. In the menuconfig this option is available under Device Drivers&lt;BR /&gt;&amp;gt; MXC support drivers &amp;gt; MXC Vivante GPU support &amp;gt; MXC Vivante GPU support.&lt;BR /&gt;On the screen displayed, select Configure the kernel, select Device Drivers &amp;gt; MXC support drivers &amp;gt; MXC Vivante GPU support&lt;BR /&gt;&amp;gt; MXC Vivante GPU support, and then exit. When the next screen appears, select the following options to enable the GPU driver:&lt;BR /&gt;• Package list &amp;gt; imx-gpu-viv&lt;BR /&gt;• This package provides proprietary binary libraries, and test code built from the GPU for framebuffer&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 22 Aug 2023 03:15:36 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2023-08-22T03:15:36Z</dc:date>
    <item>
      <title>Gpu performance on imx7ulp device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gpu-performance-on-imx7ulp-device/m-p/1698337#M210191</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I am using the imx7ulp board for my project . I am using yoct os . I have to know the gpu performance while rendering or capturing the image. I observed while rendering the image , the logs present in the code was used it under os/linux/drivers/gpu/drm/etnaviv that means my gpu using the ethnaviv driver instead of galcore driver. could you please help me in meausring the performance of gpu which is using the ethnaviv driver for rendering.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 03 Aug 2023 06:44:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gpu-performance-on-imx7ulp-device/m-p/1698337#M210191</guid>
      <dc:creator>ravicalm</dc:creator>
      <dc:date>2023-08-03T06:44:22Z</dc:date>
    </item>
    <item>
      <title>Re: Gpu performance on imx7ulp device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gpu-performance-on-imx7ulp-device/m-p/1698346#M210192</link>
      <description>&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201299"&gt;@Dhruvit&lt;/a&gt;/@chivara could you please respond i hope u guys have given info on gputop tool/gpuinfo.sh script which will internally uses galcore but in my case while rendering I am seeing the logs in ethnaviv module instead of galcore so could you please share any tool or point to the code where we can see the percentage of gpu used .</description>
      <pubDate>Thu, 03 Aug 2023 06:49:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gpu-performance-on-imx7ulp-device/m-p/1698346#M210192</guid>
      <dc:creator>ravicalm</dc:creator>
      <dc:date>2023-08-03T06:49:51Z</dc:date>
    </item>
    <item>
      <title>Re: Gpu performance on imx7ulp device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gpu-performance-on-imx7ulp-device/m-p/1698348#M210193</link>
      <description>&lt;P&gt;is ethanaviv driver runs/helps&amp;nbsp; on gpu or helps the gpu for rendering could you please confirm?&lt;/P&gt;&lt;P&gt;is ethanviv driver will run on cpu?&lt;/P&gt;&lt;P&gt;could you please clarify me about the ethnaviv driver&lt;/P&gt;</description>
      <pubDate>Thu, 03 Aug 2023 06:51:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gpu-performance-on-imx7ulp-device/m-p/1698348#M210193</guid>
      <dc:creator>ravicalm</dc:creator>
      <dc:date>2023-08-03T06:51:45Z</dc:date>
    </item>
    <item>
      <title>Re: Gpu performance on imx7ulp device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gpu-performance-on-imx7ulp-device/m-p/1699268#M210296</link>
      <description>&lt;P&gt;Could you tell us which version BSP are you using, we can help confirm.&lt;/P&gt;</description>
      <pubDate>Fri, 04 Aug 2023 08:54:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gpu-performance-on-imx7ulp-device/m-p/1699268#M210296</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2023-08-04T08:54:47Z</dc:date>
    </item>
    <item>
      <title>Re: Gpu performance on imx7ulp device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gpu-performance-on-imx7ulp-device/m-p/1699276#M210297</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I have the following info &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Operating System: &lt;/SPAN&gt;&lt;SPAN&gt;Poky (Yocto Project Reference Distro) 2.7.1 (warrior) &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Kernel: Linux 4.14.98 &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;uname -a Linux fly 4.14.98 &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;#&lt;/SPAN&gt;&lt;SPAN&gt;1 SMP PREEMPT Mon Jul 10 16:01:38 UTC 2023&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;armv7l GNU/Linux build/yocto/poky/meta-yocto-bsp/conf : file content&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;# We have a conf and classes directory, add to&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;BBPATH BBPATH .= ":${LAYERDIR}" # We have recipes-* directories,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;add to BBFILES BBFILES += "${LAYERDIR}/recipes-*/*/*.bb \ ${LAYERDIR}/recipes-*/*/*.bbappend" &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;BBFILE_COLLECTIONS += "yoctobsp" BBFILE_PATTERN_yoctobsp = "^${LAYERDIR}/"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;BBFILE_PRIORITY_yoctobsp = "5"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;LAYERVERSION_yoctobsp = "4"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;LAYERSERIES_COMPAT_yoctobsp = "warrior"&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 04 Aug 2023 09:03:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gpu-performance-on-imx7ulp-device/m-p/1699276#M210297</guid>
      <dc:creator>ravicalm</dc:creator>
      <dc:date>2023-08-04T09:03:07Z</dc:date>
    </item>
    <item>
      <title>Re: Gpu performance on imx7ulp device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gpu-performance-on-imx7ulp-device/m-p/1699302#M210301</link>
      <description>I have the following info&lt;BR /&gt;&lt;BR /&gt;Operating System: Poky (Yocto Project Reference Distro) 2.7.1 (warrior)&lt;BR /&gt;&lt;BR /&gt;Kernel: Linux 4.14.98&lt;BR /&gt;&lt;BR /&gt;uname -a Linux fly 4.14.98&lt;BR /&gt;&lt;BR /&gt;#1 SMP PREEMPT Mon Jul 10 16:01:38 UTC 2023&lt;BR /&gt;&lt;BR /&gt;armv7l GNU/Linux build/yocto/poky/meta-yocto-bsp/conf : file content&lt;BR /&gt;&lt;BR /&gt;# We have a conf and classes directory, add to&lt;BR /&gt;&lt;BR /&gt;BBPATH BBPATH .= ":${LAYERDIR}" # We have recipes-* directories,&lt;BR /&gt;&lt;BR /&gt;add to BBFILES BBFILES += "${LAYERDIR}/recipes-*/*/*.bb \ ${LAYERDIR}/recipes-*/*/*.bbappend"&lt;BR /&gt;&lt;BR /&gt;BBFILE_COLLECTIONS += "yoctobsp" BBFILE_PATTERN_yoctobsp = "^${LAYERDIR}/"&lt;BR /&gt;&lt;BR /&gt;BBFILE_PRIORITY_yoctobsp = "5"&lt;BR /&gt;&lt;BR /&gt;LAYERVERSION_yoctobsp = "4"&lt;BR /&gt;&lt;BR /&gt;LAYERSERIES_COMPAT_yoctobsp = "warrior"</description>
      <pubDate>Fri, 04 Aug 2023 09:15:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gpu-performance-on-imx7ulp-device/m-p/1699302#M210301</guid>
      <dc:creator>ravicalm</dc:creator>
      <dc:date>2023-08-04T09:15:20Z</dc:date>
    </item>
    <item>
      <title>Re: Gpu performance on imx7ulp device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gpu-performance-on-imx7ulp-device/m-p/1700668#M210430</link>
      <description>&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/57740"&gt;@Rita_Wang&lt;/a&gt; reply??</description>
      <pubDate>Tue, 08 Aug 2023 04:27:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gpu-performance-on-imx7ulp-device/m-p/1700668#M210430</guid>
      <dc:creator>ravicalm</dc:creator>
      <dc:date>2023-08-08T04:27:09Z</dc:date>
    </item>
    <item>
      <title>Re: Gpu performance on imx7ulp device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gpu-performance-on-imx7ulp-device/m-p/1708693#M211188</link>
      <description>&lt;P&gt;You are using the ethnaviv driver not the GPU driver we using, so we do not have test the performance for this driver.&lt;/P&gt;
&lt;P&gt;If you want to use the GPU of NXP, you can modify in the &lt;SPAN&gt;&lt;SPAN class="ui-provider fy b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;Menuconfig&lt;/SPAN&gt;&lt;/SPAN&gt;.&lt;/P&gt;
&lt;P&gt;You can refer to our i.MX_Graphics_User's_Guide.pdf document.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class="ui-provider fy b c d e f g h i j k l m n o p q r s t u v w x y z ab ac ae af ag ah ai aj ak"&gt;In menu configuration enable the following module for the GPU driver:&lt;BR /&gt;CONFIG_MXC_GPU_VIV is a configuration option for GPU driver. In the menuconfig this option is available under Device Drivers&lt;BR /&gt;&amp;gt; MXC support drivers &amp;gt; MXC Vivante GPU support &amp;gt; MXC Vivante GPU support.&lt;BR /&gt;On the screen displayed, select Configure the kernel, select Device Drivers &amp;gt; MXC support drivers &amp;gt; MXC Vivante GPU support&lt;BR /&gt;&amp;gt; MXC Vivante GPU support, and then exit. When the next screen appears, select the following options to enable the GPU driver:&lt;BR /&gt;• Package list &amp;gt; imx-gpu-viv&lt;BR /&gt;• This package provides proprietary binary libraries, and test code built from the GPU for framebuffer&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Aug 2023 03:15:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gpu-performance-on-imx7ulp-device/m-p/1708693#M211188</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2023-08-22T03:15:36Z</dc:date>
    </item>
    <item>
      <title>Re: Gpu performance on imx7ulp device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gpu-performance-on-imx7ulp-device/m-p/1708717#M211191</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/57740"&gt;@Rita_Wang&lt;/a&gt; I am not able to found MXC support drivers under the menuconfig I will give the screen shot of my menuconfig&lt;/P&gt;</description>
      <pubDate>Tue, 22 Aug 2023 04:23:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gpu-performance-on-imx7ulp-device/m-p/1708717#M211191</guid>
      <dc:creator>ravicalm</dc:creator>
      <dc:date>2023-08-22T04:23:14Z</dc:date>
    </item>
    <item>
      <title>Re: Gpu performance on imx7ulp device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gpu-performance-on-imx7ulp-device/m-p/1710235#M211312</link>
      <description>&lt;P&gt;You can following our i.MX Graphics User’s Guide document.&lt;/P&gt;</description>
      <pubDate>Thu, 24 Aug 2023 02:54:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gpu-performance-on-imx7ulp-device/m-p/1710235#M211312</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2023-08-24T02:54:10Z</dc:date>
    </item>
  </channel>
</rss>